/* * Copyright (c) 2013-2014, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /*============================================================================ * @file MessageQ.c * * @brief MessageQ module "server" implementation * * This implementation is geared for use in a "client/server" model, whereby * system-wide data is maintained here as needed and process-specific data * is handled at the "client" level. At the moment, LAD is the only "user" * of this implementation. * * The MessageQ module supports the structured sending and receiving of * variable length messages. This module can be used for homogeneous or * heterogeneous multi-processor messaging. * * MessageQ provides more sophisticated messaging than other modules. It is * typically used for complex situations such as multi-processor messaging. * * The following are key features of the MessageQ module: * -Writers and readers can be relocated to another processor with no * runtime code changes. * -Timeouts are allowed when receiving messages. * -Readers can determine the writer and reply back. * -Receiving a message is deterministic when the timeout is zero. * -Messages can reside on any message queue. * -Supports zero-copy transfers. * -Can send and receive from any type of thread. * -Notification mechanism is specified by application. * -Allows QoS (quality of service) on message buffer pools. For example, * using specific buffer pools for specific message queues. * * Messages are sent and received via a message queue. A reader is a thread * that gets (reads) messages from a message queue. A writer is a thread that * puts (writes) a message to a message queue. Each message queue has one * reader and can have many writers. A thread may read from or write to multiple * message queues. * * Conceptually, the reader thread owns a message queue. The reader thread * creates a message queue. Writer threads a created message queues to * get access to them. * * Message queues are identified by a system-wide unique name. Internally, * MessageQ uses the NameServermodule for managing * these names. The names are used for opening a message queue. Using * names is not required. * * Messages must be allocated from the MessageQ module. Once a message is * allocated, it can be sent on any message queue. Once a message is sent, the * writer loses ownership of the message and should not attempt to modify the * message. Once the reader receives the message, it owns the message. It * may either free the message or re-use the message. * * Messages in a message queue can be of variable length. The only * requirement is that the first field in the definition of a message must be a * MsgHeader structure. For example: * typedef struct MyMsg { * MessageQ_MsgHeader header; * ... * } MyMsg; * * The MessageQ API uses the MessageQ_MsgHeader internally. Your application * should not modify or directly access the fields in the MessageQ_MsgHeader. * * All messages sent via the MessageQ module must be allocated from a * Heap implementation. The heap can be used for * other memory allocation not related to MessageQ. * * An application can use multiple heaps. The purpose of having multiple * heaps is to allow an application to regulate its message usage. For * example, an application can allocate critical messages from one heap of fast * on-chip memory and non-critical messages from another heap of slower * external memory * * MessageQ does support the usage of messages that allocated via the * alloc function. Please refer to the staticMsgInit * function description for more details. * * In a multiple processor system, MessageQ communications to other * processors via MessageQTransport instances. There must be one and * only one MessageQTransport instance for each processor where communication * is desired. * So on a four processor system, each processor must have three * MessageQTransport instance. * * The user only needs to create the MessageQTransport instances. The instances * are responsible for registering themselves with MessageQ. * This is accomplished via the registerTransport function. * * ============================================================================ */ /* Standard headers */ #include /* Qnx specific header files */ #include #include #include #include #include #include #include #include #include #include #include /* Module level headers */ #include #include #include <_MultiProc.h> #include #include <_MessageQ.h> #include <_IpcLog.h> /* ============================================================================= * Macros/Constants * ============================================================================= */ /*! * @brief Name of the reserved NameServer used for MessageQ. */ #define MessageQ_NAMESERVER "MessageQ" /* Slot 0 reserved for NameServer messages: */ #define RESERVED_MSGQ_INDEX 1 /* Define BENCHMARK to quiet key MessageQ APIs: */ //#define BENCHMARK /* ============================================================================= * Structures & Enums * ============================================================================= */ /* structure for MessageQ module state */ typedef struct MessageQ_ModuleObject { Int refCount; /*!< Reference count */ NameServer_Handle nameServer; /*!< Handle to the local NameServer used for storing GP objects */ pthread_mutex_t gate; /*!< Handle of gate to be used for local thread safety */ MessageQ_Config cfg; /*!< Current config values */ MessageQ_Config defaultCfg; /*!< Default config values */ MessageQ_Params defaultInstParams; /*!< Default instance creation parameters */ MessageQ_Handle * queues; /*!< Global array of message queues */ UInt16 numQueues; /*!< Initial number of messageQ objects allowed */ Bool canFreeQueues; /*!< Grow option */ Bits16 seqNum; /*!< sequence number */ } MessageQ_ModuleObject; /*! * @brief Structure for the Handle for the MessageQ. */ typedef struct MessageQ_Object { MessageQ_Params params; /*! Instance specific creation parameters */ MessageQ_QueueId queue; /* Unique id */ MessageQ_QueueIndex queueIndex; /* 16-bit index into the queues array */ Ptr nsKey; /* NameServer key */ Int ownerPid; /* Process ID of owner */ } MessageQ_Object; /* ============================================================================= * Globals * ============================================================================= */ static MessageQ_ModuleObject MessageQ_state = { .refCount = 0, .nameServer = NULL, .queues = NULL, .numQueues = 2u, .canFreeQueues = FALSE, .gate = PTHREAD_MUTEX_INITIALIZER, .defaultCfg.traceFlag = FALSE, .defaultCfg.maxRuntimeEntries = 32u, .defaultCfg.maxNameLen = 32u, }; /*! * @var MessageQ_module * * @brief Pointer to the MessageQ module state. */ MessageQ_ModuleObject * MessageQ_module = &MessageQ_state; /* ============================================================================= * Forward declarations of internal functions * ============================================================================= */ /* Grow the MessageQ table */ static UInt16 _MessageQ_grow(MessageQ_Object * obj); /* ============================================================================= * APIS * ============================================================================= */ /* Function to get default configuration for the MessageQ module. * */ Void MessageQ_getConfig(MessageQ_Config * cfg) { assert(cfg != NULL); /* If setup has not yet been called... */ if (MessageQ_module->refCount < 1) { memcpy(cfg, &MessageQ_module->defaultCfg, sizeof(MessageQ_Config)); } else { memcpy(cfg, &MessageQ_module->cfg, sizeof(MessageQ_Config)); } } /* Function to setup the MessageQ module. */ Int MessageQ_setup(const MessageQ_Config * cfg) { Int status = MessageQ_S_SUCCESS; NameServer_Params params; pthread_mutex_lock(&(MessageQ_module->gate)); LOG1("MessageQ_setup: entered, refCount=%d\n", MessageQ_module->refCount) MessageQ_module->refCount++; if (MessageQ_module->refCount > 1) { status = MessageQ_S_ALREADYSETUP; LOG1("MessageQ module has been already setup, refCount=%d\n", MessageQ_module->refCount) goto exitSetup; } /* Initialize the parameters */ NameServer_Params_init(¶ms); params.maxValueLen = sizeof(UInt32); params.maxNameLen = cfg->maxNameLen; /* Create the nameserver for modules */ MessageQ_module->nameServer = NameServer_create(MessageQ_NAMESERVER, ¶ms); memcpy(&MessageQ_module->cfg, (void *)cfg, sizeof(MessageQ_Config)); MessageQ_module->seqNum = 0; MessageQ_module->numQueues = cfg->maxRuntimeEntries; MessageQ_module->queues = (MessageQ_Handle *) calloc(1, sizeof(MessageQ_Handle) * MessageQ_module->numQueues); exitSetup: LOG1("MessageQ_setup: exiting, refCount=%d\n", MessageQ_module->refCount) pthread_mutex_unlock(&(MessageQ_module->gate)); return (status); } /* * Function to destroy the MessageQ module. */ Int MessageQ_destroy(void) { Int status = MessageQ_S_SUCCESS; UInt32 i; pthread_mutex_lock(&(MessageQ_module->gate)); LOG1("MessageQ_destroy: entered, refCount=%d\n", MessageQ_module->refCount) /* Decrease the refCount */ MessageQ_module->refCount--; if (MessageQ_module->refCount > 0) { goto exitDestroy; } /* Delete any Message Queues that have not been deleted so far. */ for (i = 0; i< MessageQ_module->numQueues; i++) { if (MessageQ_module->queues [i] != NULL) { MessageQ_delete(&(MessageQ_module->queues [i])); } } if (MessageQ_module->nameServer != NULL) { /* Delete the nameserver for modules */ status = NameServer_delete(&MessageQ_module->nameServer); } /* Since MessageQ_module->gate was not allocated, no need to delete. */ if (MessageQ_module->queues != NULL) { free(MessageQ_module->queues); MessageQ_module->queues = NULL; } memset(&MessageQ_module->cfg, 0, sizeof(MessageQ_Config)); MessageQ_module->numQueues = 0u; MessageQ_module->canFreeQueues = TRUE; exitDestroy: LOG1("MessageQ_destroy: exiting, refCount=%d\n", MessageQ_module->refCount) pthread_mutex_unlock(&(MessageQ_module->gate)); return (status); } /* Function to initialize the parameters for the MessageQ instance. */ Void MessageQ_Params_init(MessageQ_Params * params) { memcpy(params, &(MessageQ_module->defaultInstParams), sizeof(MessageQ_Params)); return; } /* * Function to create a MessageQ object for receiving. */ MessageQ_Handle MessageQ_createWithQueueId(String name, const MessageQ_Params * params, UInt32 queueId) { Int status = MessageQ_S_SUCCESS; MessageQ_Object * obj = NULL; Bool found = FALSE; UInt16 count = 0; UInt16 queueIndex = 0u; UInt16 procId; int i; LOG1("MessageQ_create: creating '%s'\n", name) /* Create the generic obj */ obj = (MessageQ_Object *)calloc(1, sizeof(MessageQ_Object)); pthread_mutex_lock(&(MessageQ_module->gate)); count = MessageQ_module->numQueues; /* Search the dynamic array for any holes */ /* We start from 1, as 0 is reserved for binding NameServer: */ for (i = RESERVED_MSGQ_INDEX; i < count ; i++) { if (MessageQ_module->queues [i] == NULL) { MessageQ_module->queues [i] = (MessageQ_Handle)obj; queueIndex = i; found = TRUE; break; } } if (found == FALSE) { /* Growth is always allowed. */ queueIndex = _MessageQ_grow(obj); } pthread_mutex_unlock(&(MessageQ_module->gate)); if (params != NULL) { /* Populate the params member */ memcpy((Ptr)&obj->params, (Ptr)params, sizeof(MessageQ_Params)); } procId = MultiProc_self(); obj->queueIndex = queueIndex; /* create globally unique messageQ ID */ obj->queue = (MessageQ_QueueId)(((UInt32)procId << 16) | queueId); obj->ownerPid = 0; if (name != NULL) { obj->nsKey = NameServer_addUInt32(MessageQ_module->nameServer, name, obj->queue); } /* Cleanup if fail */ if (status < 0) { MessageQ_delete((MessageQ_Handle *)&obj); } LOG1("MessageQ_create: returning %p\n", obj) return ((MessageQ_Handle)obj); } /* * Function to delete a MessageQ object for a specific slave processor. */ Int MessageQ_delete(MessageQ_Handle * handlePtr) { Int status = MessageQ_S_SUCCESS; MessageQ_Object *obj; MessageQ_Handle queue; obj = (MessageQ_Object *)(*handlePtr); LOG1("MessageQ_delete: deleting %p\n", obj) queue = MessageQ_module->queues[obj->queueIndex]; if (queue != obj) { LOG1(" ERROR: obj != MessageQ_module->queues[%d]\n", (MessageQ_QueueIndex)(obj->queueIndex)) } if (obj->nsKey != NULL) { /* Remove from the name server */ status = NameServer_removeEntry(MessageQ_module->nameServer, obj->nsKey); if (status < 0) { /* Override with a MessageQ status code. */ status = MessageQ_E_FAIL; } else { status = MessageQ_S_SUCCESS; } } pthread_mutex_lock(&(MessageQ_module->gate)); /* Clear the MessageQ obj from array. */ MessageQ_module->queues[(MessageQ_QueueIndex)obj->queueIndex] = NULL; /* Release the local lock */ pthread_mutex_unlock(&(MessageQ_module->gate)); /* Now free the obj */ free(obj); *handlePtr = NULL; LOG1("MessageQ_delete: returning %d\n", status) return (status); } /* Returns the MessageQ_QueueId associated with the handle. */ MessageQ_QueueId MessageQ_getQueueId(MessageQ_Handle handle) { MessageQ_Object * obj = (MessageQ_Object *)handle; UInt32 queueId; queueId = (obj->queue); return queueId; } /*! * @brief Grow the MessageQ table * * @param obj Pointer to the MessageQ object. * * @sa _MessageQ_grow * */ static UInt16 _MessageQ_grow(MessageQ_Object * obj) { UInt16 queueIndex = MessageQ_module->numQueues; UInt16 oldSize; MessageQ_Handle * queues; MessageQ_Handle * oldQueues; /* No parameter validation required since this is an internal function. */ oldSize = (MessageQ_module->numQueues) * sizeof(MessageQ_Handle); /* Allocate larger table */ queues = calloc(1, oldSize + sizeof(MessageQ_Handle)); /* Copy contents into new table */ memcpy(queues, MessageQ_module->queues, oldSize); /* Fill in the new entry */ queues[queueIndex] = (MessageQ_Handle)obj; /* Hook-up new table */ oldQueues = MessageQ_module->queues; MessageQ_module->queues = queues; MessageQ_module->numQueues++; /* Delete old table if not statically defined */ if (MessageQ_module->canFreeQueues == TRUE) { free(oldQueues); } else { MessageQ_module->canFreeQueues = TRUE; } LOG1("_MessageQ_grow: queueIndex: 0x%x\n", queueIndex) return (queueIndex); } /* * This is a helper function to initialize a message. */ Void MessageQ_msgInit(MessageQ_Msg msg) { msg->reserved0 = 0; /* We set this to distinguish from NameServerMsg */ msg->replyId = (UInt16)MessageQ_INVALIDMESSAGEQ; msg->msgId = MessageQ_INVALIDMSGID; msg->dstId = (UInt16)MessageQ_INVALIDMESSAGEQ; msg->flags = MessageQ_HEADERVERSION | MessageQ_NORMALPRI; msg->srcProc = MultiProc_self(); pthread_mutex_lock(&(MessageQ_module->gate)); msg->seqNum = MessageQ_module->seqNum++; pthread_mutex_unlock(&(MessageQ_module->gate)); } NameServer_Handle MessageQ_getNameServerHandle(void) { return MessageQ_module->nameServer; } Void MessageQ_setQueueOwner(MessageQ_Handle handle, Int pid) { handle->ownerPid = pid; return; } Void MessageQ_cleanupOwner(Int pid) { MessageQ_Handle queue; Int i; for (i = 0; i < MessageQ_module->numQueues; i++) { queue = MessageQ_module->queues[i]; if (queue != NULL && queue->ownerPid == pid) { MessageQ_delete(&queue); } } }