/* * Copyright (c) 2011, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* * omx_benchmark.c * * Benchmark average round trip time for equivalent of SysLink 2 RcmClient_exec. * * This calls the fxnDouble RcmServer function, similar to the SysLink 2 ducati * rcm/singletest. * * Requires: * -------- * test_omx.c sample, with fxnDouble registered in RcmServer table. * * To Configure Ducati code for Benchmarking: * ------------------------------------------ * In package.bld: * - Set profile=release in package.bld * In bencmark test code: * - Disable printf's, trace. * In benchmark .cfg file: * - Defaults.common$.diags_ASSERT = Diags.ALWAYS_OFF * - Defaults.common$.logger = null; * * Expected Result: (Linux, Panda Board ES 2.1, rpmsg13 branch) * --------------- * avg time: 110 usecs * * Expected Result: (Qnx, Playbook ES 2.1, no branch yet - local development) * --------------- * avg time: 140 usecs */ #include #include #include #include #include #include #include #include #include #include #include //#include #include "ti/ipc/rpmsg_omx.h" #include "omx_packet.h" #include "PerfUtils.h" #include typedef struct { int a; int b; } fxn_error_args; /* Note: Set bit 31 to indicate static function indicies: * This function order will be hardcoded on BIOS side, hence preconfigured: * See src/examples/srvmgr/test_omx.c. */ #define FXN_IDX_FXNERROR (4 | 0x80000000) unsigned long diff(struct timespec start, struct timespec end) { unsigned long nsecs; struct timespec temp; if ((end.tv_nsec-start.tv_nsec)<0) { temp.tv_sec = end.tv_sec-start.tv_sec-1; temp.tv_nsec = 1000000000+end.tv_nsec-start.tv_nsec; } else { temp.tv_sec = end.tv_sec-start.tv_sec; temp.tv_nsec = end.tv_nsec-start.tv_nsec; } nsecs = temp.tv_sec * 1000000 + temp.tv_nsec; return nsecs; } int exec_cmd(int fd, char *msg, int len, char *reply_msg, int *reply_len) { int ret = 0; ret = write(fd, msg, len); if (ret < 0) { perror("Can't write to OMX instance"); return -1; } /* Now, await normal function result from OMX service: */ // Note: len should be max length of response expected. ret = read(fd, reply_msg, len); if (ret < 0) { perror("Can't read from OMX instance"); return -1; } else { *reply_len = ret; } return(0); } void init_omx_packet(omx_packet *packet, uint16_t desc) { /* initialize the packet structure */ packet->desc |= desc << OMX_DESC_TYPE_SHIFT; packet->msg_id = 0; packet->flags = OMX_POOLID_JOBID_NONE; packet->fxn_idx = OMX_INVALIDFXNIDX; packet->result = 0; } void test_exec_call(int fd, int test_id, uint32_t test_arg) { uint16_t server_status; int packet_len; int reply_len; char packet_buf[512] = {0}; char return_buf[512] = {0}; omx_packet *packet = (omx_packet *)packet_buf; omx_packet *rtn_packet = (omx_packet *)return_buf; fxn_error_args *fxn_args = (fxn_error_args *)&packet->data[1]; /* Set Packet Header for the RCMServer, synchronous execution: */ init_omx_packet(packet, OMX_DESC_MSG); /* Set OMX Function Index to call, with data: */ packet->fxn_idx = FXN_IDX_FXNERROR; /* Set data for the OMX function: */ packet->data_size = sizeof(fxn_error_args) + sizeof(int); packet->data[0] = 0; // RPC_OMX_MAP_INFO_NONE fxn_args->a = test_id; fxn_args->b = test_arg; /* Exec command: */ packet_len = sizeof(omx_packet) + packet->data_size; exec_cmd(fd, (char *)packet, packet_len, (char *)rtn_packet, &reply_len); /* Decode reply: */ server_status = (OMX_DESC_TYPE_MASK & rtn_packet->desc) >> OMX_DESC_TYPE_SHIFT; if (server_status == OMXSERVER_STATUS_SUCCESS) { printf ("omx_errors: called fxnError(%d)), result = %d\n", fxn_args->a, rtn_packet->result); } else { printf("omx_errors: Failed to execute fxnError: server status: %d\n", server_status); } } int main(int argc, char *argv[]) { int fd; int ret; int test_id = -1; int core_id = 0; uint32_t test_arg = (uint32_t)-1; bool test_arg_set = false; int c; struct omx_conn_req connreq = { .name = "OMX" }; while (1) { c = getopt (argc, argv, "t:c:a:"); if (c == -1) break; switch (c) { case 't': test_id = atoi(optarg); break; case 'c': core_id = atoi(optarg); break; case 'a': sscanf(optarg, "%x", &test_arg); test_arg_set = true; break; default: printf ("Unrecognized argument\n"); } } switch (test_id) { case 1: printf("DivByZero Test\n"); break; case 2: printf("WatchDog Test\n"); break; case 3: printf("MMU Fault Test\n"); if (test_arg == 1) { test_id = 3; } else if (test_arg == 2) { test_id = 4; } else { printf("Invalid arg\n"); return 1; } break; case 4: printf("AMMU Fault Test\n"); if (test_arg == 1) { test_id = 5; } else if (test_arg == 2) { test_id = 6; } else { printf("Invalid arg\n"); return 1; } break; case 5: printf("Read Inv. Addr Test\n"); test_id = 7; if (!test_arg_set) { printf("Invalid arg\n"); return 1; } break; case 6: printf("Write Inv. Addr Test\n"); test_id = 8; if (!test_arg_set) { printf("Invalid arg\n"); return 1; } break; default: printf("Invalid test id\n"); return 1; } if (core_id < 0 || core_id > 1) { printf("Invalid core id\n"); return 1; } printf("omx_sample: Connecting to core %d\n", core_id); if (core_id == 0) { /* Connect to the OMX ServiceMgr on Ducati core 0: */ fd = open("/dev/rpmsg-omx0", O_RDWR); } else { /* Connect to the OMX ServiceMgr on Ducati core 1: */ fd = open("/dev/rpmsg-omx1", O_RDWR); } if (fd < 0) { perror("Can't open OMX device"); return 1; } /* Create an OMX server instance, and rebind its address to this * file descriptor. */ ret = ioctl(fd, OMX_IOCCONNECT, &connreq); if (ret < 0) { perror("Can't connect to OMX instance"); return 1; } printf("omx_sample: Connected to %s\n", connreq.name); test_exec_call(fd, test_id, test_arg); /* Terminate connection and destroy OMX instance */ ret = close(fd); if (ret < 0) { perror("Can't close OMX fd ??"); return 1; } printf("omx_sample: Closed connection to %s!\n", connreq.name); return 0; }