]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - ipc/ipcdev.git/blobdiff - configure.ac
VirtQueue: dra7xx: poll for init completion status
[ipc/ipcdev.git] / configure.ac
index 9e6e55c72cde9da19c37eb9b2ba89bd6bd559a60..4d4a559cf33b4492da8fa24ac867d9fc7462b141 100644 (file)
@@ -1,5 +1,5 @@
 #
-#   Copyright (c) 2013-2015 Texas Instruments Incorporated - http://www.ti.com
+#   Copyright (c) 2013-2018 Texas Instruments Incorporated - http://www.ti.com
 #
 #   Redistribution and use in source and binary forms, with or without
 #   modification, are permitted provided that the following conditions
@@ -50,6 +50,7 @@ AM_INIT_AUTOMAKE([foreign])
 AM_MAINTAINER_MODE([disable])
 
 # Initalize libtool but disable fortran check
+LT_INIT
 define([AC_LIBTOOL_LANG_F77_CONFIG], [:])dnl
 AC_PROG_LIBTOOL(gcc)
 
@@ -67,7 +68,7 @@ AC_SUBST([AM_LDFLAGS])
 
 # Add config variables/options and check them
 # Note that 6614 isn't documented and, though it may work, is planned for removal
-AC_ARG_VAR(PLATFORM, Platform to build. Options are: 'OMAPL138' 'OMAP54XX' '66AK2E' 'TCI6630' 'TCI6636' 'TCI6638' '66AK2G' and 'DRA7XX'. If not defined all platforms will be built.)
+AC_ARG_VAR(PLATFORM, Platform to build. Options are: 'OMAPL138' 'OMAP54XX' '66AK2E' 'TCI6630' 'TCI6636' 'TCI6638' '66AK2G' 'DRA7XX' and 'AM65XX'. If not defined all platforms will be built.)
 AC_ARG_VAR(CMEM_INSTALL_DIR, Installation path directory to the CMEM libraries)
 AC_ARG_VAR(KERNEL_INSTALL_DIR, Installation path to the Linux kernel.)
 AC_ARG_VAR(AF_RPMSG, Address Family used by the RPMSG driver)
@@ -92,9 +93,11 @@ AS_IF([test "x$PLATFORM" = "xOMAPL138"],
   [AC_MSG_NOTICE([PLATFORM is set to ${PLATFORM}])],
   [AS_IF([test "x$PLATFORM" = "xDRA7XX"],
   [AC_MSG_NOTICE([PLATFORM is set to ${PLATFORM}])],
+  [AS_IF([test "x$PLATFORM" = "xAM65XX"],
+  [AC_MSG_NOTICE([PLATFORM is set to ${PLATFORM}])],
   [AS_IF([test "x$PLATFORM" = "x"],
   [AC_MSG_NOTICE([PLATFORM is not set. All supported platforms will be built ....])],
-  [AC_MSG_ERROR([PLATFORM is set to "${PLATFORM}": run ./configure --help for available PLATFORM options])])])])])])])])])])])
+  [AC_MSG_ERROR([PLATFORM is set to "${PLATFORM}": run ./configure --help for available PLATFORM options])])])])])])])])])])])])
 
 # If platform is specified, make sure at least one of
 # KERNEL_INSTALL_DIR or AF_MSG are set.
@@ -123,6 +126,7 @@ AM_CONDITIONAL([TCI6638], [test "x$PLATFORM" = "xTCI6638"])
 AM_CONDITIONAL([C66AK2G], [test "x$PLATFORM" = "x66AK2G"])
 AM_CONDITIONAL([OMAP54XX_SMP], [test "x$PLATFORM" = "xOMAP54XX"])
 AM_CONDITIONAL([DRA7XX], [test "x$PLATFORM" = "xDRA7XX"])
+AM_CONDITIONAL([AM65XX], [test "x$PLATFORM" = "xAM65XX"])
 AM_CONDITIONAL([CMEM], [test "x$CMEM_INSTALL_DIR" != "x"])
 AM_CONDITIONAL([KDIR], [test "x$KERNEL_INSTALL_DIR" != "x"])
 AM_CONDITIONAL([KERNEL_INSTALL_DIR], [test -n "$KERNEL_INSTALL_DIR"])