diff --git a/configure b/configure
index 38610a5049ca28f9df3add4bf89bb82ce8165780..df1798ffd614efd85ea734b4fc0b5ec33d3febf7 100755 (executable)
--- a/configure
+++ b/configure
CXX C++ compiler command
CXXFLAGS C++ compiler flags
CXXCPP C++ preprocessor
- PLATFORM Platform to build. Options are: 'OMAPL138' 'OMAP54XX' 'C66AK2E'
+ PLATFORM Platform to build. Options are: 'OMAPL138' 'OMAP54XX' '66AK2E'
'TCI6630' 'TCI6636' 'TCI6638' and 'DRA7XX'. If not defined all
platforms will be built.
CMEM_INSTALL_DIR
{ echo "$as_me:$LINENO: PLATFORM is set to ${PLATFORM}" >&5
echo "$as_me: PLATFORM is set to ${PLATFORM}" >&6;}
else
- if test "x$PLATFORM" = "xC66AK2E"; then
+ if test "x$PLATFORM" = "x66AK2E"; then
{ echo "$as_me:$LINENO: PLATFORM is set to ${PLATFORM}" >&5
echo "$as_me: PLATFORM is set to ${PLATFORM}" >&6;}
else
-if test "x$PLATFORM" = "xC66AK2E"; then
+if test "x$PLATFORM" = "x66AK2E"; then
C66AK2E_TRUE=
C66AK2E_FALSE='#'
else
ac_config_files="$ac_config_files linux/src/tests/Makefile"
+ ac_config_files="$ac_config_files linux/src/transport/Makefile"
+
cat >confcache <<\_ACEOF
# This file is a shell script that caches the results of configure
# tests run on this system so they can be shared between configure
"linux/src/mm/libmmrpc.pc" ) CONFIG_FILES="$CONFIG_FILES linux/src/mm/libmmrpc.pc" ;;
"linux/src/daemon/Makefile" ) CONFIG_FILES="$CONFIG_FILES linux/src/daemon/Makefile" ;;
"linux/src/tests/Makefile" ) CONFIG_FILES="$CONFIG_FILES linux/src/tests/Makefile" ;;
+ "linux/src/transport/Makefile" ) CONFIG_FILES="$CONFIG_FILES linux/src/transport/Makefile" ;;
"depfiles" ) CONFIG_COMMANDS="$CONFIG_COMMANDS depfiles" ;;
*) { { echo "$as_me:$LINENO: error: invalid argument: $ac_config_target" >&5
echo "$as_me: error: invalid argument: $ac_config_target" >&2;}