index 04701da536f33a7c39d7bb01b87a70ae3a776df5..fc98710e2a1df7159cd72a01ffc011784748c3bc 100755 (executable)
--- a/linux/build-aux/depcomp
+++ b/linux/build-aux/depcomp
#! /bin/sh
# depcomp - compile a program generating dependencies as side-effects
-scriptversion=2005-07-09.11
+scriptversion=2013-05-30.07; # UTC
-# Copyright (C) 1999, 2000, 2003, 2004, 2005 Free Software Foundation, Inc.
+# Copyright (C) 1999-2014 Free Software Foundation, Inc.
# This program is free software; you can redistribute it and/or modify
# it under the terms of the GNU General Public License as published by
# GNU General Public License for more details.
# You should have received a copy of the GNU General Public License
-# along with this program; if not, write to the Free Software
-# Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA
-# 02110-1301, USA.
+# along with this program. If not, see <http://www.gnu.org/licenses/>.
# As a special exception to the GNU General Public License, if you
# distribute this file as part of a program that contains a
case $1 in
'')
- echo "$0: No command. Try \`$0 --help' for more information." 1>&2
- exit 1;
- ;;
+ echo "$0: No command. Try '$0 --help' for more information." 1>&2
+ exit 1;
+ ;;
-h | --h*)
cat <<\EOF
Usage: depcomp [--help] [--version] PROGRAM [ARGS]
Environment variables:
depmode Dependency tracking mode.
- source Source file read by `PROGRAMS ARGS'.
- object Object file output by `PROGRAMS ARGS'.
+ source Source file read by 'PROGRAMS ARGS'.
+ object Object file output by 'PROGRAMS ARGS'.
DEPDIR directory where to store dependencies.
depfile Dependency file to output.
- tmpdepfile Temporary file to use when outputing dependencies.
+ tmpdepfile Temporary file to use when outputting dependencies.
libtool Whether libtool is used (yes/no).
Report bugs to <bug-automake@gnu.org>.
;;
esac
+# Get the directory component of the given path, and save it in the
+# global variables '$dir'. Note that this directory component will
+# be either empty or ending with a '/' character. This is deliberate.
+set_dir_from ()
+{
+ case $1 in
+ */*) dir=`echo "$1" | sed -e 's|/[^/]*$|/|'`;;
+ *) dir=;;
+ esac
+}
+
+# Get the suffix-stripped basename of the given path, and save it the
+# global variable '$base'.
+set_base_from ()
+{
+ base=`echo "$1" | sed -e 's|^.*/||' -e 's/\.[^.]*$//'`
+}
+
+# If no dependency file was actually created by the compiler invocation,
+# we still have to create a dummy depfile, to avoid errors with the
+# Makefile "include basename.Plo" scheme.
+make_dummy_depfile ()
+{
+ echo "#dummy" > "$depfile"
+}
+
+# Factor out some common post-processing of the generated depfile.
+# Requires the auxiliary global variable '$tmpdepfile' to be set.
+aix_post_process_depfile ()
+{
+ # If the compiler actually managed to produce a dependency file,
+ # post-process it.
+ if test -f "$tmpdepfile"; then
+ # Each line is of the form 'foo.o: dependency.h'.
+ # Do two passes, one to just change these to
+ # $object: dependency.h
+ # and one to simply output
+ # dependency.h:
+ # which is needed to avoid the deleted-header problem.
+ { sed -e "s,^.*\.[$lower]*:,$object:," < "$tmpdepfile"
+ sed -e "s,^.*\.[$lower]*:[$tab ]*,," -e 's,$,:,' < "$tmpdepfile"
+ } > "$depfile"
+ rm -f "$tmpdepfile"
+ else
+ make_dummy_depfile
+ fi
+}
+
+# A tabulation character.
+tab=' '
+# A newline character.
+nl='
+'
+# Character ranges might be problematic outside the C locale.
+# These definitions help.
+upper=ABCDEFGHIJKLMNOPQRSTUVWXYZ
+lower=abcdefghijklmnopqrstuvwxyz
+digits=0123456789
+alpha=${upper}${lower}
+
if test -z "$depmode" || test -z "$source" || test -z "$object"; then
echo "depcomp: Variables source, object and depmode must be set" 1>&2
exit 1
rm -f "$tmpdepfile"
+# Avoid interferences from the environment.
+gccflag= dashmflag=
+
# Some modes work just like other modes, but use different flags. We
# parameterize here, but still list the modes in the big case below,
# to make depend.m4 easier to write. Note that we *cannot* use a case
fi
if test "$depmode" = dashXmstdout; then
- # This is just like dashmstdout with a different argument.
- dashmflag=-xM
- depmode=dashmstdout
+ # This is just like dashmstdout with a different argument.
+ dashmflag=-xM
+ depmode=dashmstdout
+fi
+
+cygpath_u="cygpath -u -f -"
+if test "$depmode" = msvcmsys; then
+ # This is just like msvisualcpp but w/o cygpath translation.
+ # Just convert the backslash-escaped backslashes to single forward
+ # slashes to satisfy depend.m4
+ cygpath_u='sed s,\\\\,/,g'
+ depmode=msvisualcpp
+fi
+
+if test "$depmode" = msvc7msys; then
+ # This is just like msvc7 but w/o cygpath translation.
+ # Just convert the backslash-escaped backslashes to single forward
+ # slashes to satisfy depend.m4
+ cygpath_u='sed s,\\\\,/,g'
+ depmode=msvc7
+fi
+
+if test "$depmode" = xlc; then
+ # IBM C/C++ Compilers xlc/xlC can output gcc-like dependency information.
+ gccflag=-qmakedep=gcc,-MF
+ depmode=gcc
fi
case "$depmode" in
## gcc 3 implements dependency tracking that does exactly what
## we want. Yay! Note: for some reason libtool 1.4 doesn't like
## it if -MD -MP comes after the -MF stuff. Hmm.
- "$@" -MT "$object" -MD -MP -MF "$tmpdepfile"
+## Unfortunately, FreeBSD c89 acceptance of flags depends upon
+## the command line argument order; so add the flags where they
+## appear in depend2.am. Note that the slowdown incurred here
+## affects only configure: in makefiles, %FASTDEP% shortcuts this.
+ for arg
+ do
+ case $arg in
+ -c) set fnord "$@" -MT "$object" -MD -MP -MF "$tmpdepfile" "$arg" ;;
+ *) set fnord "$@" "$arg" ;;
+ esac
+ shift # fnord
+ shift # $arg
+ done
+ "$@"
stat=$?
- if test $stat -eq 0; then :
- else
+ if test $stat -ne 0; then
rm -f "$tmpdepfile"
exit $stat
fi
;;
gcc)
+## Note that this doesn't just cater to obsosete pre-3.x GCC compilers.
+## but also to in-use compilers like IMB xlc/xlC and the HP C compiler.
+## (see the conditional assignment to $gccflag above).
## There are various ways to get dependency output from gcc. Here's
## why we pick this rather obscure method:
## - Don't want to use -MD because we'd like the dependencies to end
## up in a subdir. Having to rename by hand is ugly.
## (We might end up doing this anyway to support other compilers.)
## - The DEPENDENCIES_OUTPUT environment variable makes gcc act like
-## -MM, not -M (despite what the docs say).
+## -MM, not -M (despite what the docs say). Also, it might not be
+## supported by the other compilers which use the 'gcc' depmode.
## - Using -M directly means running the compiler twice (even worse
## than renaming).
if test -z "$gccflag"; then
fi
"$@" -Wp,"$gccflag$tmpdepfile"
stat=$?
- if test $stat -eq 0; then :
- else
+ if test $stat -ne 0; then
rm -f "$tmpdepfile"
exit $stat
fi
rm -f "$depfile"
echo "$object : \\" > "$depfile"
- alpha=ABCDEFGHIJKLMNOPQRSTUVWXYZabcdefghijklmnopqrstuvwxyz
-## The second -e expression handles DOS-style file names with drive letters.
+ # The second -e expression handles DOS-style file names with drive
+ # letters.
sed -e 's/^[^:]*: / /' \
-e 's/^['$alpha']:\/[^:]*: / /' < "$tmpdepfile" >> "$depfile"
-## This next piece of magic avoids the `deleted header file' problem.
+## This next piece of magic avoids the "deleted header file" problem.
## The problem is that when a header file which appears in a .P file
## is deleted, the dependency causes make to die (because there is
## typically no way to rebuild the header). We avoid this by adding
## dummy dependencies for each header file. Too bad gcc doesn't do
## this for us directly.
- tr ' ' '
-' < "$tmpdepfile" |
-## Some versions of gcc put a space before the `:'. On the theory
+## Some versions of gcc put a space before the ':'. On the theory
## that the space means something, we add a space to the output as
-## well.
+## well. hp depmode also adds that space, but also prefixes the VPATH
+## to the object. Take care to not repeat it in the output.
## Some versions of the HPUX 10.20 sed can't process this invocation
## correctly. Breaking it into two sed invocations is a workaround.
- sed -e 's/^\\$//' -e '/^$/d' -e '/:$/d' | sed -e 's/$/ :/' >> "$depfile"
+ tr ' ' "$nl" < "$tmpdepfile" \
+ | sed -e 's/^\\$//' -e '/^$/d' -e "s|.*$object$||" -e '/:$/d' \
+ | sed -e 's/$/ :/' >> "$depfile"
rm -f "$tmpdepfile"
;;
"$@" -MDupdate "$tmpdepfile"
fi
stat=$?
- if test $stat -eq 0; then :
- else
+ if test $stat -ne 0; then
rm -f "$tmpdepfile"
exit $stat
fi
if test -f "$tmpdepfile"; then # yes, the sourcefile depend on other files
echo "$object : \\" > "$depfile"
-
# Clip off the initial element (the dependent). Don't try to be
# clever and replace this with sed code, as IRIX sed won't handle
# lines with more than a fixed number of characters (4096 in
# IRIX 6.2 sed, 8192 in IRIX 6.5). We also remove comment lines;
- # the IRIX cc adds comments like `#:fec' to the end of the
+ # the IRIX cc adds comments like '#:fec' to the end of the
# dependency line.
- tr ' ' '
-' < "$tmpdepfile" \
- | sed -e 's/^.*\.o://' -e 's/#.*$//' -e '/^$/ d' | \
- tr '
-' ' ' >> $depfile
- echo >> $depfile
-
+ tr ' ' "$nl" < "$tmpdepfile" \
+ | sed -e 's/^.*\.o://' -e 's/#.*$//' -e '/^$/ d' \
+ | tr "$nl" ' ' >> "$depfile"
+ echo >> "$depfile"
# The second pass generates a dummy entry for each header file.
- tr ' ' '
-' < "$tmpdepfile" \
- | sed -e 's/^.*\.o://' -e 's/#.*$//' -e '/^$/ d' -e 's/$/:/' \
- >> $depfile
+ tr ' ' "$nl" < "$tmpdepfile" \
+ | sed -e 's/^.*\.o://' -e 's/#.*$//' -e '/^$/ d' -e 's/$/:/' \
+ >> "$depfile"
else
- # The sourcefile does not contain any dependencies, so just
- # store a dummy comment line, to avoid errors with the Makefile
- # "include basename.Plo" scheme.
- echo "#dummy" > "$depfile"
+ make_dummy_depfile
fi
rm -f "$tmpdepfile"
;;
+xlc)
+ # This case exists only to let depend.m4 do its work. It works by
+ # looking at the text of this script. This case will never be run,
+ # since it is checked for above.
+ exit 1
+ ;;
+
aix)
# The C for AIX Compiler uses -M and outputs the dependencies
# in a .u file. In older versions, this file always lives in the
- # current directory. Also, the AIX compiler puts `$object:' at the
+ # current directory. Also, the AIX compiler puts '$object:' at the
# start of each line; $object doesn't have directory information.
# Version 6 uses the directory in both cases.
- stripped=`echo "$object" | sed 's/\(.*\)\..*$/\1/'`
- tmpdepfile="$stripped.u"
+ set_dir_from "$object"
+ set_base_from "$object"
if test "$libtool" = yes; then
+ tmpdepfile1=$dir$base.u
+ tmpdepfile2=$base.u
+ tmpdepfile3=$dir.libs/$base.u
"$@" -Wc,-M
else
+ tmpdepfile1=$dir$base.u
+ tmpdepfile2=$dir$base.u
+ tmpdepfile3=$dir$base.u
"$@" -M
fi
stat=$?
-
- if test -f "$tmpdepfile"; then :
- else
- stripped=`echo "$stripped" | sed 's,^.*/,,'`
- tmpdepfile="$stripped.u"
+ if test $stat -ne 0; then
+ rm -f "$tmpdepfile1" "$tmpdepfile2" "$tmpdepfile3"
+ exit $stat
fi
- if test $stat -eq 0; then :
- else
+ for tmpdepfile in "$tmpdepfile1" "$tmpdepfile2" "$tmpdepfile3"
+ do
+ test -f "$tmpdepfile" && break
+ done
+ aix_post_process_depfile
+ ;;
+
+tcc)
+ # tcc (Tiny C Compiler) understand '-MD -MF file' since version 0.9.26
+ # FIXME: That version still under development at the moment of writing.
+ # Make that this statement remains true also for stable, released
+ # versions.
+ # It will wrap lines (doesn't matter whether long or short) with a
+ # trailing '\', as in:
+ #
+ # foo.o : \
+ # foo.c \
+ # foo.h \
+ #
+ # It will put a trailing '\' even on the last line, and will use leading
+ # spaces rather than leading tabs (at least since its commit 0394caf7
+ # "Emit spaces for -MD").
+ "$@" -MD -MF "$tmpdepfile"
+ stat=$?
+ if test $stat -ne 0; then
rm -f "$tmpdepfile"
exit $stat
fi
-
- if test -f "$tmpdepfile"; then
- outname="$stripped.o"
- # Each line is of the form `foo.o: dependent.h'.
- # Do two passes, one to just change these to
- # `$object: dependent.h' and one to simply `dependent.h:'.
- sed -e "s,^$outname:,$object :," < "$tmpdepfile" > "$depfile"
- sed -e "s,^$outname: \(.*\)$,\1:," < "$tmpdepfile" >> "$depfile"
- else
- # The sourcefile does not contain any dependencies, so just
- # store a dummy comment line, to avoid errors with the Makefile
- # "include basename.Plo" scheme.
- echo "#dummy" > "$depfile"
- fi
+ rm -f "$depfile"
+ # Each non-empty line is of the form 'foo.o : \' or ' dep.h \'.
+ # We have to change lines of the first kind to '$object: \'.
+ sed -e "s|.*:|$object :|" < "$tmpdepfile" > "$depfile"
+ # And for each line of the second kind, we have to emit a 'dep.h:'
+ # dummy dependency, to avoid the deleted-header problem.
+ sed -n -e 's|^ *\(.*\) *\\$|\1:|p' < "$tmpdepfile" >> "$depfile"
rm -f "$tmpdepfile"
;;
-icc)
- # Intel's C compiler understands `-MD -MF file'. However on
- # icc -MD -MF foo.d -c -o sub/foo.o sub/foo.c
- # ICC 7.0 will fill foo.d with something like
- # foo.o: sub/foo.c
- # foo.o: sub/foo.h
- # which is wrong. We want:
- # sub/foo.o: sub/foo.c
- # sub/foo.o: sub/foo.h
- # sub/foo.c:
- # sub/foo.h:
- # ICC 7.1 will output
+## The order of this option in the case statement is important, since the
+## shell code in configure will try each of these formats in the order
+## listed in this file. A plain '-MD' option would be understood by many
+## compilers, so we must ensure this comes after the gcc and icc options.
+pgcc)
+ # Portland's C compiler understands '-MD'.
+ # Will always output deps to 'file.d' where file is the root name of the
+ # source file under compilation, even if file resides in a subdirectory.
+ # The object file name does not affect the name of the '.d' file.
+ # pgcc 10.2 will output
# foo.o: sub/foo.c sub/foo.h
- # and will wrap long lines using \ :
+ # and will wrap long lines using '\' :
# foo.o: sub/foo.c ... \
# sub/foo.h ... \
# ...
+ set_dir_from "$object"
+ # Use the source, not the object, to determine the base name, since
+ # that's sadly what pgcc will do too.
+ set_base_from "$source"
+ tmpdepfile=$base.d
+
+ # For projects that build the same source file twice into different object
+ # files, the pgcc approach of using the *source* file root name can cause
+ # problems in parallel builds. Use a locking strategy to avoid stomping on
+ # the same $tmpdepfile.
+ lockdir=$base.d-lock
+ trap "
+ echo '$0: caught signal, cleaning up...' >&2
+ rmdir '$lockdir'
+ exit 1
+ " 1 2 13 15
+ numtries=100
+ i=$numtries
+ while test $i -gt 0; do
+ # mkdir is a portable test-and-set.
+ if mkdir "$lockdir" 2>/dev/null; then
+ # This process acquired the lock.
+ "$@" -MD
+ stat=$?
+ # Release the lock.
+ rmdir "$lockdir"
+ break
+ else
+ # If the lock is being held by a different process, wait
+ # until the winning process is done or we timeout.
+ while test -d "$lockdir" && test $i -gt 0; do
+ sleep 1
+ i=`expr $i - 1`
+ done
+ fi
+ i=`expr $i - 1`
+ done
+ trap - 1 2 13 15
+ if test $i -le 0; then
+ echo "$0: failed to acquire lock after $numtries attempts" >&2
+ echo "$0: check lockdir '$lockdir'" >&2
+ exit 1
+ fi
- "$@" -MD -MF "$tmpdepfile"
- stat=$?
- if test $stat -eq 0; then :
- else
+ if test $stat -ne 0; then
rm -f "$tmpdepfile"
exit $stat
fi
sed "s,^[^:]*:,$object :," < "$tmpdepfile" > "$depfile"
# Some versions of the HPUX 10.20 sed can't process this invocation
# correctly. Breaking it into two sed invocations is a workaround.
- sed 's,^[^:]*: \(.*\)$,\1,;s/^\\$//;/^$/d;/:$/d' < "$tmpdepfile" |
- sed -e 's/$/ :/' >> "$depfile"
+ sed 's,^[^:]*: \(.*\)$,\1,;s/^\\$//;/^$/d;/:$/d' < "$tmpdepfile" \
+ | sed -e 's/$/ :/' >> "$depfile"
rm -f "$tmpdepfile"
;;
+hp2)
+ # The "hp" stanza above does not work with aCC (C++) and HP's ia64
+ # compilers, which have integrated preprocessors. The correct option
+ # to use with these is +Maked; it writes dependencies to a file named
+ # 'foo.d', which lands next to the object file, wherever that
+ # happens to be.
+ # Much of this is similar to the tru64 case; see comments there.
+ set_dir_from "$object"
+ set_base_from "$object"
+ if test "$libtool" = yes; then
+ tmpdepfile1=$dir$base.d
+ tmpdepfile2=$dir.libs/$base.d
+ "$@" -Wc,+Maked
+ else
+ tmpdepfile1=$dir$base.d
+ tmpdepfile2=$dir$base.d
+ "$@" +Maked
+ fi
+ stat=$?
+ if test $stat -ne 0; then
+ rm -f "$tmpdepfile1" "$tmpdepfile2"
+ exit $stat
+ fi
+
+ for tmpdepfile in "$tmpdepfile1" "$tmpdepfile2"
+ do
+ test -f "$tmpdepfile" && break
+ done
+ if test -f "$tmpdepfile"; then
+ sed -e "s,^.*\.[$lower]*:,$object:," "$tmpdepfile" > "$depfile"
+ # Add 'dependent.h:' lines.
+ sed -ne '2,${
+ s/^ *//
+ s/ \\*$//
+ s/$/:/
+ p
+ }' "$tmpdepfile" >> "$depfile"
+ else
+ make_dummy_depfile
+ fi
+ rm -f "$tmpdepfile" "$tmpdepfile2"
+ ;;
+
tru64)
- # The Tru64 compiler uses -MD to generate dependencies as a side
- # effect. `cc -MD -o foo.o ...' puts the dependencies into `foo.o.d'.
- # At least on Alpha/Redhat 6.1, Compaq CCC V6.2-504 seems to put
- # dependencies in `foo.d' instead, so we check for that too.
- # Subdirectories are respected.
- dir=`echo "$object" | sed -e 's|/[^/]*$|/|'`
- test "x$dir" = "x$object" && dir=
- base=`echo "$object" | sed -e 's|^.*/||' -e 's/\.o$//' -e 's/\.lo$//'`
-
- if test "$libtool" = yes; then
- # With Tru64 cc, shared objects can also be used to make a
- # static library. This mecanism is used in libtool 1.4 series to
- # handle both shared and static libraries in a single compilation.
- # With libtool 1.4, dependencies were output in $dir.libs/$base.lo.d.
- #
- # With libtool 1.5 this exception was removed, and libtool now
- # generates 2 separate objects for the 2 libraries. These two
- # compilations output dependencies in in $dir.libs/$base.o.d and
- # in $dir$base.o.d. We have to check for both files, because
- # one of the two compilations can be disabled. We should prefer
- # $dir$base.o.d over $dir.libs/$base.o.d because the latter is
- # automatically cleaned when .libs/ is deleted, while ignoring
- # the former would cause a distcleancheck panic.
- tmpdepfile1=$dir.libs/$base.lo.d # libtool 1.4
- tmpdepfile2=$dir$base.o.d # libtool 1.5
- tmpdepfile3=$dir.libs/$base.o.d # libtool 1.5
- tmpdepfile4=$dir.libs/$base.d # Compaq CCC V6.2-504
- "$@" -Wc,-MD
- else
- tmpdepfile1=$dir$base.o.d
- tmpdepfile2=$dir$base.d
- tmpdepfile3=$dir$base.d
- tmpdepfile4=$dir$base.d
- "$@" -MD
- fi
-
- stat=$?
- if test $stat -eq 0; then :
- else
- rm -f "$tmpdepfile1" "$tmpdepfile2" "$tmpdepfile3" "$tmpdepfile4"
- exit $stat
- fi
-
- for tmpdepfile in "$tmpdepfile1" "$tmpdepfile2" "$tmpdepfile3" "$tmpdepfile4"
- do
- test -f "$tmpdepfile" && break
- done
- if test -f "$tmpdepfile"; then
- sed -e "s,^.*\.[a-z]*:,$object:," < "$tmpdepfile" > "$depfile"
- # That's a tab and a space in the [].
- sed -e 's,^.*\.[a-z]*:[ ]*,,' -e 's,$,:,' < "$tmpdepfile" >> "$depfile"
- else
- echo "#dummy" > "$depfile"
- fi
- rm -f "$tmpdepfile"
- ;;
+ # The Tru64 compiler uses -MD to generate dependencies as a side
+ # effect. 'cc -MD -o foo.o ...' puts the dependencies into 'foo.o.d'.
+ # At least on Alpha/Redhat 6.1, Compaq CCC V6.2-504 seems to put
+ # dependencies in 'foo.d' instead, so we check for that too.
+ # Subdirectories are respected.
+ set_dir_from "$object"
+ set_base_from "$object"
+
+ if test "$libtool" = yes; then
+ # Libtool generates 2 separate objects for the 2 libraries. These
+ # two compilations output dependencies in $dir.libs/$base.o.d and
+ # in $dir$base.o.d. We have to check for both files, because
+ # one of the two compilations can be disabled. We should prefer
+ # $dir$base.o.d over $dir.libs/$base.o.d because the latter is
+ # automatically cleaned when .libs/ is deleted, while ignoring
+ # the former would cause a distcleancheck panic.
+ tmpdepfile1=$dir$base.o.d # libtool 1.5
+ tmpdepfile2=$dir.libs/$base.o.d # Likewise.
+ tmpdepfile3=$dir.libs/$base.d # Compaq CCC V6.2-504
+ "$@" -Wc,-MD
+ else
+ tmpdepfile1=$dir$base.d
+ tmpdepfile2=$dir$base.d
+ tmpdepfile3=$dir$base.d
+ "$@" -MD
+ fi
+
+ stat=$?
+ if test $stat -ne 0; then
+ rm -f "$tmpdepfile1" "$tmpdepfile2" "$tmpdepfile3"
+ exit $stat
+ fi
+
+ for tmpdepfile in "$tmpdepfile1" "$tmpdepfile2" "$tmpdepfile3"
+ do
+ test -f "$tmpdepfile" && break
+ done
+ # Same post-processing that is required for AIX mode.
+ aix_post_process_depfile
+ ;;
+
+msvc7)
+ if test "$libtool" = yes; then
+ showIncludes=-Wc,-showIncludes
+ else
+ showIncludes=-showIncludes
+ fi
+ "$@" $showIncludes > "$tmpdepfile"
+ stat=$?
+ grep -v '^Note: including file: ' "$tmpdepfile"
+ if test $stat -ne 0; then
+ rm -f "$tmpdepfile"
+ exit $stat
+ fi
+ rm -f "$depfile"
+ echo "$object : \\" > "$depfile"
+ # The first sed program below extracts the file names and escapes
+ # backslashes for cygpath. The second sed program outputs the file
+ # name when reading, but also accumulates all include files in the
+ # hold buffer in order to output them again at the end. This only
+ # works with sed implementations that can handle large buffers.
+ sed < "$tmpdepfile" -n '
+/^Note: including file: *\(.*\)/ {
+ s//\1/
+ s/\\/\\\\/g
+ p
+}' | $cygpath_u | sort -u | sed -n '
+s/ /\\ /g
+s/\(.*\)/'"$tab"'\1 \\/p
+s/.\(.*\) \\/\1:/
+H
+$ {
+ s/.*/'"$tab"'/
+ G
+ p
+}' >> "$depfile"
+ echo >> "$depfile" # make sure the fragment doesn't end with a backslash
+ rm -f "$tmpdepfile"
+ ;;
+
+msvc7msys)
+ # This case exists only to let depend.m4 do its work. It works by
+ # looking at the text of this script. This case will never be run,
+ # since it is checked for above.
+ exit 1
+ ;;
#nosideeffect)
# This comment above is used by automake to tell side-effect
# Remove the call to Libtool.
if test "$libtool" = yes; then
- while test $1 != '--mode=compile'; do
+ while test "X$1" != 'X--mode=compile'; do
shift
done
shift
fi
- # Remove `-o $object'.
+ # Remove '-o $object'.
IFS=" "
for arg
do
done
test -z "$dashmflag" && dashmflag=-M
- # Require at least two characters before searching for `:'
+ # Require at least two characters before searching for ':'
# in the target name. This is to cope with DOS-style filenames:
- # a dependency such as `c:/foo/bar' could be seen as target `c' otherwise.
+ # a dependency such as 'c:/foo/bar' could be seen as target 'c' otherwise.
"$@" $dashmflag |
- sed 's:^[ ]*[^: ][^:][^:]*\:[ ]*:'"$object"'\: :' > "$tmpdepfile"
+ sed "s|^[$tab ]*[^:$tab ][^:][^:]*:[$tab ]*|$object: |" > "$tmpdepfile"
rm -f "$depfile"
cat < "$tmpdepfile" > "$depfile"
- tr ' ' '
-' < "$tmpdepfile" | \
-## Some versions of the HPUX 10.20 sed can't process this invocation
-## correctly. Breaking it into two sed invocations is a workaround.
- sed -e 's/^\\$//' -e '/^$/d' -e '/:$/d' | sed -e 's/$/ :/' >> "$depfile"
+ # Some versions of the HPUX 10.20 sed can't process this sed invocation
+ # correctly. Breaking it into two sed invocations is a workaround.
+ tr ' ' "$nl" < "$tmpdepfile" \
+ | sed -e 's/^\\$//' -e '/^$/d' -e '/:$/d' \
+ | sed -e 's/$/ :/' >> "$depfile"
rm -f "$tmpdepfile"
;;
"$@" || exit $?
# Remove any Libtool call
if test "$libtool" = yes; then
- while test $1 != '--mode=compile'; do
+ while test "X$1" != 'X--mode=compile'; do
shift
done
shift
fi
# X makedepend
shift
- cleared=no
- for arg in "$@"; do
+ cleared=no eat=no
+ for arg
+ do
case $cleared in
no)
set ""; shift
cleared=yes ;;
esac
+ if test $eat = yes; then
+ eat=no
+ continue
+ fi
case "$arg" in
-D*|-I*)
set fnord "$@" "$arg"; shift ;;
# Strip any option that makedepend may not understand. Remove
# the object too, otherwise makedepend will parse it as a source file.
+ -arch)
+ eat=yes ;;
-*|$object)
;;
*)
set fnord "$@" "$arg"; shift ;;
esac
done
- obj_suffix="`echo $object | sed 's/^.*\././'`"
+ obj_suffix=`echo "$object" | sed 's/^.*\././'`
touch "$tmpdepfile"
${MAKEDEPEND-makedepend} -o"$obj_suffix" -f"$tmpdepfile" "$@"
rm -f "$depfile"
- cat < "$tmpdepfile" > "$depfile"
- sed '1,2d' "$tmpdepfile" | tr ' ' '
-' | \
-## Some versions of the HPUX 10.20 sed can't process this invocation
-## correctly. Breaking it into two sed invocations is a workaround.
- sed -e 's/^\\$//' -e '/^$/d' -e '/:$/d' | sed -e 's/$/ :/' >> "$depfile"
+ # makedepend may prepend the VPATH from the source file name to the object.
+ # No need to regex-escape $object, excess matching of '.' is harmless.
+ sed "s|^.*\($object *:\)|\1|" "$tmpdepfile" > "$depfile"
+ # Some versions of the HPUX 10.20 sed can't process the last invocation
+ # correctly. Breaking it into two sed invocations is a workaround.
+ sed '1,2d' "$tmpdepfile" \
+ | tr ' ' "$nl" \
+ | sed -e 's/^\\$//' -e '/^$/d' -e '/:$/d' \
+ | sed -e 's/$/ :/' >> "$depfile"
rm -f "$tmpdepfile" "$tmpdepfile".bak
;;
# Remove the call to Libtool.
if test "$libtool" = yes; then
- while test $1 != '--mode=compile'; do
+ while test "X$1" != 'X--mode=compile'; do
shift
done
shift
fi
- # Remove `-o $object'.
+ # Remove '-o $object'.
IFS=" "
for arg
do
esac
done
- "$@" -E |
- sed -n -e '/^# [0-9][0-9]* "\([^"]*\)".*/ s:: \1 \\:p' \
- -e '/^#line [0-9][0-9]* "\([^"]*\)".*/ s:: \1 \\:p' |
- sed '$ s: \\$::' > "$tmpdepfile"
+ "$@" -E \
+ | sed -n -e '/^# [0-9][0-9]* "\([^"]*\)".*/ s:: \1 \\:p' \
+ -e '/^#line [0-9][0-9]* "\([^"]*\)".*/ s:: \1 \\:p' \
+ | sed '$ s: \\$::' > "$tmpdepfile"
rm -f "$depfile"
echo "$object : \\" > "$depfile"
cat < "$tmpdepfile" >> "$depfile"
msvisualcpp)
# Important note: in order to support this mode, a compiler *must*
- # always write the preprocessed file to stdout, regardless of -o,
- # because we must use -o when running libtool.
+ # always write the preprocessed file to stdout.
"$@" || exit $?
+
+ # Remove the call to Libtool.
+ if test "$libtool" = yes; then
+ while test "X$1" != 'X--mode=compile'; do
+ shift
+ done
+ shift
+ fi
+
IFS=" "
for arg
do
case "$arg" in
+ -o)
+ shift
+ ;;
+ $object)
+ shift
+ ;;
"-Gm"|"/Gm"|"-Gi"|"/Gi"|"-ZI"|"/ZI")
- set fnord "$@"
- shift
- shift
- ;;
+ set fnord "$@"
+ shift
+ shift
+ ;;
*)
- set fnord "$@" "$arg"
- shift
- shift
- ;;
+ set fnord "$@" "$arg"
+ shift
+ shift
+ ;;
esac
done
- "$@" -E |
- sed -n '/^#line [0-9][0-9]* "\([^"]*\)"/ s::echo "`cygpath -u \\"\1\\"`":p' | sort | uniq > "$tmpdepfile"
+ "$@" -E 2>/dev/null |
+ sed -n '/^#line [0-9][0-9]* "\([^"]*\)"/ s::\1:p' | $cygpath_u | sort -u > "$tmpdepfile"
rm -f "$depfile"
echo "$object : \\" > "$depfile"
- . "$tmpdepfile" | sed 's% %\\ %g' | sed -n '/^\(.*\)$/ s:: \1 \\:p' >> "$depfile"
- echo " " >> "$depfile"
- . "$tmpdepfile" | sed 's% %\\ %g' | sed -n '/^\(.*\)$/ s::\1\::p' >> "$depfile"
+ sed < "$tmpdepfile" -n -e 's% %\\ %g' -e '/^\(.*\)$/ s::'"$tab"'\1 \\:p' >> "$depfile"
+ echo "$tab" >> "$depfile"
+ sed < "$tmpdepfile" -n -e 's% %\\ %g' -e '/^\(.*\)$/ s::\1\::p' >> "$depfile"
rm -f "$tmpdepfile"
;;
+msvcmsys)
+ # This case exists only to let depend.m4 do its work. It works by
+ # looking at the text of this script. This case will never be run,
+ # since it is checked for above.
+ exit 1
+ ;;
+
none)
exec "$@"
;;
# eval: (add-hook 'write-file-hooks 'time-stamp)
# time-stamp-start: "scriptversion="
# time-stamp-format: "%:y-%02m-%02d.%02H"
-# time-stamp-end: "$"
+# time-stamp-time-zone: "UTC"
+# time-stamp-end: "; # UTC"
# End: