index 3c26db1f6deb312045381b6596b2793332c5444b..8ec76e8d445a7961e2177c310822702f1076c59a 100644 (file)
--- a/linux/include/_GateMP.h
+++ b/linux/include/_GateMP.h
/*!
* @brief Structure for the Handle for the GateMP.
*/
/*!
* @brief Structure for the Handle for the GateMP.
*/
-typedef struct {
+typedef struct GateMP_Object_tag {
GateMP_Params params;
/*!< Instance specific creation parameters */
GateMP_RemoteProtect remoteProtect;
GateMP_Params params;
/*!< Instance specific creation parameters */
GateMP_RemoteProtect remoteProtect;
/* Stop the GateMP module */
Int GateMP_stop(Void);
/* Stop the GateMP module */
Int GateMP_stop(Void);
+Int GateMP_attach(UInt16 procId);
+Int GateMP_detach(UInt16 procId);
+
#if defined (__cplusplus)
}
#endif /* defined (__cplusplus) */
#if defined (__cplusplus)
}
#endif /* defined (__cplusplus) */