diff --git a/linux/src/daemon/lad.c b/linux/src/daemon/lad.c
index 11dc1a79c58e64613bfd494f85bd63a57113b2cd..c18e3dc357502e2a96ddbfc1ac9d23eeb0b8511f 100644 (file)
--- a/linux/src/daemon/lad.c
+++ b/linux/src/daemon/lad.c
#include <ti/ipc/Std.h>
+#include <ctype.h>
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <sys/types.h>
#include <signal.h>
#include <unistd.h>
+#include <dirent.h>
#include <ti/ipc/MessageQ.h>
#include <_MessageQ.h>
#define DAEMON 1 /* 1 = run as a daemon; 0 = run as app */
+#define READ_BUF_SIZE 50
+
Bool logFile = FALSE;
FILE *logPtr = NULL;
struct timeval start_tv;
static FILE * responseFIFOFilePtr[LAD_MAXNUMCLIENTS];
/* local internal routines */
+static Bool isDaemonRunning(Char *pidName);
static LAD_ClientHandle assignClientId(Void);
+static Void cleanupFifos(Void);
static Void cleanupDepartedClients(Void);
static Int connectToLAD(String clientName, Int pid, String clientProto, Int *clientIdPtr);
static Void disconnectFromLAD(Int clientId);
}
}
+ if (isDaemonRunning(argv[0])) {
+ printf("Multiple instances of LAD are not supported!\n");
+ exit(EXIT_FAILURE);
+ }
+
/* change to LAD's working directory */
if ((chdir(LAD_WORKINGDIR)) < 0) {
"\nERROR: Failed to change to LAD's working directory!\n");
exit(EXIT_FAILURE);
}
+ } else {
+ cleanupFifos();
}
/* process command line args */
}
+/*
+ * ======== isDaemonRunning ========
+ */
+static Bool isDaemonRunning(Char *pidName)
+{
+ DIR *dir;
+ pid_t pid;
+ Int dirNum;
+ FILE *fp;
+ struct dirent * next;
+ Bool isRunning = FALSE;
+ Char filename [READ_BUF_SIZE];
+ Char buffer [READ_BUF_SIZE];
+ Char *bptr = buffer;
+ Char *name;
+
+ pid = getpid();
+ dir = opendir("/proc");
+ if (!dir) {
+ printf("Warning: Cannot open /proc filesystem\n");
+ return isRunning;
+ }
+
+ name = strrchr(pidName, '/');
+ if (name) {
+ pidName = (name + 1);
+ }
+
+ while ((next = readdir(dir)) != NULL) {
+ /* If it isn't a number, we don't want it */
+ if (!isdigit(*next->d_name)) {
+ continue;
+ }
+
+ dirNum = strtol(next->d_name, NULL, 10);
+ if (dirNum == pid) {
+ continue;
+ }
+
+ snprintf(filename, READ_BUF_SIZE, "/proc/%s/cmdline", next->d_name);
+ if (!(fp = fopen(filename, "r"))) {
+ continue;
+ }
+ if (fgets(buffer, READ_BUF_SIZE, fp) == NULL) {
+ fclose(fp);
+ continue;
+ }
+ fclose (fp);
+
+ name = strrchr(buffer, '/');
+ if (name && (name + 1)) {
+ bptr = name + 1;
+ }
+ else {
+ bptr = buffer;
+ }
+
+ /* Buffer should contain the entire command line */
+ if (strcmp(bptr, pidName) == 0) {
+ isRunning = TRUE;
+ break;
+ }
+ }
+ closedir (dir);
+
+ return isRunning;
+}
+
/*
* ======== assignClientId ========
*/
return(clientId);
}
+/*
+ * ======== cleanupFifos ========
+ */
+static void cleanupFifos(Void)
+{
+ DIR *dir;
+ struct dirent entry;
+ struct dirent *result;
+ size_t dirnamelen;
+ size_t maxcopy;
+ Char pathname[PATH_MAX];
+ Char *namep;
+
+ if ((dir = opendir(LAD_WORKINGDIR)) == NULL)
+ return;
+
+ dirnamelen = snprintf(pathname, sizeof(pathname), "%s/", LAD_WORKINGDIR);
+ if (dirnamelen >= sizeof(pathname)) {
+ closedir(dir);
+ return;
+ }
+ namep = pathname + dirnamelen;
+ maxcopy = PATH_MAX - dirnamelen;
+ while (readdir_r(dir, &entry, &result) == 0 && result != NULL) {
+ /* Delete old FIFOs left over */
+ if ((entry.d_type == DT_FIFO) && (strlen(entry.d_name) < maxcopy)) {
+ strncpy(namep, entry.d_name, maxcopy);
+ unlink(pathname);
+ }
+ }
+ closedir(dir);
+}
/*
* ======== cleanupDepartedClients ========
@@ -983,9 +1096,6 @@ static Int connectToLAD(String clientName, Int pid, String clientProto, Int *cli
openResponseFIFO:
- /* if response FIFO exists from previous LAD session delete it now */
- unlink(clientName);
-
/* create the dedicated response FIFO to the client */
statusIO = mkfifo(clientName, 0777);
if (statusIO != 0) {