index 8d4659f36e632e38d1f8cc4cef25ce2c229a99db..951b52e6cd5092921c9a8cc4c5900a8b2813ea19 100644 (file)
*/
Int MultiProc_setBaseIdOfCluster(UInt16 id);
-/*
- * ======== MultiProc_rprocSetId ========
- * Update processor ID mapping at run-time
- *
- * Internal use only. This function is temporary and will be
- * removed in a future build.
- *
- * When using remoteproc to load a DSP processor, the VirtIO channel
- * ID is non-deterministic. This function is part of a larger hack to
- * update the mapping from ProcID to VirtIO Channel ID each time a DSP
- * is loaded.
- */
-Int MultiProc_rprocSetId(UInt16 procId, UInt rprocId);
-
#if defined (__cplusplus)
}
#endif /* defined (__cplusplus) */