diff --git a/packages/ti/ipc/family/omap54xx/VirtQueue.c b/packages/ti/ipc/family/omap54xx/VirtQueue.c
index 6916a93e2eeea7f972233941f45730a476a4e361..8c7dd5579828192ecd00f40484a158f0d240dc27 100644 (file)
#include <xdc/runtime/Diags.h>
#include <ti/sysbios/hal/Hwi.h>
-#include <ti/sysbios/knl/Semaphore.h>
#include <ti/sysbios/knl/Clock.h>
+#include <ti/sysbios/gates/GateHwi.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/hal/Cache.h>
#define ID_A9_TO_SYSM3 ID_A9_TO_SELF
#define ID_DSP_TO_A9 ID_SELF_TO_A9
#define ID_A9_TO_DSP ID_A9_TO_SELF
-#define ID_APPM3_TO_A9 200
-#define ID_A9_TO_APPM3 201
+#define ID_APPM3_TO_A9 2
+#define ID_A9_TO_APPM3 3
typedef struct VirtQueue_Object {
/* Id for this VirtQueue_Object */
/* Will eventually be used to kick remote processor */
UInt16 procId;
+
+ /* Gate to protect from multiple threads */
+ GateHwi_Handle gateH;
} VirtQueue_Object;
static struct VirtQueue_Object *queueRegistry[NUM_QUEUES] = {NULL};
Int VirtQueue_addUsedBuf(VirtQueue_Handle vq, Int16 head, Int len)
{
struct vring_used_elem *used;
+ IArg key;
+ key = GateHwi_enter(vq->gateH);
if ((head > vq->vring.num) || (head < 0)) {
+ GateHwi_leave(vq->gateH, key);
Error_raise(NULL, Error_E_generic, 0, 0);
}
used->len = len;
vq->vring.used->idx++;
+ GateHwi_leave(vq->gateH, key);
return (0);
}
Int VirtQueue_addAvailBuf(VirtQueue_Object *vq, Void *buf)
{
UInt16 avail;
+ IArg key;
if (vq->num_free == 0) {
/* There's no more space */
vq->num_free--;
+ key = GateHwi_enter(vq->gateH);
avail = vq->vring.avail->idx++ % vq->vring.num;
vq->vring.desc[avail].addr = mapVAtoPA(buf);
vq->vring.desc[avail].len = RP_MSG_BUF_SIZE;
+ GateHwi_leave(vq->gateH, key);
return (vq->num_free);
}
{
UInt16 head;
Void *buf;
+ IArg key;
+ key = GateHwi_enter(vq->gateH);
/* There's nothing available? */
if (vq->last_used_idx == vq->vring.used->idx) {
- return (NULL);
+ buf = NULL;
}
+ else {
+ head = vq->vring.used->ring[vq->last_used_idx % vq->vring.num].id;
+ vq->last_used_idx++;
- head = vq->vring.used->ring[vq->last_used_idx % vq->vring.num].id;
- vq->last_used_idx++;
-
- buf = mapPAtoVA(vq->vring.desc[head].addr);
+ buf = mapPAtoVA(vq->vring.desc[head].addr);
+ }
+ GateHwi_leave(vq->gateH, key);
return (buf);
}
*/
Int16 VirtQueue_getAvailBuf(VirtQueue_Handle vq, Void **buf, Int *len)
{
- UInt16 head;
+ Int16 head;
+ IArg key;
+ key = GateHwi_enter(vq->gateH);
Log_print6(Diags_USER1, "getAvailBuf vq: 0x%x %d %d %d 0x%x 0x%x\n",
(IArg)vq, vq->last_avail_idx, vq->vring.avail->idx, vq->vring.num,
(IArg)&vq->vring.avail, (IArg)vq->vring.avail);
if (vq->last_avail_idx == vq->vring.avail->idx) {
/* We need to know about added buffers */
vq->vring.used->flags &= ~VRING_USED_F_NO_NOTIFY;
-
- return (-1);
+ head = (-1);
}
- /*
- * Grab the next descriptor number they're advertising, and increment
- * the index we've seen.
- */
- head = vq->vring.avail->ring[vq->last_avail_idx++ % vq->vring.num];
-
- *buf = mapPAtoVA(vq->vring.desc[head].addr);
- *len = vq->vring.desc[head].len;
+ else {
+ /*
+ * Grab the next descriptor number they're advertising, and increment
+ * the index we've seen.
+ */
+ head = vq->vring.avail->ring[vq->last_avail_idx++ % vq->vring.num];
+
+ *buf = mapPAtoVA(vq->vring.desc[head].addr);
+ *len = vq->vring.desc[head].len;
+ }
+ GateHwi_leave(vq->gateH, key);
return (head);
}
case (UInt)RP_MBOX_ABORT_REQUEST:
{
+ /* Suppress Coverity Error: FORWARD_NULL: */
+ // coverity[assign_zero]
Fxn f = (Fxn)0x0;
Log_print0(Diags_USER1, "Crash on demand ...\n");
+ // coverity[var_deref_op]
f();
}
return;
@@ -469,7 +490,15 @@ VirtQueue_Handle VirtQueue_create(UInt16 remoteProcId, VirtQueue_Params *params,
Void *vringAddr;
vq = Memory_alloc(NULL, sizeof(VirtQueue_Object), 0, eb);
- if (!vq) {
+ if (NULL == vq) {
+ return (NULL);
+ }
+
+ /* Create the thread protection gate */
+ vq->gateH = GateHwi_create(NULL, eb);
+ if (Error_check(eb)) {
+ Log_error0("VirtQueue_create: could not create gate object");
+ Memory_free(NULL, vq, sizeof(VirtQueue_Object));
return (NULL);
}
@@ -482,7 +511,7 @@ VirtQueue_Handle VirtQueue_create(UInt16 remoteProcId, VirtQueue_Params *params,
if (MultiProc_self() == appm3ProcId) {
/* vqindices that belong to AppM3 should be big so they don't
* collide with SysM3's virtqueues */
- vq->id += 200;
+ vq->id += 2;
}
#endif
@@ -506,12 +535,18 @@ VirtQueue_Handle VirtQueue_create(UInt16 remoteProcId, VirtQueue_Params *params,
vringAddr = (struct vring *) IPC_MEM_VRING3;
break;
#endif
+ default:
+ GateHwi_delete(&vq->gateH);
+ Memory_free(NULL, vq, sizeof(VirtQueue_Object));
+ return (NULL);
}
Log_print3(Diags_USER1,
"vring: %d 0x%x (0x%x)\n", vq->id, (IArg)vringAddr,
RP_MSG_RING_SIZE);
+ /* See coverity related comment in vring_init() */
+ // coverity[overrun-call]
vring_init(&(vq->vring), RP_MSG_NUM_BUFS, vringAddr, RP_MSG_VRING_ALIGN);
/*
@@ -519,7 +554,7 @@ VirtQueue_Handle VirtQueue_create(UInt16 remoteProcId, VirtQueue_Params *params,
* available
*/
if (vq->procId == hostProcId) {
- vq->vring.used->flags |= VRING_USED_F_NO_NOTIFY;
+ vq->vring.used->flags &= ~VRING_USED_F_NO_NOTIFY;
}
queueRegistry[vq->id] = vq;
InterruptProxy_intSend(0, (UInt)RP_MSG_MBOX_CRASH);
}
-/*!
- * ======== VirtQueue_postInitDone ========
- */
-Void VirtQueue_postInitDone(Void)
-{
- InterruptProxy_intSend(0, (UInt)RP_MSG_BOOTINIT_DONE);
-}
-
#define CACHE_WB_TICK_PERIOD 5
/*!