index 88d1973496ee0a59dc21a4f2a221682e56d6010a..feee339acb2eea18a3a126ca128f414d4209b516 100644 (file)
int MmRpc_use(MmRpc_Handle handle, MmRpc_BufType type, int num,
MmRpc_BufDesc *desc);
-/*!
- * @brief Get the id of an MmRpc instance
- * (currently only supported in QNX)
- *
- * @param[in] handle Service handle returned by MmRpc_create()
- *
- * @retval 32-bit id corresponding to the MmRpc instance
- *
- * @remark This returns the id corresponding to the MmRpc instance.
- * This id can be used to identify the MmRpc instance
- * on the slave core during instance deletion.
- */
-uint32_t MmRpc_getId(MmRpc_Handle handle);
-
/*!
* @brief Initialize the instance create parameter structure
*