index a89903281645b3bb5963d0224ad9ccfc7fac8658..415c2fd79cee3d79ab318cb0bc36d5018fa5129c 100644 (file)
OmapRpc_MsgType_FUNCTION_INFO = 3,
/** Ask the ServiceMgr to create a new instance of the service.
* No secondary data is needed. */
- OmapRpc_MsgType_CREATE_INSTANCE = 4,
+ OmapRpc_MsgType_CREATE_INSTANCE = 6,
/** The return message from OMAPRPC_CREATE_INSTANCE,
* contains the new endpoint address in the OmapRpc_InstanceHandle */
- OmapRpc_MsgType_INSTANCE_CREATED = 5,
+ OmapRpc_MsgType_INSTANCE_CREATED = 8,
/** Ask the Service Mgr to destroy an instance */
- OmapRpc_MsgType_DESTROY_INSTANCE = 6,
+ OmapRpc_MsgType_DESTROY_INSTANCE = 4,
/** The return message from OMAPRPC_DESTROY_INSTANCE.
* contains the old endpoint address in the OmapRpc_InstanceHandle */
OmapRpc_MsgType_INSTANCE_DESTROYED = 7,
/** Ask the Service Instance to call a particular function */
- OmapRpc_MsgType_CALL_FUNCTION = 8,
+ OmapRpc_MsgType_CALL_FUNCTION = 5,
/** The return values from a function call */
OmapRpc_MsgType_FUNCTION_RETURN = 9,
/** Returned from either the ServiceMgr or Service Instance