index c848d2ada02925e66a02cffa28f427c08d997954..499284a68787b90c3b331a3705a94025d86cc30d 100644 (file)
--- a/qnx/include/ti/ipc/Std.h
+++ b/qnx/include/ti/ipc/Std.h
typedef char Char;
typedef unsigned char UChar;
typedef char Char;
typedef unsigned char UChar;
-typedef short Short;
typedef unsigned short UShort;
typedef int Int;
typedef unsigned int UInt;
typedef long Long;
typedef unsigned long ULong;
typedef unsigned short UShort;
typedef int Int;
typedef unsigned int UInt;
typedef long Long;
typedef unsigned long ULong;
-typedef float Float;
-typedef double Double;
-typedef long double LDouble;
typedef void Void;
typedef void Void;
typedef int * IArg;
typedef unsigned int * UArg;
typedef int * IArg;
typedef unsigned int * UArg;
-typedef char Int8;
typedef short Int16;
typedef int Int32;
typedef short Int16;
typedef int Int32;
typedef unsigned short UInt16;
typedef unsigned int UInt32;
typedef unsigned int SizeT;
typedef unsigned short UInt16;
typedef unsigned int UInt32;
typedef unsigned int SizeT;
-typedef unsigned char Bits8;
typedef unsigned short Bits16;
typedef UInt32 Bits32;
typedef unsigned short Bits16;
typedef UInt32 Bits32;
-/* taken from bridge */
-typedef void *PVOID; /* p */
-typedef PVOID HANDLE; /* h */
-
#define TRUE 1
#define FALSE 0
#define FAIL -1
#define TRUE 1
#define FALSE 0
#define FAIL -1