Prevent SR0 owner from being stopped if host process is still using GateMP
[ipc/ipcdev.git] / qnx / src / ipc3x_dev / ti / syslink / inc / _GateMP_daemon.h
index bdb103aa8395ac6426e2cf6e769d2191a2f93161..87c4f11a679c3a9c07077dbfa8dceeff0261bf85 100644 (file)
@@ -53,9 +53,11 @@ extern "C" {
 Int GateMP_setup(Int32 * sr0ProcId);
 
 /*!
- * Function to destroy the GateMP module.
+ * Function to destroy the GateMP module. If forced is set
+ * we terminate the module regardless of whether there
+ * are processes that are using GateMP on the host.
  */
-Void GateMP_destroy(Void);
+Int GateMP_destroy(Bool forced);
 
 /*!
  * Find a free resource id for a particular protection type.