]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - ipc/ipcdev.git/blobdiff - qnx/src/ipc3x_dev/ti/syslink/ipc/hlos/knl/MessageQ_daemon.c
Add reserved queue support for QNX
[ipc/ipcdev.git] / qnx / src / ipc3x_dev / ti / syslink / ipc / hlos / knl / MessageQ_daemon.c
index 0d84713df66b8fd0b52956a79af849cd9fb5b3a1..e73f6bbe8ce4497ff1afdff234d290f7a8ca3e5c 100644 (file)
@@ -1,5 +1,5 @@
 /*
- * Copyright (c) 2013-2014, Texas Instruments Incorporated
+ * Copyright (c) 2013-2015, Texas Instruments Incorporated
  * All rights reserved.
  *
  * Redistribution and use in source and binary forms, with or without
  */
 #define MessageQ_NAMESERVER  "MessageQ"
 
-/* Slot 0 reserved for NameServer messages: */
-#define RESERVED_MSGQ_INDEX  1
-
 /* Define BENCHMARK to quiet key MessageQ APIs: */
 //#define BENCHMARK
 
@@ -174,7 +171,7 @@ typedef struct MessageQ_ModuleObject {
     /*!< Handle to the local NameServer used for storing GP objects */
     pthread_mutex_t     gate;
     /*!< Handle of gate to be used for local thread safety */
-    MessageQ_Config     cfg;
+    MessageQ_Config    *cfg;
     /*!< Current config values */
     MessageQ_Config     defaultCfg;
     /*!< Default config values */
@@ -198,8 +195,6 @@ typedef struct MessageQ_Object {
     /*! Instance specific creation parameters */
     MessageQ_QueueId        queue;
     /* Unique id */
-    MessageQ_QueueIndex     queueIndex;
-    /* 16-bit index into the queues array */
     Ptr                     nsKey;
     /* NameServer key */
     Int                     ownerPid;
@@ -211,6 +206,8 @@ typedef struct MessageQ_Object {
  *  Globals
  * =============================================================================
  */
+extern MessageQ_Config ti_ipc_MessageQ_cfg;
+
 static MessageQ_ModuleObject MessageQ_state =
 {
     .refCount               = 0,
@@ -219,9 +216,11 @@ static MessageQ_ModuleObject MessageQ_state =
     .numQueues              = 2u,
     .canFreeQueues          = FALSE,
     .gate                   = PTHREAD_MUTEX_INITIALIZER,
+    .cfg                    = &ti_ipc_MessageQ_cfg,
     .defaultCfg.traceFlag   = FALSE,
-    .defaultCfg.maxRuntimeEntries = 32u,
-    .defaultCfg.maxNameLen    = 32u,
+    .defaultCfg.maxRuntimeEntries  = 32u,
+    .defaultCfg.maxNameLen         = 32u,
+    .defaultCfg.numReservedEntries = 0
 };
 
 /*!
@@ -255,7 +254,7 @@ Void MessageQ_getConfig(MessageQ_Config * cfg)
         memcpy(cfg, &MessageQ_module->defaultCfg, sizeof(MessageQ_Config));
     }
     else {
-        memcpy(cfg, &MessageQ_module->cfg, sizeof(MessageQ_Config));
+        memcpy(cfg, MessageQ_module->cfg, sizeof(MessageQ_Config));
     }
 }
 
@@ -272,7 +271,8 @@ Int MessageQ_setup(const MessageQ_Config * cfg)
     MessageQ_module->refCount++;
     if (MessageQ_module->refCount > 1) {
         status = MessageQ_S_ALREADYSETUP;
-        LOG1("MessageQ module has been already setup, refCount=%d\n", MessageQ_module->refCount)
+        LOG1("MessageQ module has been already setup, refCount=%d\n",
+            MessageQ_module->refCount)
 
         goto exitSetup;
     }
@@ -280,16 +280,14 @@ Int MessageQ_setup(const MessageQ_Config * cfg)
     /* Initialize the parameters */
     NameServer_Params_init(&params);
     params.maxValueLen = sizeof(UInt32);
-    params.maxNameLen  = cfg->maxNameLen;
+    params.maxNameLen  = MessageQ_module->cfg->maxNameLen;
 
     /* Create the nameserver for modules */
     MessageQ_module->nameServer = NameServer_create(MessageQ_NAMESERVER,
                                                     &params);
 
-    memcpy(&MessageQ_module->cfg, (void *)cfg, sizeof(MessageQ_Config));
-
     MessageQ_module->seqNum = 0;
-    MessageQ_module->numQueues = cfg->maxRuntimeEntries;
+    MessageQ_module->numQueues = MessageQ_module->cfg->maxRuntimeEntries;
     MessageQ_module->queues = (MessageQ_Handle *)
         calloc(1, sizeof(MessageQ_Handle) * MessageQ_module->numQueues);
 
@@ -338,7 +336,6 @@ Int MessageQ_destroy(void)
         MessageQ_module->queues = NULL;
     }
 
-    memset(&MessageQ_module->cfg, 0, sizeof(MessageQ_Config));
     MessageQ_module->numQueues  = 0u;
     MessageQ_module->canFreeQueues = TRUE;
 
@@ -353,34 +350,68 @@ exitDestroy:
 /*
  *   Function to create a MessageQ object for receiving.
  */
-MessageQ_Handle MessageQ_createWithQueueId(String name, const MessageQ_Params * params,
-    UInt32 queueId)
+MessageQ_Handle MessageQ_create(String name, const MessageQ_Params * params)
 {
     Int                 status    = MessageQ_S_SUCCESS;
     MessageQ_Object   * obj    = NULL;
     Bool                found  = FALSE;
     UInt16              count  = 0;
     UInt16              queueIndex = 0u;
+    UInt16              queuePort;
     UInt16              procId;
     int                 i;
+    UInt                numReserved;
 
     LOG1("MessageQ_create: creating '%s'\n", name)
 
     /* Create the generic obj */
     obj = (MessageQ_Object *)calloc(1, sizeof(MessageQ_Object));
 
+    if (obj == NULL) {
+        LOG0("MessageQ_create: Error: no memory\n")
+        return (NULL);
+    }
+
+    numReserved = MessageQ_module->cfg->numReservedEntries;
+
     pthread_mutex_lock(&(MessageQ_module->gate));
 
-    count = MessageQ_module->numQueues;
+    /* check if creating a reserved queue */
+    if (params->queueIndex != MessageQ_ANY) {
+        queueIndex = params->queueIndex;
 
-    /* Search the dynamic array for any holes */
-    /* We start from 1, as 0 is reserved for binding NameServer: */
-    for (i = RESERVED_MSGQ_INDEX; i < count ; i++) {
-        if (MessageQ_module->queues [i] == NULL) {
-            MessageQ_module->queues [i] = (MessageQ_Handle)obj;
-            queueIndex = i;
-            found = TRUE;
-            break;
+        if (queueIndex > numReserved) {
+            LOG2("MessageQ_create: Error: requested queue index %d is greater "
+                    "than reserved maximum %d\n", queueIndex, numReserved - 1)
+            free(obj);
+            obj = NULL;
+        }
+        else if (MessageQ_module->queues[queueIndex] != NULL) {
+            LOG1("MessageQ_create: Error: requested queue index %d is already "
+                    "in use.\n", queueIndex);
+            free(obj);
+            obj = NULL;
+        }
+
+        if (obj == NULL) {
+            pthread_mutex_unlock(&(MessageQ_module->gate));
+            return (NULL);
+        }
+
+        MessageQ_module->queues[queueIndex] = (MessageQ_Handle)obj;
+        found = TRUE;
+    }
+    else {
+        count = MessageQ_module->numQueues;
+
+        /* Search the dynamic array for any holes */
+        for (i = numReserved; i < count ; i++) {
+            if (MessageQ_module->queues [i] == NULL) {
+                MessageQ_module->queues [i] = (MessageQ_Handle)obj;
+                queueIndex = i;
+                found = TRUE;
+                break;
+            }
         }
     }
 
@@ -397,9 +428,9 @@ MessageQ_Handle MessageQ_createWithQueueId(String name, const MessageQ_Params *
     }
 
     procId = MultiProc_self();
-    obj->queueIndex = queueIndex;
     /* create globally unique messageQ ID */
-    obj->queue = (MessageQ_QueueId)(((UInt32)procId << 16) | queueId);
+    queuePort = queueIndex + MessageQ_PORTOFFSET;
+    obj->queue = (MessageQ_QueueId)(((UInt32)procId << 16) | queuePort);
     obj->ownerPid = 0;
 
     if (name != NULL) {
@@ -412,7 +443,7 @@ MessageQ_Handle MessageQ_createWithQueueId(String name, const MessageQ_Params *
         MessageQ_delete((MessageQ_Handle *)&obj);
     }
 
-    LOG1("MessageQ_create: returning %p\n", obj)
+    LOG2("MessageQ_create: returning obj=%p, qid=0x%x\n", obj, obj->queue)
 
     return ((MessageQ_Handle)obj);
 }
@@ -426,14 +457,16 @@ Int MessageQ_delete(MessageQ_Handle * handlePtr)
     Int              status = MessageQ_S_SUCCESS;
     MessageQ_Object *obj;
     MessageQ_Handle queue;
+    UInt16          queueIndex;
 
     obj = (MessageQ_Object *)(*handlePtr);
 
     LOG1("MessageQ_delete: deleting %p\n", obj)
 
-    queue = MessageQ_module->queues[obj->queueIndex];
+    queueIndex = MessageQ_getQueueIndex(obj->queue);
+    queue = MessageQ_module->queues[queueIndex];
     if (queue != obj) {
-        LOG1("    ERROR: obj != MessageQ_module->queues[%d]\n", (MessageQ_QueueIndex)(obj->queueIndex))
+        LOG1("    ERROR: obj != MessageQ_module->queues[%d]\n", queueIndex)
     }
 
     if (obj->nsKey != NULL) {
@@ -452,7 +485,7 @@ Int MessageQ_delete(MessageQ_Handle * handlePtr)
     pthread_mutex_lock(&(MessageQ_module->gate));
 
     /* Clear the MessageQ obj from array. */
-    MessageQ_module->queues[(MessageQ_QueueIndex)obj->queueIndex] = NULL;
+    MessageQ_module->queues[queueIndex] = NULL;
 
     /* Release the local lock */
     pthread_mutex_unlock(&(MessageQ_module->gate));