Move Watchdog module configuration assignments to module$use()
authorRobert Tivy <rtivy@ti.com>
Sat, 6 Sep 2014 00:12:40 +0000 (17:12 -0700)
committerRobert Tivy <rtivy@ti.com>
Sat, 6 Sep 2014 00:12:40 +0000 (17:12 -0700)
commitce45a9737cff5aa330d6f1631dfb55dee2e10ea9
treef9a786f76a2fe1c1bf6817b4e3ae4d0d49bd9498
parent8d6fb4ba2834a41a19079960a073c927213426a7
Move Watchdog module configuration assignments to module$use()

When the ti.deh package is loaded the Watchdog module$meta$init() method
is run.  If the package is loaded by an architecture/device that is not
supported by Watchdog then module$meta$init() fails and the whole
configuration fails.  This happens even when the Watchdog module is *not*
used, such as when the ti.deh package gets loaded as a result of an
xdc.module() reference.
packages/ti/deh/Watchdog.xs