summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (from parent 1: 378db5c)
raw | patch | inline | side by side (from parent 1: 378db5c)
author | Chris Ring <cring@ti.com> | |
Tue, 16 Apr 2013 00:25:18 +0000 (17:25 -0700) | ||
committer | Chris Ring <cring@ti.com> | |
Tue, 16 Apr 2013 17:13:08 +0000 (10:13 -0700) |
This is a poor-man's cherry-pick of
1d2b0271c6d75e4a06c02875ec2841ef23467f84 and
e6c589ac8c5a15af450366c28f5bcf69d4b3d74a
from the IPC 1.25 (ipc-i) stream.
This change was tracked as SDOCM00100430 in IPC 1.x.
1d2b0271c6d75e4a06c02875ec2841ef23467f84 and
e6c589ac8c5a15af450366c28f5bcf69d4b3d74a
from the IPC 1.25 (ipc-i) stream.
This change was tracked as SDOCM00100430 in IPC 1.x.
diff --git a/packages/ti/sdo/ipc/family/f28m35x/IpcMgr.c b/packages/ti/sdo/ipc/family/f28m35x/IpcMgr.c
index e99abadabd34287d7fa9055d0e33d999457ccdd2..1256fd940b54eb4a76b4781f68c1295ed154879a 100644 (file)
NotifyDriverCirc_Params notifyDrvParams;
TransportCirc_Params transportParams;
#ifdef xdc_target__isaCompatible_v7M
- UInt32 i;
- volatile UInt32 *memcnf = (volatile UInt32 *)IpcMgr_MEMCNF;
- volatile UInt32 *msmsel = (volatile UInt32 *)IpcMgr_MSxMSEL;
- volatile UInt32 *mssrcr = (volatile UInt32 *)IpcMgr_MSxSRCR;
volatile UInt32 *set = (volatile UInt32 *)MTOCIPCSET;
volatile UInt32 *stat = (volatile UInt32 *)CTOMIPCSTS;
volatile UInt32 *ack = (volatile UInt32 *)CTOMIPCACK;
}
#ifdef xdc_target__isaCompatible_v7M
- /*
- * The M3 writes the shared memory enable and owner select
- * registers before either processor starts using shared memory.
- */
-
- /* write the shared memory configuration register */
- *memcnf = IpcMgr_sharedMemoryEnable;
-
- /* write the owner select register */
- *msmsel = IpcMgr_sharedMemoryOwnerMask;
-
- /* init the owner write access registers */
- for (i = 0; i < 2; i++) {
- mssrcr[i] = (IpcMgr_sharedMemoryAccess[(i * 4)]) |
- (IpcMgr_sharedMemoryAccess[(i * 4) + 1] << 8) |
- (IpcMgr_sharedMemoryAccess[(i * 4) + 2] << 16) |
- (IpcMgr_sharedMemoryAccess[(i * 4) + 3] << 24);
- }
#else
Void IpcMgr_init()
{
#ifdef xdc_target__isaCompatible_v7M
- volatile UInt32 *mwrallow = (volatile UInt32 *)IpcMgr_MWRALLOW;
- volatile UInt32 *mtocrTestInit = (volatile UInt32 *)IpcMgr_MTOCRTESTINIT;
- volatile UInt32 *mtocrInitDone = (volatile UInt32 *)IpcMgr_MTOCRINITDONE;
-
- /* allow writes to protected registers. */
- *mwrallow = 0xA5A5A5A5;
-
- /* init MtoCMsgRam */
- *mtocrTestInit |= 0x1;
-
- /* make sure init is done */
- while ((*mtocrInitDone & 0x1) != 0x1) {
- }
-
- /* Disable writes to protected registers. */
- *mwrallow = 0;
#else
diff --git a/packages/ti/sdo/ipc/family/f28m35x/IpcMgr.xdc b/packages/ti/sdo/ipc/family/f28m35x/IpcMgr.xdc
index 513947a3746f23e13701c7f87e75e9da15aa3788..79d575d7c785cc448b57c1a7da7c7a2d655a3d17 100644 (file)
* If any data is loaded to a shared RAM segment, the segment must
* be enabled prior to loading the program through other means.
*/
- config Bits32 sharedMemoryEnable = 0xffffffff;
+ metaonly config Bits32 sharedMemoryEnable = 0xffffffff;
/*!
* ======== sharedMemoryOwnerMask ========
* the sharedMemoryAccess bits. Setting a '1' in any bit position
* makes the C28 the owner of that shared RAM segment.
*/
- config Bits32 sharedMemoryOwnerMask = 0;
+ metaonly config Bits32 sharedMemoryOwnerMask = 0;
/*!
* ======== sharedMemoryAccess ========
* It determines the owner write access to each shared RAM segment.
* By default, the owner is allowed to fetch, DMA write, and CPU write.
*/
- config Bits32 sharedMemoryAccess[8];
+ metaonly config Bits32 sharedMemoryAccess[8];
/*!
* ======== readAddr ========
diff --git a/packages/ti/sdo/ipc/family/f28m35x/IpcMgr.xs b/packages/ti/sdo/ipc/family/f28m35x/IpcMgr.xs
index a53ab97aa0cfe946dcabb0157e248d9f52fcc14d..c1aa21fe0404562d5a10df1ec6100223f7968cad 100644 (file)
var NameServerBlock = null;
var TransportCirc = null;
var Hwi = null;
+var Boot = null;
/*
* ======== module$meta$init ========
Hwi = xdc.useModule("ti.sysbios.hal.Hwi");
Startup = xdc.useModule("xdc.runtime.Startup");
+ if (Program.build.target.name.match(/M3.*/)) {
+ Boot = xdc.useModule("ti.catalog.arm.cortexm3.concertoInit.Boot");
+ }
+
/* Init the number of messages for notify driver */
NotifyDriverCirc.numMsgs = IpcMgr.numNotifyMsgs;
"configured on the M3 core. Configuring this on the C28 core has no " +
"effect", this);
}
+
+ if ((Program.build.target.name.match(/M3.*/)) &&
+ ("sharedMemoryEnable" in Boot)) {
+ if (Boot.$written("sharedMemoryEnable") &&
+ Boot.sharedMemoryEnable != IpcMgr.sharedMemoryEnable) {
+ IpcMgr.$logWarning("Boot.sharedMemoryEnable was set to " +
+ "a value different from IpcMgr.sharedMemoryEnable. " +
+ "IpcMgr.sharedMemoryEnable will override the Boot setting.",
+ IpcMgr, "sharedMemoryEnable");
+ }
+
+ /* override Boot's sharedMemoryEnable with IpcMgr's */
+ Boot.sharedMemoryEnable = IpcMgr.sharedMemoryEnable;
+
+ if (Boot.$written("sharedMemoryOwnerMask") &&
+ Boot.sharedMemoryOwnerMask != IpcMgr.sharedMemoryOwnerMask) {
+ IpcMgr.$logWarning("Boot.sharedMemoryOwnerMask was set to " +
+ "a value different from IpcMgr.sharedMemoryOwnerMask. " +
+ "IpcMgr.sharedMemoryOwnerMask will override the Boot setting.",
+ IpcMgr, "sharedMemoryOwnerMask");
+ }
+
+ /* override Boot's sharedMemoryOwnerMask with IpcMgr's */
+ Boot.sharedMemoryOwnerMask = IpcMgr.sharedMemoryOwnerMask;
+
+ if (Boot.$written("sharedMemoryAccess")) {
+ IpcMgr.$logWarning("Boot.sharedMemoryAccess was modified " +
+ "but IpcMgr.sharedMemoryAccess will override the Boot setting.",
+ IpcMgr, "sharedMemoryAccess");
+ }
+
+ /* override Boot's sharedMemoryAccess with IpcMgr's */
+ for (var i = 0; i < IpcMgr.sharedMemoryAccess.length; i++) {
+ Boot.sharedMemoryAccess[i] = IpcMgr.sharedMemoryAccess[i];
+ }
+ }
}
/*