summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 884d1cb)
raw | patch | inline | side by side (parent: 884d1cb)
author | Chris Ring <cring@ti.com> | |
Mon, 10 Feb 2014 17:47:21 +0000 (09:47 -0800) | ||
committer | Chris Ring <cring@ti.com> | |
Mon, 10 Feb 2014 17:56:08 +0000 (09:56 -0800) |
Similar to commit 16adcaad which cleaned up OMAP5 code, this
removes dead code for DRA7XX. Most of the changes remove
untested, and likely broken, non-SMP code.
In at least one case, the code cleanup may fix previously
undiscovered issues. For example, in VirtQueue_isr(), the first
switch() block was [likely inadvertently] skipped for DSP2. There
is no known issue because of this, but now with this cleanup, DSP2
will (and should!) participate in this initial switch statement.
removes dead code for DRA7XX. Most of the changes remove
untested, and likely broken, non-SMP code.
In at least one case, the code cleanup may fix previously
undiscovered issues. For example, in VirtQueue_isr(), the first
switch() block was [likely inadvertently] skipped for DSP2. There
is no known issue because of this, but now with this cleanup, DSP2
will (and should!) participate in this initial switch statement.
packages/ti/ipc/family/vayu/VirtQueue.c | patch | blob | history |
index 4ca8f1db5fb509ece75d2775b567f6da05cb13fe..5b11e7cc6f33e10ed87cf01ee7f8205275addc99 100644 (file)
/*
/*
- * Copyright (c) 2011-2013, Texas Instruments Incorporated
+ * Copyright (c) 2011-2014, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
#include <ti/sysbios/hal/Hwi.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/gates/GateHwi.h>
#include <ti/sysbios/hal/Hwi.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/gates/GateHwi.h>
-#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/hal/Cache.h>
#include <ti/ipc/MultiProc.h>
#include <ti/sysbios/hal/Cache.h>
#include <ti/ipc/MultiProc.h>
#include "VirtQueue.h"
#include "VirtQueue.h"
+/*
+ * The following three VIRTIO_* defines must match those in
+ * <Linux_kernel>/include/uapi/linux/virtio_config.h
+ */
+#define VIRTIO_CONFIG_S_ACKNOWLEDGE 1
+#define VIRTIO_CONFIG_S_DRIVER 2
+#define VIRTIO_CONFIG_S_DRIVER_OK 4
+
+#define VRING_BUFS_PRIMED (VIRTIO_CONFIG_S_ACKNOWLEDGE | \
+ VIRTIO_CONFIG_S_DRIVER | VIRTIO_CONFIG_S_DRIVER_OK)
+
/* Used for defining the size of the virtqueue registry */
/* Used for defining the size of the virtqueue registry */
-#define NUM_QUEUES 4
+#define NUM_QUEUES 2
/* Predefined device addresses */
#ifdef DSP
#define IPC_MEM_VRING0 0xA0000000
#define IPC_MEM_VRING1 0xA0004000
/* Predefined device addresses */
#ifdef DSP
#define IPC_MEM_VRING0 0xA0000000
#define IPC_MEM_VRING1 0xA0004000
-#define IPC_MEM_VRING2 0xA0008000
-#define IPC_MEM_VRING3 0xA000c000
#else
#define IPC_MEM_VRING0 0x60000000
#define IPC_MEM_VRING1 0x60004000
#else
#define IPC_MEM_VRING0 0x60000000
#define IPC_MEM_VRING1 0x60004000
-#define IPC_MEM_VRING2 0x60008000
-#define IPC_MEM_VRING3 0x6000c000
#endif
/*
#endif
/*
- * Sizes of the virtqueues (expressed in number of buffers supported,
+ * Size of the virtqueues (expressed in number of buffers supported,
* and must be power of two)
*/
* and must be power of two)
*/
-#define VQ0_SIZE 256
-#define VQ1_SIZE 256
-#define VQ2_SIZE 256
-#define VQ3_SIZE 256
+#define VQ_SIZE 256
/*
* enum - Predefined Mailbox Messages
/*
* enum - Predefined Mailbox Messages
};
#define DIV_ROUND_UP(n,d) (((n) + (d) - 1) / (d))
};
#define DIV_ROUND_UP(n,d) (((n) + (d) - 1) / (d))
-#define RP_MSG_NUM_BUFS (VQ0_SIZE) /* must be power of two */
+#define RP_MSG_NUM_BUFS (VQ_SIZE) /* must be power of two */
#define RP_MSG_BUF_SIZE (512)
#define RP_MSG_BUFS_SPACE (RP_MSG_NUM_BUFS * RP_MSG_BUF_SIZE * 2)
#define RP_MSG_BUF_SIZE (512)
#define RP_MSG_BUFS_SPACE (RP_MSG_NUM_BUFS * RP_MSG_BUF_SIZE * 2)
/* The total IPC space needed to communicate with a remote processor */
#define RPMSG_IPC_MEM (RP_MSG_BUFS_SPACE + 2 * RP_MSG_RING_SIZE)
/* The total IPC space needed to communicate with a remote processor */
#define RPMSG_IPC_MEM (RP_MSG_BUFS_SPACE + 2 * RP_MSG_RING_SIZE)
-#define ID_SYSM3_TO_A9 ID_SELF_TO_A9
-#define ID_A9_TO_SYSM3 ID_A9_TO_SELF
-#define ID_DSP_TO_A9 ID_SELF_TO_A9
-#define ID_A9_TO_DSP ID_A9_TO_SELF
-#define ID_APPM3_TO_A9 2
-#define ID_A9_TO_APPM3 3
-
typedef struct VirtQueue_Object {
/* Id for this VirtQueue_Object */
UInt16 id;
typedef struct VirtQueue_Object {
/* Id for this VirtQueue_Object */
UInt16 id;
static struct VirtQueue_Object *queueRegistry[NUM_QUEUES] = {NULL};
static UInt16 hostProcId;
static struct VirtQueue_Object *queueRegistry[NUM_QUEUES] = {NULL};
static UInt16 hostProcId;
-#ifndef SMP
-static UInt16 dsp1ProcId;
-static UInt16 sysm3ProcId;
-static UInt16 appm3ProcId;
-#endif
#define DSPEVENTID 5
IInterrupt_IntInfo intInfo;
#define DSPEVENTID 5
IInterrupt_IntInfo intInfo;
-#if defined(M3_ONLY) && !defined(SMP)
-extern Void OffloadM3_init();
-extern Int OffloadM3_processSysM3Tasks(UArg msg);
-#endif
-
/*!
* ======== _VirtQueue_init ========
*
/*!
* ======== _VirtQueue_init ========
*
Log_print1(Diags_USER1, "VirtQueue_isr received msg = 0x%x\n", msg);
Log_print1(Diags_USER1, "VirtQueue_isr received msg = 0x%x\n", msg);
-#ifndef SMP
- if (MultiProc_self() == sysm3ProcId || MultiProc_self() == dsp1ProcId) {
-#endif
- switch(msg) {
- case (UInt)RP_MSG_MBOX_READY:
- return;
+ switch(msg) {
+ case (UInt)RP_MSG_MBOX_READY:
+ return;
- case (UInt)RP_MBOX_ECHO_REQUEST:
- InterruptProxy_intSend(hostProcId, NULL,
- (UInt)(RP_MBOX_ECHO_REPLY));
- return;
+ case (UInt)RP_MBOX_ECHO_REQUEST:
+ InterruptProxy_intSend(hostProcId, NULL, (UInt)(RP_MBOX_ECHO_REPLY));
+ return;
- case (UInt)RP_MBOX_ABORT_REQUEST:
- {
- /* Suppress Coverity Error: FORWARD_NULL: */
- /* coverity[assign_zero] */
- Fxn f = (Fxn)0x0;
- Log_print0(Diags_USER1, "Crash on demand ...\n");
- /* coverity[var_deref_op] */
- f();
- }
- return;
+ case (UInt)RP_MBOX_ABORT_REQUEST:
+ {
+ /* Suppress Coverity Error: FORWARD_NULL: */
+ /* coverity[assign_zero] */
+ Fxn f = (Fxn)0x0;
+ Log_print0(Diags_USER1, "Crash on demand ...\n");
+ /* coverity[var_deref_op] */
+ f();
+ }
+ return;
- case (UInt)RP_MSG_FLUSH_CACHE:
- Cache_wbAll();
- return;
+ case (UInt)RP_MSG_FLUSH_CACHE:
+ Cache_wbAll();
+ return;
#ifndef DSP
#ifndef DSP
- case (UInt)RP_MSG_HIBERNATION:
- if (IpcPower_canHibernate() == FALSE) {
- InterruptProxy_intSend(hostProcId, NULL,
- (UInt)RP_MSG_HIBERNATION_CANCEL);
- return;
- }
-
- /* Fall through */
- case (UInt)RP_MSG_HIBERNATION_FORCE:
-#ifndef SMP
- /* Core0 should notify Core1 */
- if (MultiProc_self() == sysm3ProcId) {
- InterruptProxy_intSend(appm3ProcId, NULL,
- (UInt)(RP_MSG_HIBERNATION));
- }
-#endif
- /* Ack request */
+ case (UInt)RP_MSG_HIBERNATION:
+ if (IpcPower_canHibernate() == FALSE) {
InterruptProxy_intSend(hostProcId, NULL,
InterruptProxy_intSend(hostProcId, NULL,
- (UInt)RP_MSG_HIBERNATION_ACK);
- IpcPower_suspend();
+ (UInt)RP_MSG_HIBERNATION_CANCEL);
return;
return;
-#endif
- default:
-#if defined(M3_ONLY) && !defined(SMP)
- /* Check and process any Inter-M3 Offload messages */
- if (OffloadM3_processSysM3Tasks(msg))
- return;
-#endif
+ }
- /*
- * If the message isn't one of the above, it's either part of the
- * 2-message synchronization sequence or it a virtqueue message
- */
- break;
- }
-#ifndef SMP
- }
- else if (msg & 0xFFFF0000) {
-#ifndef DSP
- if (msg == (UInt)RP_MSG_HIBERNATION) {
+ /* Fall through */
+ case (UInt)RP_MSG_HIBERNATION_FORCE:
+ /* Ack request */
+ InterruptProxy_intSend(hostProcId, NULL,
+ (UInt)RP_MSG_HIBERNATION_ACK);
IpcPower_suspend();
IpcPower_suspend();
- }
+ return;
#endif
#endif
- return;
+ default:
+ /*
+ * If the message isn't one of the above, it's either part of the
+ * 2-message synchronization sequence or it a virtqueue message
+ */
+ break;
}
}
- if (MultiProc_self() == sysm3ProcId && (msg == ID_A9_TO_APPM3 || msg == ID_APPM3_TO_A9)) {
- InterruptProxy_intSend(appm3ProcId, NULL, (UInt)msg);
+ /* Don't let unknown messages to pass as a virtqueue index */
+ if (msg >= NUM_QUEUES) {
+ /* Adding print here deliberately, we should never see this */
+ System_printf("VirtQueue_isr: Invalid mailbox message 0x%x "
+ "received\n", msg);
+ return;
}
}
- else {
-#endif
- /* Don't let unknown messages to pass as a virtqueue index */
- if (msg >= NUM_QUEUES) {
- /* Adding print here deliberately, we should never see this */
- System_printf("VirtQueue_isr: Invalid mailbox message 0x%x "
- "received\n", msg);
- return;
- }
- vq = queueRegistry[msg];
- if (vq) {
- vq->callback(vq);
- }
-#ifndef SMP
+ vq = queueRegistry[msg];
+ if (vq) {
+ vq->callback(vq);
}
}
-#endif
}
}
@@ -560,14 +511,6 @@ VirtQueue_Handle VirtQueue_create(UInt16 remoteProcId, VirtQueue_Params *params,
vq->procId = remoteProcId;
vq->last_avail_idx = 0;
vq->procId = remoteProcId;
vq->last_avail_idx = 0;
-#ifndef SMP
- if (MultiProc_self() == appm3ProcId) {
- /* vqindices that belong to AppM3 should be big so they don't
- * collide with SysM3's virtqueues */
- vq->id += 2;
- }
-#endif
-
switch (vq->id) {
/* IPC transport vrings */
case ID_SELF_TO_A9:
switch (vq->id) {
/* IPC transport vrings */
case ID_SELF_TO_A9:
@@ -578,16 +521,6 @@ VirtQueue_Handle VirtQueue_create(UInt16 remoteProcId, VirtQueue_Params *params,
/* A9 -> IPU/DSP */
vringAddr = (struct vring *) IPC_MEM_VRING1;
break;
/* A9 -> IPU/DSP */
vringAddr = (struct vring *) IPC_MEM_VRING1;
break;
-#ifndef SMP
- case ID_APPM3_TO_A9:
- /* APPM3 -> A9 */
- vringAddr = (struct vring *) IPC_MEM_VRING2;
- break;
- case ID_A9_TO_APPM3:
- /* A9 -> APPM3 */
- vringAddr = (struct vring *) IPC_MEM_VRING3;
- break;
-#endif
default:
GateHwi_delete(&vq->gateH);
Memory_free(NULL, vq, sizeof(VirtQueue_Object));
default:
GateHwi_delete(&vq->gateH);
Memory_free(NULL, vq, sizeof(VirtQueue_Object));
@@ -615,28 +548,12 @@ VirtQueue_Handle VirtQueue_create(UInt16 remoteProcId, VirtQueue_Params *params,
return (vq);
}
return (vq);
}
-/*
- * The following three VIRTIO_* defines must match those in
- * <Linux_kernel>/include/uapi/linux/virtio_config.h
- */
-#define VIRTIO_CONFIG_S_ACKNOWLEDGE 1
-#define VIRTIO_CONFIG_S_DRIVER 2
-#define VIRTIO_CONFIG_S_DRIVER_OK 4
-
-#define VRING_BUFS_PRIMED (VIRTIO_CONFIG_S_ACKNOWLEDGE | \
- VIRTIO_CONFIG_S_DRIVER | VIRTIO_CONFIG_S_DRIVER_OK)
-
/*!
* ======== VirtQueue_startup ========
*/
Void VirtQueue_startup()
{
hostProcId = MultiProc_getId("HOST");
/*!
* ======== VirtQueue_startup ========
*/
Void VirtQueue_startup()
{
hostProcId = MultiProc_getId("HOST");
-#ifndef SMP
- dsp1ProcId = MultiProc_getId("DSP1");
- sysm3ProcId = MultiProc_getId("CORE0");
- appm3ProcId = MultiProc_getId("CORE1");
-#endif
#ifdef DSP
intInfo.intVectorId = DSPEVENTID;
#ifdef DSP
intInfo.intVectorId = DSPEVENTID;