OMAP5: Use #define'd VRING0 addr and remove unnecessary #ifdef
authorChris Ring <cring@ti.com>
Fri, 15 Mar 2013 17:36:09 +0000 (10:36 -0700)
committerChris Ring <cring@ti.com>
Fri, 15 Mar 2013 17:36:09 +0000 (10:36 -0700)
Minor code cleanup.  There is already a #define with the VRING0 address, but
there is a block of code that's not using that #define, rather it's
hardcoding the address.  Switching to the #define'd address enables further
cleanup in mapPAtoVA().

packages/ti/ipc/family/omap54xx/VirtQueue.c

index ab0117399e720fe62a73a17577984220c74f0455..6916a93e2eeea7f972233941f45730a476a4e361 100644 (file)
@@ -211,11 +211,7 @@ extern Int OffloadM3_processSysM3Tasks(UArg msg);
 
 static inline Void * mapPAtoVA(UInt pa)
 {
-#ifndef DSPC674
-    return (Void *)((pa & 0x000fffffU) | 0xa0000000U);
-#else
-    return (Void *)((pa & 0x000fffffU) | 0x9fb00000U);
-#endif
+    return (Void *)((pa & 0x000fffffU) | IPC_MEM_VRING0);
 }
 
 static inline UInt mapVAtoPA(Void * va)