summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 00e4eb7)
raw | patch | inline | side by side (parent: 00e4eb7)
author | G Anthony <a0783926@ti.com> | |
Thu, 25 Jul 2013 23:43:45 +0000 (16:43 -0700) | ||
committer | Ramsey Harris <ramsey@ti.com> | |
Tue, 6 Aug 2013 18:02:18 +0000 (11:02 -0700) |
Previously, various methods (or none) have been implemented to ensure that
the slave has buffers available in the vring to the host before sending its
first message.
VirtQueue_startup() now polls the status bit in the VDEV struct of the Resource
table for a completion status, written by the host after the VDEV is created
successfully.
This resolves a race condition where the first slave RPMSG send would block
in a non-task context on a Semaphore_pend(), when the slave loads faster than
than the host can prime the send buffers in the vring to the host.
This patch implements the solution for Vayu separately.
Signed-off-by: G Anthony <a0783926@ti.com>
the slave has buffers available in the vring to the host before sending its
first message.
VirtQueue_startup() now polls the status bit in the VDEV struct of the Resource
table for a completion status, written by the host after the VDEV is created
successfully.
This resolves a race condition where the first slave RPMSG send would block
in a non-task context on a Semaphore_pend(), when the slave loads faster than
than the host can prime the send buffers in the vring to the host.
This patch implements the solution for Vayu separately.
Signed-off-by: G Anthony <a0783926@ti.com>
packages/ti/ipc/family/vayu/VirtQueue.c | patch | blob | history |
index 80310820508d6b8ba5a0425b6f17a22782686f74..42e9b8680afe849481b3c27760f2cb7c80545698 100644 (file)
#endif
#include <string.h>
+#include <ti/ipc/remoteproc/Resource.h>
+#include <ti/ipc/remoteproc/rsc_types.h>
#include <ti/ipc/rpmsg/_VirtQueue.h>
#include <ti/sdo/ipc/notifyDrivers/IInterrupt.h>
@@ -605,6 +607,17 @@ VirtQueue_Handle VirtQueue_create(UInt16 remoteProcId, VirtQueue_Params *params,
return (vq);
}
+/*
+ * The following three VIRTIO_* defines must match those in
+ * <Linux_kernel>/include/uapi/linux/virtio_config.h
+ */
+#define VIRTIO_CONFIG_S_ACKNOWLEDGE 1
+#define VIRTIO_CONFIG_S_DRIVER 2
+#define VIRTIO_CONFIG_S_DRIVER_OK 4
+
+#define VRING_BUFS_PRIMED (VIRTIO_CONFIG_S_ACKNOWLEDGE | \
+ VIRTIO_CONFIG_S_DRIVER | VIRTIO_CONFIG_S_DRIVER_OK)
+
/*!
* ======== VirtQueue_startup ========
*/
IpcPower_init();
#endif
+ /*
+ * Wait for HLOS (Virtio device) to indicate that priming of host's receive
+ * buffers is complete, indicating that host is ready to send.
+ *
+ * Though this is a Linux Virtio configuration status, it must be
+ * implemented by each non-Linux HLOS as well.
+ */
+ Log_print1(Diags_USER1, "VirtQueue_startup: VDEV status: 0x%x\n",
+ Resource_getVdevStatus(VIRTIO_ID_RPMSG));
+ Log_print0(Diags_USER1, "VirtQueue_startup: Polling VDEV status...\n");
+ while (Resource_getVdevStatus(VIRTIO_ID_RPMSG) != VRING_BUFS_PRIMED);
+ Log_print1(Diags_USER1, "VirtQueue_startup: VDEV status: 0x%x\n",
+ Resource_getVdevStatus(VIRTIO_ID_RPMSG));
+
InterruptProxy_intRegister(hostProcId, &intInfo, (Fxn)VirtQueue_isr, NULL);
+ Log_print0(Diags_USER1, "Passed VirtQueue_startup\n");
}
/*!