Linux: Update user AF_RPMSG define for 3.9 kernel
authorArnie Reynoso <ariner@ti.com>
Wed, 16 Oct 2013 17:11:11 +0000 (10:11 -0700)
committerRobert Tivy <rtivy@ti.com>
Fri, 15 Nov 2013 04:58:14 +0000 (20:58 -0800)
IPC's Linux user space support contains a copy of a few
kernel-defined structs and definitions.  This is necessary
because the kernel headers are not include-able by user space.
One of these values is the socket address family used for
rpmsg-based sockets - AF_RPMSG.  This definition is always
'one more' than the last address family defined by the kernel's
socket.h.

Prior to Linux 3.9, this was aways 40.  In Linux 3.9, a new
address family was introduced (AF_VSOCK), and as a result we
needed to set AF_RPMSG to 41.  To enable this, the user space
header reflects on the kernel version and appropriately assigns
the value of AF_RPMSG.

Note that in addition to adding 3.9+ support, this commit also
cleans up some dead code.

linux/include/net/rpmsg.h

index 223d6c4cc1d0407f6b79c3a07e152be20a2b30a6..3afb8350a75cca0c3a6111f34334a939b1b33dd5 100644 (file)
 
 /* user space needs this */
 #ifndef AF_RPMSG
 
 /* user space needs this */
 #ifndef AF_RPMSG
+#include <linux/version.h>
+#if LINUX_VERSION_CODE < KERNEL_VERSION(3,9,0)
 #define AF_RPMSG        40
 #define AF_RPMSG        40
-#define PF_RPMSG        AF_RPMSG
-#endif
+#else
+#define AF_RPMSG        41
+#endif /* LINUX_VERSION_CODE */
+#endif /* AF_RPMSG */
 
 /* Connection and socket states */
 enum {
 
 /* Connection and socket states */
 enum {
@@ -61,16 +65,4 @@ struct sockaddr_rpmsg {
 
 #define RPMSG_LOCALHOST ((__u32) ~0UL)
 
 
 #define RPMSG_LOCALHOST ((__u32) ~0UL)
 
-#ifdef __KERNEL__
-
-#include <net/sock.h>
-#include <linux/rpmsg.h>
-
-struct rpmsg_socket {
-        struct sock sk;
-        struct rpmsg_channel *rpdev;
-        bool unregister_rpdev;
-};
-
-#endif /* __KERNEL__ */
 #endif /* __NET_RPMSG_H */
 #endif /* __NET_RPMSG_H */