summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: fce38d1)
raw | patch | inline | side by side (parent: fce38d1)
author | Suman Anna <s-anna@ti.com> | |
Fri, 30 Oct 2015 16:37:13 +0000 (11:37 -0500) | ||
committer | Sam Nelson <sam.nelson@ti.com> | |
Wed, 4 Nov 2015 19:35:45 +0000 (14:35 -0500) |
The TCI6638/TCI6614 resource table structure definitions are
incorrect - the offset variable was defined to be an array
of 13, whereas the real valid entries are either 2 or 3,
thereby mis-representing the offsets of the resources in the
actual resource table when compared to the resource structure
definition. Fix this properly by adjusting the array length.
While at this, also remove the current TYPE_CARVEOUT entry as
well, Keystone family of SoCs do not have an MMU, so can not
really support dynamically allocated addresses for text or
data sections.
Signed-off-by: Suman Anna <s-anna@ti.com>
incorrect - the offset variable was defined to be an array
of 13, whereas the real valid entries are either 2 or 3,
thereby mis-representing the offsets of the resources in the
actual resource table when compared to the resource structure
definition. Fix this properly by adjusting the array length.
While at this, also remove the current TYPE_CARVEOUT entry as
well, Keystone family of SoCs do not have an MMU, so can not
really support dynamically allocated addresses for text or
data sections.
Signed-off-by: Suman Anna <s-anna@ti.com>
packages/ti/ipc/remoteproc/rsc_table_tci6614.h | patch | blob | history | |
packages/ti/ipc/remoteproc/rsc_table_tci6638.h | patch | blob | history |
diff --git a/packages/ti/ipc/remoteproc/rsc_table_tci6614.h b/packages/ti/ipc/remoteproc/rsc_table_tci6614.h
index 7c6a03f74b41cbf9ef70b5a373d380653e67a2b5..2d39d31d9050061be5d53c0f686cdaca9ca79d0a 100644 (file)
UInt32 version;
UInt32 num;
UInt32 reserved[2];
- UInt32 offset[13];
+ UInt32 offset[2];
/* rpmsg vdev entry */
struct fw_rsc_vdev rpmsg_vdev;
struct fw_rsc_vdev_vring rpmsg_vring0;
struct fw_rsc_vdev_vring rpmsg_vring1;
- /* data carveout entry */
- struct fw_rsc_carveout data_cout;
-
/* trace entry */
struct fw_rsc_trace trace;
};
struct resource_table ti_ipc_remoteproc_ResourceTable = {
1, /* we're the first version that implements this */
- 3, /* number of entries in the table */
+ 2, /* number of entries in the table */
0, 0, /* reserved, must be zero */
/* offsets to entries */
{
offsetof(struct resource_table, rpmsg_vdev),
- offsetof(struct resource_table, data_cout),
offsetof(struct resource_table, trace),
},
{ RPMSG_VRING0_DA, 4096, RPMSG_VQ0_SIZE, 1, 0 },
{ RPMSG_VRING1_DA, 4096, RPMSG_VQ1_SIZE, 2, 0 },
- {
- TYPE_CARVEOUT, CARVEOUTADDR, CARVEOUTADDR, CARVEOUTSIZE, 0, 0, "carveout:dsp",
- },
-
{
TYPE_TRACE, TRACEBUFADDR, TRACEBUFSIZE, 0, "trace:dsp",
},
diff --git a/packages/ti/ipc/remoteproc/rsc_table_tci6638.h b/packages/ti/ipc/remoteproc/rsc_table_tci6638.h
index 12c9b34d11c6eaf6f4436b3c99c35dbc039951a6..fecc7e2c7636274ec8a720b6d36cf1d6dc735a87 100644 (file)
struct my_resource_table {
struct resource_table base;
- UInt32 offset[13];
+#ifndef TRACE_RESOURCE_ONLY
+ UInt32 offset[2];
+#else
+ UInt32 offset[1];
+#endif
#ifndef TRACE_RESOURCE_ONLY
/* rpmsg vdev entry */
struct fw_rsc_vdev_vring rpmsg_vring0;
struct fw_rsc_vdev_vring rpmsg_vring1;
#endif
- /* data carveout entry */
- struct fw_rsc_carveout data_cout;
/* trace entry */
struct fw_rsc_trace trace;
struct my_resource_table ti_ipc_remoteproc_ResourceTable = {
1, /* we're the first version that implements this */
#ifndef TRACE_RESOURCE_ONLY
- 3, /* number of entries in the table */
+ 2, /* number of entries in the table */
#else
- 2,
+ 1,
#endif
0, 0, /* reserved, must be zero */
/* offsets to entries */
#ifndef TRACE_RESOURCE_ONLY
offsetof(struct my_resource_table, rpmsg_vdev),
#endif
- offsetof(struct my_resource_table, data_cout),
offsetof(struct my_resource_table, trace),
},
#endif
{
- TYPE_CARVEOUT, CARVEOUTADDR, CARVEOUTADDR, CARVEOUTSIZE, 0, 0, "carveout:dsp",
- },
-
- {
- TYPE_TRACE, TRACEBUFADDR, TRACEBUFSIZE, 0, "trace:dsp",
+ TYPE_TRACE, TRACEBUFADDR, TRACEBUFSIZE, 0, "trace:dsp",
},
};