Tests: Update Tests to Remove INTMEM type usage
[ipc/ipcdev.git] / packages / ti /
2016-05-18 Angela StegmaierTests: Update Tests to Remove INTMEM type usage
2016-04-27 John GodbeyShared memory cache management
2016-03-11 Angela StegmaierGateMP: Fix for hostSupport with GateMPSupportNull 3.42 ipc-3.42-next 3.42.01.03
2016-02-19 Stephen Molfettadeh: Watchdog: Timer structures declared as volatile
2016-02-18 Sam Nelsonipc: Remove warnings found with MISRA checkers
2016-02-12 Angela Stegmaiertests: gatempapp: update cmem and sr0 addresses to...
2016-02-12 Sam NelsonGateMP: Correct exception string
2016-02-12 Sam NelsonGateMP: Add check for zero resources case
2016-01-27 Sam Nelsontests: Update messageq_multicore to use ti.ipc.remotepr... 3.42.00.00_eng
2015-12-21 Angela StegmaierMmRpc: MmServiceMgr: Use Any Address for Port
2015-12-15 Angela StegmaierMerge remote-tracking branch 'origin/3.40' into ipc...
2015-12-04 Sam Nelsontci663x: Correct error in Interrupt configuration 3.41.00.06_eng
2015-12-02 Sam Nelsonbios: Update to remove reference to old ti.bios 3.41.00.05_eng
2015-12-02 John GodbeyAdded K2E and K2L ARM Alias to Settings.xs
2015-11-25 Sam NelsonInterrupt: tci663x: Update Interrupt numbers for 66AK2G 3.41.00.04_eng
2015-11-24 John GodbeyStandardize #ifdef usage in the Interrupt Module
2015-11-24 John GodbeyK2E and K2L RTOS support in IPC Settings
2015-11-17 John GodbeyMultiprocSetup ARM-RTOS check 3.41.00.03_eng
2015-11-17 John GodbeySupport for Interrupts on ARM-RTOS in the K2 family.
2015-11-16 Sam Nelsontests: Remove reference to tci6638.Interrupt module
2015-11-16 Sam NelsonMultiproc: Remove internal API MultiProc_rprocSetId
2015-11-16 Sam Nelson66AK2G: Linux: Add support for K2G
2015-11-04 Suman AnnaRemoteproc: TCI66xx: Fix up resource tables 3.41.00.02_eng
2015-10-06 Sam Nelsonipc: transport: Add TCI6638 to use _rpmsg2 library 3.41.00.01_eng
2015-10-06 Sam Nelsontci6638: rpmsg: Add define RPMSG_NS_2_0 for Keystone2...
2015-10-06 Sam Nelsontci6638: VirtQueue: Remove per core patch of the vring...
2015-10-05 Angela StegmaierEnable Examples Compilation with C++ Compiler
2015-10-05 Angela StegmaierMerge remote-tracking branch 'origin/ipc-3.40-next...
2015-10-01 Angela StegmaierTests: ping_rpmsg: Update Test with Proper Socket Usage
2015-09-29 Ramsey HarrisMove Interrupt and NotifyCircSetup modules into tci663x
2015-09-29 Ramsey HarrisFix test dual_transports to comply with MessageQApp
2015-09-17 Ramsey HarrisSDOCM00115347 Keystone 2 Interrupt module doesn't valid...
2015-09-15 Ramsey HarrisInitial Keystone 2 Galileo build support on DSP
2015-09-15 Ramsey HarrisRemove transport network interface hack
2015-09-15 Ramsey HarrisEliminate config warning raised by ti.sdo.ipcmgr
2015-09-11 Ramsey HarrisRemove references to package ti.sdo.ipc.family.f28m35x
2015-09-11 Ramsey HarrisSDOCM00077054 NameServer UG needs to document calling...
2015-09-11 Ramsey HarrisFor custom builds, add missing package dependencies
2015-09-11 Chris Ringc28: remove c28 support
2015-09-10 Ramsey HarrisSDOCM00118895 Missing access qualifier FAR in RPMessage...
2015-09-09 Ramsey HarrisSDOCM00118574 Remove interface hack from transport...
2015-09-08 Ramsey HarrisSDOCM00118895 Missing access qualifier FAR in RPMessage...
2015-09-04 Ramsey HarrisSDOCM00069628 GateMPSupportNull.getNumResources should...
2015-08-27 Ramsey HarrisSDOCM00114683 Display QueueId in ROV for reserved queues
2015-08-19 vwan@ti.comEnable PM in test_omx test executables on DRA7xx DSPs 3.40.00.05_eng 3.40.00.06 3.41.00.00_eng
2015-08-17 vwan@ti.comExport source files of ti.pm package
2015-08-17 vwan@ti.comAdd power management support to DRA7xx DSP (part 3)
2015-08-07 vwan@ti.comAdd power management support to DRA7xx DSP (part 2)
2015-08-07 Ramsey HarrisSDOCM00114069 IPC custom build does not include files...
2015-07-24 Robert TivyMerge remote-tracking branch 'origin/3.36' into ipc...
2015-07-22 Ramsey HarrisAdd log events to NameServer and NameMap
2015-07-09 Ramsey HarrisInclude RPMessage in the configuration model 3.36 ipc-3.36-next 3.36.02.13
2015-07-09 Robert TivyAdd support for device TMS320C66AK2H12
2015-07-09 Ramsey HarrisSDOCM00115097 RPMessage (Linux) has large data footprint
2015-06-30 Robert TivyPrevent %-by-0 in Assert_isTrue() expressions 3.40.00.02_eng
2015-06-26 Robert TivyAdd Power module to gatempapp.cfg
2015-06-25 vwan@ti.comAdd power management support to DRA7xx DSP
2015-06-19 Robert TivyMerge branch '3.36' into ipc-next
2015-05-20 Ramsey HarrisSDOCM00116544 Cache management for ARM speculative...
2015-05-20 Ramsey HarrisFix compiler warning when asserts are disabled
2015-05-20 Ramsey HarrisSilence unused variable warning when asserts disabled
2015-05-08 Ramsey HarrisWrap the ARM assembly statement in a check for GNU... 3.36.00.07
2015-05-08 Ramsey HarrisAdd data memory barrier to transport swi function
2015-05-08 Robert TivyGeneral cleanup in fault test
2015-05-08 Robert TivyThrow error if configured device not found in Watchdog...
2015-04-30 Robert TivyAdd Deh & Watchdog config for Vayu DSP1 and IPU1 in...
2015-04-28 Suman AnnaPower: Add the suspend hooks properly for IPUs
2015-04-28 Suman AnnaPower: Fixup idleCount for IPU running SMP
2015-04-25 Robert TivyAdd fault tolerance for TransportRpmsg socket failure
2015-04-24 Ramsey HarrisNew MultiProc API to update processor mapping
2015-04-16 Ramsey HarrisSDOCM00115768 Incorrect check for invalid pointer in...
2015-04-15 Ramsey HarrisSDOCM00115769 Ipc_attach should not call Task_setPri
2015-04-14 Robert TivyAdd capability to specify specific Watchdog timer for Deh
2015-03-27 Ramsey HarrisSDOCM00115098 New MultiProc cdoc links for "See Also... 3.36.00.03_eng
2015-03-20 Ramsey HarrisAdd Ipc attach phase to Linux implementation
2015-03-17 Ramsey HarrisCorrect the argument name in MessageQ_openQueueId
2015-03-17 Robert TivyFix doxygen comment (@Returns -> @return)
2015-03-06 Ramsey HarrisSDOCM00115110 GateMP_open crashes on Keystone 2 3.35 ipc-3.35-next 3.35.01.06_eng 3.35.01.07
2015-02-27 Robert TivyMerge branch '3.30' into ipc-next 3.35.00.05 3.36.00.00_eng
2015-02-27 vwan@ti.comAvoid changing the entry point on cores not loaded...
2015-02-27 Robert TivyFix incorrect generation of --diags option usage
2015-02-26 Ramsey HarrisAdd new IpcMgr.h header file to package release
2015-02-26 Ramsey HarrisReduced MessageQ port offset from 0x800 to 0x80
2015-02-26 Ramsey HarrisSDOCM00114985 Macro to extract destination address...
2015-02-25 Ramsey HarrisSDOCM00114354 IPC Manager needs a public header file
2015-02-25 Ramsey HarrisSDOCM00114964 Processor data array size should match...
2015-02-19 vwan@ti.comSimplify configuration of maximum name length in NameServer
2015-02-19 Ramsey HarrisSDOCM00103540 Incorrect number of hardware spin locks...
2015-02-13 Ramsey HarrisSDOCM00114730 Reserved message queues on Linux/Keystone II
2015-02-04 Ramsey HarrisFixed run-time configuration of cluster baseId 3.35.00.03_eng
2015-02-04 Ramsey HarrisNew method for run-time configuration of cluster baseId
2015-02-04 Ramsey HarrisSDOCM00114696 Add method to return address of shared...
2015-02-04 Ramsey HarrisSDOCM00114392 Interrupt module on tci6638 does not...
2015-02-03 Ramsey HarrisAdd missing transport header files to Linux install...
2015-01-29 vwan@ti.comRemove references to SysLink in QNX code base
2015-01-23 Chris Ringdocs: Remove BIOS-only comment from GateMP
2015-01-23 Robert TivyMove 'ret' declaration inside XDC %if to avoid 'unused...
2015-01-21 Ramsey HarrisAdded transport factory to remove circular dependency
2015-01-17 Ramsey HarrisSDOCM00114518 MessageQ_setMsgPri overwrites entire...
2015-01-17 Ramsey HarrisRemoved registerTransportId from MessageQ.xdc file
next