ipc/ipcdev.git
7 years agoLAD: Dead code removal
Chris Ring [Sat, 14 Dec 2013 00:53:16 +0000 (16:53 -0800)]
LAD: Dead code removal

Removed some dead code.

7 years agoRemoteproc: DRA7xx: Cleanup references to OMAP5
Suman Anna [Thu, 19 Dec 2013 01:12:26 +0000 (17:12 -0800)]
Remoteproc: DRA7xx: Cleanup references to OMAP5

OMAP5 has it own resource table files, so clean up any references
to OMAP5 from the DRA7xx resource table files.

Signed-off-by: Suman Anna <s-anna@ti.com>
7 years agoIpcMgr: Fix comment typo 3.21.00.01_eng
Chris Ring [Fri, 13 Dec 2013 20:09:44 +0000 (12:09 -0800)]
IpcMgr: Fix comment typo

No functional change - just fixed a typo.

7 years agoDRA7XX: Improve SMP detection and error messages
Chris Ring [Fri, 13 Dec 2013 19:35:48 +0000 (11:35 -0800)]
DRA7XX: Improve SMP detection and error messages

Specifically for the ti.ipc.family.vayu package, which is limited
to use on HLOS-based systems, only SMP BIOS is supported on the
IPUs.  This commit improves the package's SMP detection (in
getLibs()) and error reporting (in validate()).

7 years agoIgnore 'remote get' timeouts in NameServer_get when procId array is supplied in QNX.
vwan@ti.com [Fri, 13 Dec 2013 01:50:03 +0000 (17:50 -0800)]
Ignore 'remote get' timeouts in NameServer_get when procId array is supplied in QNX.

This patch fixes an oversight in commit 2427c7d168fb42a3e277f7d4c7827e7cdc955ac2,
where 'remote get' timeouts were ignored when procId array is NULL, but not
for the case when the procId array is supplied.

7 years agoChange NameServer_get to ignore 'remote get' timeouts in BIOS
vwan@ti.com [Fri, 13 Dec 2013 01:56:21 +0000 (17:56 -0800)]
Change NameServer_get to ignore 'remote get' timeouts in BIOS

This patch allows NameServer requests to succeed even when some of the other
remote cores are not yet ready to handle NameServer requests.

7 years agoFix wrong assertion in packages/ti/sdo/ipc/family/vayu/InterruptDsp.c
vwan@ti.com [Fri, 13 Dec 2013 01:59:22 +0000 (17:59 -0800)]
Fix wrong assertion in packages/ti/sdo/ipc/family/vayu/InterruptDsp.c

7 years agoMerge remote-tracking branch 'origin/ipc-3.20-next' into ipc-next 3.21.00.00_eng
Chris Ring [Mon, 9 Dec 2013 20:54:15 +0000 (12:54 -0800)]
Merge remote-tracking branch 'origin/ipc-3.20-next' into ipc-next

7 years agoMerge remote-tracking branch 'origin/ipc-3.10-next' into ipc-3.20-next ipc-3.20-next
Chris Ring [Mon, 9 Dec 2013 20:51:40 +0000 (12:51 -0800)]
Merge remote-tracking branch 'origin/ipc-3.10-next' into ipc-3.20-next

7 years agoMerge remote-tracking branch 'origin/3.00' into ipc-3.10-next ipc-3.10-next
Chris Ring [Mon, 9 Dec 2013 20:46:10 +0000 (12:46 -0800)]
Merge remote-tracking branch 'origin/3.00' into ipc-3.10-next

Conflicts:
linux/src/tests/Makefile.am
linux/src/tests/Makefile.in

7 years agoSDOCM00105512: Support unnamed Linux MessageQs
Chris Ring [Fri, 6 Dec 2013 00:52:42 +0000 (16:52 -0800)]
SDOCM00105512: Support unnamed Linux MessageQs

The MessageQ API supports unnamed MessageQs; update Linux's
LAD-based MessageQ creation command to handle this.

Previously a segment fault would occur due to strncpy() being
passed a NULL src string array.

7 years agoRemoves all references to OMAP4 and TI81xx devices in QNX codebase
vwan@ti.com [Sat, 23 Nov 2013 01:03:28 +0000 (17:03 -0800)]
Removes all references to OMAP4 and TI81xx devices in QNX codebase

This is to address SDOCM00101830.

Signed-off-by: VW <vwan@ti.com>
8 years agoLinux: Update autotools to require KERNEL path 3.00 ipc-3.00-next 3.00.04.29
Arnie Reynoso [Wed, 16 Oct 2013 17:14:10 +0000 (10:14 -0700)]
Linux: Update autotools to require KERNEL path

The IPC Linx-side build now requires KERNEL path to be set to
build all libraries and test applications redardless of platform.

This change is needed since rpmsg has been made Linux kernel version
aware.
(cherry picked from commit ffd46a7143ff4e25ea14085b44ff5105c9912769)

Conflicts:
linux/src/tests/Makefile.am
linux/src/tests/Makefile.in
products.mak

8 years agoLinux: Update user AF_RPMSG define for 3.9 kernel
Arnie Reynoso [Wed, 16 Oct 2013 17:11:11 +0000 (10:11 -0700)]
Linux: Update user AF_RPMSG define for 3.9 kernel

IPC's Linux user space support contains a copy of a few
kernel-defined structs and definitions.  This is necessary
because the kernel headers are not include-able by user space.
One of these values is the socket address family used for
rpmsg-based sockets - AF_RPMSG.  This definition is always
'one more' than the last address family defined by the kernel's
socket.h.

Prior to Linux 3.9, this was aways 40.  In Linux 3.9, a new
address family was introduced (AF_VSOCK), and as a result we
needed to set AF_RPMSG to 41.  To enable this, the user space
header reflects on the kernel version and appropriately assigns
the value of AF_RPMSG.

Note that in addition to adding 3.9+ support, this commit also
cleans up some dead code.

8 years agoRelease the OMAP5 DSP MMU from reset after loading the core 3.20 3.20.00.06
vwan@ti.com [Wed, 13 Nov 2013 18:16:28 +0000 (10:16 -0800)]
Release the OMAP5 DSP MMU from reset after loading the core

This patch reverts the behavior from a previous patch that moved the MMU release
to be done prior to the load. It was causing the IPC resource manager to crash when
reloading the Tesla multiple times.

Signed-off-by: VW <vwan@ti.com>
8 years agoList supported core ids for QNX IPC manager in help/use text.
vwan@ti.com [Tue, 12 Nov 2013 21:36:42 +0000 (13:36 -0800)]
List supported core ids for QNX IPC manager in help/use text.

Signed-off-by: VW <vwan@ti.com>
8 years agoSDOCM00104726 Fix RcmServer.c compile warning
Ramsey Harris [Tue, 12 Nov 2013 18:37:39 +0000 (10:37 -0800)]
SDOCM00104726 Fix RcmServer.c compile warning

The C28 is a 16-bit processor. I added a cast to promote the key
to a 32-bit value to give sufficient room for the shift operation.
This promotion was happening implicitly on 32-bit processors.

8 years agoAdd support for loading to IPU internal memory on QNX OMAP5 3.20.00.05_eng
vwan@ti.com [Fri, 8 Nov 2013 02:02:43 +0000 (18:02 -0800)]
Add support for loading to IPU internal memory on QNX OMAP5

Add static memory entry to inform loader of internal memory area on IPU.
Also remove some code that was overriding the static entries.
This addresses SDOCM00104907.

Signed-off-by: VW <vwan@ti.com>
8 years agoAdd support for loading to slaves' internal memory on QNX Vayu
vwan@ti.com [Fri, 8 Nov 2013 00:47:44 +0000 (16:47 -0800)]
Add support for loading to slaves' internal memory on QNX Vayu

Add static memory entry to inform loader of internal memory areas on DSP1 and IPU2.
This addresses SDOCM00104907.

Signed-off-by: VW <vwan@ti.com>
8 years agoSDOCM00099002 Make LibType_Debug build profile same as custom.
Ramsey Harris [Wed, 6 Nov 2013 19:56:10 +0000 (11:56 -0800)]
SDOCM00099002 Make LibType_Debug build profile same as custom.

Merged updates in ti.sysbios.Build module into ti.ipc.sdo.Build.
Turn off package library builds when building IPC for product
release. Added ti.sdo.ipc.Build.libType config param. Added source
files to Pkg.otherFiles for source only release. Added package
debug library build support. Removed package ti.sdo.utils from
ti.sdo.ipc.Build file list, it builds separately now.

8 years agoSDOCM00104913: Warnings when DRM_PREFIX not set
Arnie Reynoso [Thu, 7 Nov 2013 16:06:32 +0000 (08:06 -0800)]
SDOCM00104913: Warnings when DRM_PREFIX not set

When DRM_PREFIX isn't set, the Linux test examples issue warnings of
unsafe cross-compilation.  This is due to the Makefile setting include
paths based on a non-existent DRM_PREFIX path. The Makefile now
conditionally sets include paths when autotools config variables are
set.

8 years agoLinux: Autoconf script requires updating
Arnie Reynoso [Thu, 7 Nov 2013 16:15:23 +0000 (08:15 -0800)]
Linux: Autoconf script requires updating

The Linux Autoconf script had not been updated after previous changes
to the configure.ac file had been made.

8 years agoUse size_t cast instead of fixed-length integer cast
Robert Tivy [Mon, 4 Nov 2013 23:55:44 +0000 (15:55 -0800)]
Use size_t cast instead of fixed-length integer cast

When using fixed-length integer-based cast (unsigned int or unsigned long)
to or from a pointer type, errors/warnings are thrown from one compiler
or another, depending on the integer size vs. the pointer size.  The
size_t type adjusts based on pointer size, so it allows a clean compile.

Also had to add a cast after existing cast, creating an ugly double-cast.

Signed-off-by: Robert Tivy <rtivy@ti.com>
8 years agoRemove ducati trace thread in QNX
vwan@ti.com [Tue, 5 Nov 2013 01:21:56 +0000 (17:21 -0800)]
Remove ducati trace thread in QNX

The ducati trace thread was deemed redundant wrt. the IPC trace daemon,
and was stealing early trace when the -g option is thrown due to a longer
delay between the time when the slave is started and when the thread is
created. Hence it has been removed. This patch also adjusts the trace buffer size
in GateMPApp to match up with its resource entry. This addresses SDOCM00103794.

Signed-off-by: VW <vwan@ti.com>
8 years agoSDOCM00104689 Remove MultiProc_setBaseIdOfCluster API
Ramsey Harris [Mon, 4 Nov 2013 17:03:24 +0000 (09:03 -0800)]
SDOCM00104689 Remove MultiProc_setBaseIdOfCluster API

This API never worked and the intended behavior is not supported.

8 years agoMerge 3.10.02.13 into ipc-next 3.20.00.04_eng
Chris Ring [Fri, 1 Nov 2013 00:24:47 +0000 (17:24 -0700)]
Merge 3.10.02.13 into ipc-next

8 years agoModify MessageQApp and MessageQBench in QNX to match slave-side changes 3.10 3.10.02.13
vwan@ti.com [Wed, 30 Oct 2013 21:54:08 +0000 (14:54 -0700)]
Modify MessageQApp and MessageQBench in QNX to match slave-side changes

The tests would fail due to previous changes in the messageq_single
server in how the Message Id was being assigned and used. Updated the
QNX-side test example to reflect these changes.

Signed-off-by: VW <vwan@ti.com>
8 years agoUpdate message protocol between host and server.
Ramsey Harris [Wed, 30 Oct 2013 20:55:39 +0000 (13:55 -0700)]
Update message protocol between host and server.

The message protocol changed on the server side. Updated host
application to use the new protocol.

8 years agoTest: Modified MessageQBench due to server changes
Arnie Reynoso [Wed, 30 Oct 2013 16:58:27 +0000 (09:58 -0700)]
Test: Modified MessageQBench due to server changes

The test would fail due to previous changes in the messageq_single
server in how the Message Id was being assigned and used. Updated the
Linux-side test example to reflect these changes. Performed some code
clean-up in the process.

8 years agoPrevent MMU registers from becoming unreadable
vwan@ti.com [Mon, 21 Oct 2013 22:37:38 +0000 (15:37 -0700)]
Prevent MMU registers from becoming unreadable

This commit changes the DSP domain power state transition register
CM_DSP_CLKSTCTRL from forcing a wake-up transition on the domain (SW_WKUP),
to using automatic transitions (HW_AUTO). This prevents the MMU registers from
becoming unreadable after repeatedly pulling the MMU out of reset and putting
it back into reset.

Signed-off-by: VW <vwan@ti.com>
8 years agoQNX IPC: OMAP5 - Enable DSP-MMU Fault Recovery
Angela Stegmaier [Wed, 4 Sep 2013 21:00:45 +0000 (16:00 -0500)]
QNX IPC: OMAP5 - Enable DSP-MMU Fault Recovery

Add the DSP MMU interrupt to listen for DSP-MMU faults.
Also fix a bug where the shm_phys_addr_dsp was not being
properly reset to 0, resulting in recovery failing to
happen properly.

Signed-off-by: Angela Stegmaier <angelabaker@ti.com>
Signed-off-by: VW <vwan@ti.com>
8 years agochange 'swiPriority' to module config param
Judah Vang [Fri, 25 Oct 2013 22:14:35 +0000 (15:14 -0700)]
change 'swiPriority' to module config param

Setting 'swiPriority' had no effect because it was an instance parameter
and the swi is created internally by IpcMgr.  Change 'swiPriority' to be
a module config parameter.  This allows users to change the priority of
the swi thread which created in their configuration script.

8 years agoSDOCM00104757 Fixed VirtQueue notification race condition
Ramsey Harris [Fri, 25 Oct 2013 21:29:34 +0000 (14:29 -0700)]
SDOCM00104757 Fixed VirtQueue notification race condition

Enable notification before checking message pool. This might
result in an unnecessary notification but this is benign. Disable
notification as before (when new message has been acquired).

8 years agoSDOCM00103636: ping_rpmsg OMAP5 test broken
Chris Ring [Fri, 25 Oct 2013 19:39:54 +0000 (12:39 -0700)]
SDOCM00103636: ping_rpmsg OMAP5 test broken

The OMAP5 and DRA7XX Linux kernels require slave-side code to
use RPMSG_NS_2_0-compatible calls to NameMap_register().  When
moving to the XDC-provided ti.platforms.sdp5430 platform, the
check for which platforms need to throw -DRPMSG_NS_2_0 broke.
As a result, the ping_rpmsg test, specifically for OMAP5, was
building incorrectly.

8 years agoExamples: Added ping_tasks to talk w/ Linux app
Arnie Reynoso [Tue, 22 Oct 2013 18:50:43 +0000 (11:50 -0700)]
Examples: Added ping_tasks to talk w/ Linux app

A slave-side ping_tasks example was added that interfaces with the
Linux kernel's rpmsg_client_sample. This example demonstrates how to
leverage the Linux kernel's rpmsg driver to communicate directly to
the slave-side BIOS RPMessage interface.

8 years agoExamples: Modify BIOS ping_rpmsg with dynamic Tasks
Arnie Reynoso [Tue, 22 Oct 2013 18:35:54 +0000 (11:35 -0700)]
Examples: Modify BIOS ping_rpmsg with dynamic Tasks

The ping_rpmsg test example has be modified to create it's Task
dynamically.  This is in anticipation of upcoming examples that will
reuse the ping_rpmsg configuration on the BIOS-side(slaves).

8 years agoFix TCI6636 platform typo in comment
Chris Ring [Thu, 24 Oct 2013 20:45:15 +0000 (13:45 -0700)]
Fix TCI6636 platform typo in comment

Minor comment change to fix TCI6636 platform variable name.

8 years agoOMAP5: Fix test build of nameserverapp
Chris Ring [Mon, 21 Oct 2013 18:20:11 +0000 (11:20 -0700)]
OMAP5: Fix test build of nameserverapp

When moving scripts from ti/configs/omap5 into ti/ipc/tests,
some scripts were renamed (to avoid conflicts with ti/configs/vayu
scripts of the same name).  One of the renames was missed in
nameserverapp.cfg.

Ideally this would have been included in
3cb709f6d6ebbf62b5d2ac25c9fb9f84ab2a8a1a.  Oh, well.

8 years agoMerge tag '3.10.02.12_eng' into ipc-next 3.20.00.03_eng
Chris Ring [Mon, 21 Oct 2013 02:46:01 +0000 (19:46 -0700)]
Merge tag '3.10.02.12_eng' into ipc-next

8 years agoMask off signals before creating thread pool in QNX resource manager
vwan@ti.com [Fri, 18 Oct 2013 18:39:46 +0000 (11:39 -0700)]
Mask off signals before creating thread pool in QNX resource manager

This commit ensures that SIGTERM is caught by the main thread by masking off signal
handling in the other threads of the thread pool. This allows the IPC resource
manager to terminate correctly after MessageQ is used (SDOCM00102268).

Signed-off-by: VW <vwan@ti.com>
8 years agoModified MessageQApp and messageq_single to support > 65K messages. 3.10.02.12_eng
Ramsey Harris [Sat, 19 Oct 2013 03:06:59 +0000 (20:06 -0700)]
Modified MessageQApp and messageq_single to support > 65K messages.

The test would fail when sending more then 65K messages because the
message id was only 16 bits wide. Moved message id from header into
message payload and made it 32 bits wide. Cleaned up loop to be one
based (instead of 0-based). Turned off slave side prints.

8 years agoSDOCM00104583 RPMessage crash after 65k messages
Ramsey Harris [Thu, 17 Oct 2013 23:02:26 +0000 (16:02 -0700)]
SDOCM00104583 RPMessage crash after 65k messages

The semaphore was posted for every message added to the pool.
Added VRING_USED_F_NO_NOTIFY flag to only post semaphore when
needed. Moved clearing of flag to avoid race condition with
remote processor. Also changed the semaphore from counting
mode to binary mode.

8 years agoExamples: Move ti.configs.vayu into tests
Chris Ring [Fri, 18 Oct 2013 17:57:36 +0000 (10:57 -0700)]
Examples: Move ti.configs.vayu into tests

ti.configs.vayu was a convenience package for reusable config
snippets for IPC tests.  To reinforce this, and discourage outside
use of these snippets, this commit moves the content into the test
package and deletes the ti.configs.vayu package.

8 years agoExamples: Move ti.configs.omap54xx into tests
Chris Ring [Tue, 15 Oct 2013 18:08:50 +0000 (11:08 -0700)]
Examples: Move ti.configs.omap54xx into tests

ti.configs.omap54xx was a convenience package for reusable config
snippets for IPC tests.  To reinforce this, and discourage outside
use of these snippets, this commit moves the content into the test
package and deletes the ti.configs.omap54xx package.

8 years agoSDOCM00104194 Missing vayu package dependencies
Ramsey Harris [Tue, 15 Oct 2013 22:51:02 +0000 (15:51 -0700)]
SDOCM00104194 Missing vayu package dependencies

In close() function, bring in ISA specific module using the
program's target ISA chain. Look for oldest ISA which is
supported by device processor.

8 years agoCreate a separate BIOS configuration file for NameServerApp
vwan@ti.com [Tue, 15 Oct 2013 16:43:18 +0000 (09:43 -0700)]
Create a separate BIOS configuration file for NameServerApp

This commit decouples the configuration of NameServerApp from the MessageQ
tests. This is done because NameServerApp does not use MessageQ, and can
use a simpler configuration.

Signed-off-by: VW <vwan@ti.com>
8 years agoLinux: Update autotools to require KERNEL path
Arnie Reynoso [Wed, 16 Oct 2013 17:14:10 +0000 (10:14 -0700)]
Linux: Update autotools to require KERNEL path

The IPC Linx-side build now requires KERNEL path to be set to
build all libraries and test applications redardless of platform.

This change is needed since rpmsg has been made Linux kernel version
aware.

8 years agoLinux: Update user AF_RPMSG define for 3.9 kernel
Arnie Reynoso [Wed, 16 Oct 2013 17:11:11 +0000 (10:11 -0700)]
Linux: Update user AF_RPMSG define for 3.9 kernel

IPC's Linux user space support contains a copy of a few
kernel-defined structs and definitions.  This is necessary
because the kernel headers are not include-able by user space.
One of these values is the socket address family used for
rpmsg-based sockets - AF_RPMSG.  This definition is always
'one more' than the last address family defined by the kernel's
socket.h.

Prior to Linux 3.9, this was aways 40.  In Linux 3.9, a new
address family was introduced (AF_VSOCK), and as a result we
needed to set AF_RPMSG to 41.  To enable this, the user space
header reflects on the kernel version and appropriately assigns
the value of AF_RPMSG.

Note that in addition to adding 3.9+ support, this commit also
cleans up some dead code.

8 years agoBuild: Align products.mak variables across OS's
Chris Ring [Mon, 14 Oct 2013 22:32:58 +0000 (15:32 -0700)]
Build: Align products.mak variables across OS's

The make variable to indicate a platform is now consistent
between BIOS, QNX and Linux, and only needs to be set once.

Note that this is a compatibility break for consumers (e.g. SDKs)
which automate the consumption/build of IPC.  This is consciously
being introduced in a new Major.minor release (3.20) to keep
from breaking 3.00 and 3.10 users.

This resolves SDOCM00103415.

8 years agoRemove BIOS-side rpmsg trace for NameServerApp and MessageQ tests 3.20.00.02_eng
vwan@ti.com [Wed, 9 Oct 2013 20:23:03 +0000 (13:23 -0700)]
Remove BIOS-side rpmsg trace for NameServerApp and MessageQ tests

Signed-off-by: VW <vwan@ti.com>
8 years agoRemove static allocation of IPU_MEM_IOBUFS memory in OMAP5 QNX
vwan@ti.com [Tue, 8 Oct 2013 18:16:17 +0000 (11:16 -0700)]
Remove static allocation of IPU_MEM_IOBUFS memory in OMAP5 QNX

This commit removes unnecessary static memory allocation for
IPU_MEM_IOBUFS in the IPC resource manager on OMAP5 (SDOCM00104300)

Signed-off-by: VW <vwan@ti.com>
8 years agoGateMP: typo fixes
Chris Ring [Thu, 10 Oct 2013 15:55:46 +0000 (08:55 -0700)]
GateMP: typo fixes

Resolve a few typos in the GateMP.xdc file.  One notable
change is that an Assert message was corrected.  While this
should be merely a cosmetic change, end users experiencing the
assert will see a change in the message.

8 years agoOMAP5: Provide default Notify delegate
Chris Ring [Tue, 8 Oct 2013 15:32:20 +0000 (08:32 -0700)]
OMAP5: Provide default Notify delegate

The default Notify delegate for OMAP5 is NotifySetupNull.  This
satisfies the most common use case of the A15 running an HLOS,
and the slave cores not communicating with each other.

This addresses SDOCM00103112.

8 years agoRemoved unnecessary cast in parameter assignment. 3.20.00.01_eng
Ramsey Harris [Mon, 30 Sep 2013 22:24:45 +0000 (15:24 -0700)]
Removed unnecessary cast in parameter assignment.

8 years agoQNX IPC: RscTable - Use MAP_NOINIT Flag to Allocate Mem
Angela Stegmaier [Fri, 23 Aug 2013 16:45:21 +0000 (11:45 -0500)]
QNX IPC: RscTable - Use MAP_NOINIT Flag to Allocate Mem

The QNX IPC dynamically allocates memory for the remote
core sections based on the resource table.  These sections
are allocated using an mmap call and can be quite large.
There is a performance improvement if the allocated
memory is not zero-initialized during allocation with
mmap. It may be desireable to trade off zero-initialization
of the memory for the performance improvement, so to
enable the memory to not be zero-initialized, the MAP_NOINIT
flag is added to the flags in the mmap call.

It is important to note that the MAP_NOINIT flag will only
relax the zero-init requirement if the memory being mapped
was previously freed using UNMAP_INIT_OPTIONAL. This is
considered set for any memory that hasn't been allocated before,
so can help with boot-up time. Also, The default behavior of munmap
is to not have this flag set. However, if the "-m~i" option is
used on the procnto command line, the default behavior of
munmap is changed to act like UNMAP_INIT_OPTIONAL is set.

So, this change will only gurantee the zero-init to be relaxed if the
additional change is made to use the "-m~i" option.

To be safe, this patch also explicitly zero-initializes the
vring memory after allocation, so that even if the zero-init
requirement is relaxed, the vring memory will be zero-ed.

Also, a flag named "ZEROINIT_CHUNKS" is added in the file, and
set to 0 by default. If it is desired to restore the behavior of
zero-initialization of the chunks, this can be set to 1, and
the QNX IPC rebuilt.

Signed-off-by: Angela Stegmaier <angelabaker@ti.com>
8 years agoOMAP5: resource table dead code cleanup
Chris Ring [Mon, 30 Sep 2013 20:20:44 +0000 (13:20 -0700)]
OMAP5: resource table dead code cleanup

Removed dead "#ifdef OMAP5" code chunks from two omap5-specific
files.  These files are already OMAP5-specific, they don't support
any other devices.

8 years agoAndroid: Added build support for ping_rpmsg app 3.10.01.11
Arnie Reynoso [Wed, 2 Oct 2013 20:49:34 +0000 (13:49 -0700)]
Android: Added build support for ping_rpmsg app

8 years agoAdd headers and libs to QNX 'make install' (part 2)
vwan@ti.com [Wed, 2 Oct 2013 01:05:44 +0000 (18:05 -0700)]
Add headers and libs to QNX 'make install' (part 2)

Export MessageQ-related headers and libs for QNX.  Also clean
up exported files in general to remove headers that are not needed.

This commit adds an additional file to a previous commit that
addressed SDOCM00102141.

8 years agoMerge recent 3.00 changes into 3.10 3.10.01.10_eng
Chris Ring [Tue, 1 Oct 2013 15:21:47 +0000 (08:21 -0700)]
Merge recent 3.00 changes into 3.10

8 years agoSDOCM00104043 MessageQ_open() returns not found 3.00.03.27_eng 3.00.03.28
Ramsey Harris [Tue, 1 Oct 2013 00:09:50 +0000 (17:09 -0700)]
SDOCM00104043 MessageQ_open() returns not found

Concurrency issues in NameServerRemoteNotify caused message corruption
which resulted in keys not being found. Fixed by moving state variables
from message to object state and by splitting existing swi into two
separate ones, one for request and one for response. Updated ROV.

8 years agoFix wrong usage description of resource manager (SDOCM00103947)
vwan@ti.com [Wed, 25 Sep 2013 22:45:23 +0000 (15:45 -0700)]
Fix wrong usage description of resource manager (SDOCM00103947)

This patch updates the description that appears when calling 'use ipc'.
It also removes the command line options -f and -d that are obsolete,
and updates the error messages that comes up when wrong arguments
are passed, to guide people towards correct usage.

Signed-off-by: VW <vwan@ti.com>
8 years agoAdd defaultErrFxn and an err fxn to module state
Judah Vang [Wed, 25 Sep 2013 22:13:54 +0000 (15:13 -0700)]
Add defaultErrFxn and an err fxn to module state

Update TransportCirc_setErrFxn to set the module errFxn at runtime.
Create a default Error Fxn which does nothing for TransportCirc.
If an error fxn is not specified it will be set to the default.

8 years agoSDOCM00103043:Resolve Concerto IPC stress test failures
Judah Vang [Fri, 20 Sep 2013 19:26:48 +0000 (12:26 -0700)]
SDOCM00103043:Resolve Concerto IPC stress test failures

8 years agoSDOCM00103935:Update to work with different cluster base id
Judah Vang [Fri, 20 Sep 2013 19:24:17 +0000 (12:24 -0700)]
SDOCM00103935:Update to work with different cluster base id

8 years agoSDOCM00103934:allow Swi priority to be configurable
Judah Vang [Fri, 20 Sep 2013 19:17:47 +0000 (12:17 -0700)]
SDOCM00103934:allow Swi priority to be configurable

8 years agoAndroid: Added support for MessageQ
Arnie Reynoso [Wed, 25 Sep 2013 15:50:34 +0000 (08:50 -0700)]
Android: Added support for MessageQ

Support for MessageQ and related application(LAD) was added for Android.
Android specific build files have been created/modified to build all
user-side libraries (libmmrpc, libtiipc, libtiutils) and applications
from within the Android filesystem. This include test apps (MesssageQ*).

A few changes were also needed by the common source files that
are shared across Linux and Android builds.

8 years agoLinux: Removed circular dependencies from ipc libs
Arnie Reynoso [Wed, 25 Sep 2013 20:44:00 +0000 (13:44 -0700)]
Linux: Removed circular dependencies from ipc libs

The circular dependencies between libtiipc and libtiipcutils has
been removed by moving the assignment of the user side application's
MultiProc config structure to the libtiipcutils library via a new
function (_MultiProc_initCfg).

This also forces the creation of a LAD specific libtiipcutils library
(libtiipcutils_lad), which the daemon needs to link against.

8 years agoTest: Add autotools-generated Makefile.in
Chris Ring [Wed, 25 Sep 2013 20:40:19 +0000 (13:40 -0700)]
Test: Add autotools-generated Makefile.in

This is the second half of the Makefile.am changes in
47557586d086d61d2c361796388a61598563b413.  That commit changed
Makefile.am, this commit is the associated, generated Makefile.am.

8 years agoImplement reference counting in NameServer_create/delete (SDOCM00103730)
vwan@ti.com [Mon, 23 Sep 2013 21:57:22 +0000 (14:57 -0700)]
Implement reference counting in NameServer_create/delete (SDOCM00103730)

8 years agoAdd headers and libs to QNX 'make install'
vwan@ti.com [Tue, 24 Sep 2013 17:45:08 +0000 (10:45 -0700)]
Add headers and libs to QNX 'make install'

Export MessageQ-related headers and libs for QNX.  Also clean
up exported files in general to remove headers that are not needed.

This addresses SDOCM00102141.

8 years agoNew unit test for MessageQ delivery. 3.10.01.09_eng
Ramsey Harris [Mon, 16 Sep 2013 21:09:08 +0000 (14:09 -0700)]
New unit test for MessageQ delivery.

This test validates SDOCM00103664 MessageQ_get() can discard
msgs when a msg is available from more than one remote core.

8 years agoAndroid.mk: remove HEAPTRACK library dependency
Sunita Nadampalli [Fri, 13 Sep 2013 22:30:37 +0000 (17:30 -0500)]
Android.mk: remove HEAPTRACK library dependency

BUILD_HEAPTRACKED_SHARED_LIBRARY is a local define
in hardware/ti/omap4xxx. using this build macro inside
ipc component, unnecessarily creates build dependency with
omap4xx path. And this heaptrack feature is not required
for ipc. Hence removed the HEAPTRACK option.

Signed-off-by: Sunita Nadampalli <sunitan@ti.com>
8 years agoBuild: Enable builds without SMP support
Chris Ring [Wed, 11 Sep 2013 03:54:08 +0000 (20:54 -0700)]
Build: Enable builds without SMP support

Some customers (including the TI RTOS SDK) do not use SMP
BIOS and therefore don't require the libraries.  To improve
build times and reduce the disk size for these users, a
new variable, BIOS_SMPENABLED, was created in products.mak.
Its default value is 1 (enabled), which maintains the
behavior of previous releases.  Setting it to 0 disables
the build of SMP-enabled libraries.

Note that some platforms require SMP libraries to be built,
otherwise their test executables may fail to build.

This resolves SDOCM00103413.

8 years agoMessageQ: Fix MessageQ_get() dropping messages
Robert Tivy [Tue, 10 Sep 2013 23:01:49 +0000 (16:01 -0700)]
MessageQ: Fix MessageQ_get() dropping messages

MessageQ_get() had a bug where it would loop over all remote cores
looking for and getting a message and would return the message from
the highest numbered processor (in MultiProc order) that had one
available, tossing messages received from lower numbered processors.

The MessageQ_get() loop now terminates as soon as the first message
is found.  Further to this change, on the next call to the function
it starts looking for messages from the processor that is "next" in
the (cyclic) list after the one in which it last found a message.

Fixes SDOCM00103664.

Signed-off-by: Robert Tivy <rtivy@ti.com>
8 years agoMmRpc: updated to new Linux rpmsg_rpc.h API 3.10.00.08 3.20.00.00_eng
Ramsey Harris [Thu, 5 Sep 2013 19:51:40 +0000 (12:51 -0700)]
MmRpc: updated to new Linux rpmsg_rpc.h API

Two structures changed a field name from reserved to fd.

Also aligned the QNX copy of this header to match.

8 years agoNameServer: fix Linux-requested remote ns lookups
Chris Ring [Wed, 4 Sep 2013 22:01:14 +0000 (15:01 -0700)]
NameServer: fix Linux-requested remote ns lookups

BIOS-side NameServerRemoteRpmsg.c was recently taught to
support NameServer lookups larger than 32 bits.  Prior to
that education, it assumed all requestors were asking for
only 32 bits of NameServer data.

Linux must now indicate how big its NameServer buffer is
so the BIOS-side knows how to fill it.  When this > 32-bit
lookup support was added, QNX was correctly modified; Linux
was overlooked.

For users, this commit fixes Linux NameServer lookups (which
most users see as MessageQ_open() calls) which have been broken
since 82e4969d635d0f6cbee3c6fcc3df3a7be39bc852.  Tag-wise,
this Linux-only bug was introduced in the 3.10.00.06_eng build.

8 years agoFixed compiler warning when assigning buffer address to descriptor.
Ramsey Harris [Wed, 4 Sep 2013 18:37:07 +0000 (11:37 -0700)]
Fixed compiler warning when assigning buffer address to descriptor.

8 years agoLinux: Removed install-hook to include *.la files
Arnie Reynoso [Wed, 4 Sep 2013 17:32:59 +0000 (10:32 -0700)]
Linux: Removed install-hook to include *.la files

The Linux autotools install-hook to delete *la files as part of the
installation was removed.

8 years agoDev: Add new QNX binaries to .gitignore 3.10.00.07_eng
Chris Ring [Mon, 2 Sep 2013 03:52:34 +0000 (20:52 -0700)]
Dev: Add new QNX binaries to .gitignore

8 years agoRemoved unused IPU processor name from NotifySetup.
Ramsey Harris [Sat, 31 Aug 2013 00:23:51 +0000 (17:23 -0700)]
Removed unused IPU processor name from NotifySetup.

The IPU interrupt setup is not handled by the NotifySetup module.
In addition, the IPU references were incorrect for non-smp mode.

8 years agoBuild: Cosmetic changes to products.mak
Chris Ring [Fri, 30 Aug 2013 22:45:15 +0000 (15:45 -0700)]
Build: Cosmetic changes to products.mak

Developers added the many variables to products.mak over time.
This commit tries to address inconsistencies throughout the file,
including:
   * indication of optional variables
   * descriptions of variables
   * white space

It also moves the PLATFORM variable (used by both Linux and
BIOS) out of the Linux section and into a more common area.

8 years agoOMAP5 QNX: Changed ipc.c to avoid calling GateMP since it is not yet supported
vwan@ti.com [Fri, 30 Aug 2013 01:36:51 +0000 (18:36 -0700)]
OMAP5 QNX: Changed ipc.c to avoid calling GateMP since it is not yet supported

Signed-off-by: VW <vwan@ti.com>
8 years agoFixed make install for QNX (Vayu) to export GateMPApp
vwan@ti.com [Thu, 29 Aug 2013 23:46:44 +0000 (16:46 -0700)]
Fixed make install for QNX (Vayu) to export GateMPApp

Signed-off-by: VW <vwan@ti.com>
8 years agoAdded MmRpc_use()/MmRpc_release() API functions.
Ramsey Harris [Fri, 30 Aug 2013 00:31:43 +0000 (17:31 -0700)]
Added MmRpc_use()/MmRpc_release() API functions.

These functions call into the driver to make the buffers
persistent from the remote processor view. This allows the
remote processor to maintain persistent references to the
buffers across multiple calls to MmRcp_call().

8 years agoQNX IPC: rpmsg_rpc - Don't Use Primary Offset in Translations
Angela Stegmaier [Wed, 28 Aug 2013 22:49:41 +0000 (17:49 -0500)]
QNX IPC: rpmsg_rpc - Don't Use Primary Offset in Translations

The primary offset for the params is not needed in the
translations. The translation code was incorrectly subtracting
the primary offset when calculating the location of the pointer
to be translated. The translation offset is the offset from the
start of the params data pointer, and not the offset from the
start of the params base. So, the params data pointer plus the
translation offset is all that is needed in order to get the
location of the translation.

Also, fix the reverse translations so that the correct
value is put back in the buffer.

Signed-off-by: Angela Stegmaier <angelabaker@ti.com>
8 years agoAdd base field to MmRpc_Xlt structure. 3.10.00.06_eng
Ramsey Harris [Wed, 28 Aug 2013 22:06:36 +0000 (15:06 -0700)]
Add base field to MmRpc_Xlt structure.

Fixed the offset calculation for embedded pointers by allowing
the caller to specify encoded base value. Enhanced some comments.
Code cleanup.

8 years agoChanges to support non-NameServer-capable slaves on Linux
Robert Tivy [Tue, 27 Aug 2013 23:19:16 +0000 (16:19 -0700)]
Changes to support non-NameServer-capable slaves on Linux

Ipc setup code was giving up when any slave failed to connect to Linux
sockets.  It now succeeds when at least one slave connects.  Previously,
both NameServer_setup() (in LAD) and MessageQ_attach()es called from
Ipc_start() were expected to succeed for all remote cores specified in
MultiProc.  Now those functions can tolerate slave connection failures and
will report success if at least one slave can connect.

8 years agoChange NameServer_get to ignore 'remote get' timeouts and use a reduced period.
vwan@ti.com [Wed, 28 Aug 2013 18:30:44 +0000 (11:30 -0700)]
Change NameServer_get to ignore 'remote get' timeouts and use a reduced period.

This is to fix SDOCM00102548 for QNX, so that MessageQ_open succeeds when
the IPU is loaded with an executable that does not 'speak' NameServer.

Signed-off-by: VW <vwan@ti.com>
8 years agoAdded GateMPApp test for GateMP verification
vwan@ti.com [Mon, 26 Aug 2013 21:21:47 +0000 (14:21 -0700)]
Added GateMPApp test for GateMP verification

Signed-off-by: VW <vwan@ti.com>
8 years agoGateMP: Introduce support for GateMP on QNX
vwan@ti.com [Tue, 27 Aug 2013 16:48:45 +0000 (09:48 -0700)]
GateMP: Introduce support for GateMP on QNX

To enable GateMP,throw the -g option when launching the IPC resource
manager.

On the BIOS side, DSP1 must be configured as the owner of SR0 and
the new GateMP.hostSupport config param must be set to true like
this:

     var GateMP = xdc.useModule('ti.sdo.ipc.GateMP');
     GateMP.hostSupport = true;

Note that it's initially only been validated on DRA7XX DSP1.

Signed-off-by: VW <vwan@ti.com>
8 years agoMmRpc: Added support for Android OS build
Sunita Nadampalli [Tue, 27 Aug 2013 17:04:30 +0000 (12:04 -0500)]
MmRpc: Added support for Android OS build

Introduce an initial Android.mk build script, and slight
code change to build the MmRpc library.

Signed-off-by: Sunita Nadampalli <sunitan@ti.com>
8 years agoMessageQ: Fix for Linux msgs sent to wrong slave 3.10.00.05_eng
Chris Ring [Sat, 24 Aug 2013 14:57:24 +0000 (07:57 -0700)]
MessageQ: Fix for Linux msgs sent to wrong slave

Previously the MultiProc-to-Linux-kernel-rproc-index mapping was
hard-coded in the MessageQ-based socket library to be
rprocIndex = MultiProc_id - 1.  This was too simple for the async
loading use cases on systems with > 1 slave.

A recent kernel patch looks up the rpmsg channel based on Linux
kernel rproc index, meaning the socket's 'connect' and 'bind'
calls now need to provide the actual rproc index.  Today's Linux
kernels ensure the rproc index will be consistent from run to run
(so long as all slaves are configured enabled), so this rproc-
index-to-MultiProc-id can be known and hard-coded ahead of time.

This commit records that hard-coding in the MultiProcCfg_*.c
source files, and now provides the appropriate rproc index in
the socket 'connect' and 'bind' calls.

This user-space commit requires a matching update to the kernel
space drivers.

8 years agoLinux: Remove KERNEL and DRM requirement
Arnie Reynoso [Thu, 22 Aug 2013 22:05:27 +0000 (15:05 -0700)]
Linux: Remove KERNEL and DRM requirement

Remove the KERNEL and DRM dependency for OMAP54xx and
DRA7xx builds.  We'll build as many libs/tests as possible,
given the provided dependencies.

If the user doesn't supply KERNEL, we won't build the MmRpc
libs; if they don't supply DRM, we won't build tests that
depend on DRM... but we'll still build, for example,
MessageQ libs and tests.

8 years agoMessageQ: Merge new IPC 1.25.03 MessageQ features
Chris Ring [Tue, 20 Aug 2013 18:59:03 +0000 (11:59 -0700)]
MessageQ: Merge new IPC 1.25.03 MessageQ features

The IPC 1.25.03 patch introduced two MessageQ-related features:

SDOCM00099783: MessageQ_free needs a hook function
SDOCM00095724: MessageQ_create should allow a queueId to be
specified instaned of finding free slot

These were driven by MCU/TI-RTOS programs, but may be useful for
other use cases.

This commit brings those features into IPC 3.x.

8 years agoTests: mmrpc_test: Fix unitialized status variable in mmrpc_test.c
G Anthony [Wed, 14 Aug 2013 22:25:06 +0000 (15:25 -0700)]
Tests: mmrpc_test: Fix unitialized status variable in mmrpc_test.c

This was causing the mmrpc_test to report failure, when in fact it succeeded.

Signed-off-by: G Anthony <a0783926@ti.com>
8 years agoTests: mmrpc_test: Removed omapconf comment and getchar from mmrpc_test.
G Anthony [Wed, 14 Aug 2013 22:31:54 +0000 (15:31 -0700)]
Tests: mmrpc_test: Removed omapconf comment and getchar from mmrpc_test.

This was previously inserted for debugging purposes.

Signed-off-by: G Anthony <a0783926@ti.com>
8 years agoTests: rpc_task: Invalidate the compute structure in Mx_compute fxn.
G Anthony [Wed, 14 Aug 2013 16:41:46 +0000 (09:41 -0700)]
Tests: rpc_task: Invalidate the compute structure in Mx_compute fxn.

This to ensure the cache is invalidated before reading the fields of this
structure, which may be in cached memory (Tiler).

Signed-off-by: G Anthony <a0783926@ti.com>
8 years agoBuild CMEM library only if platform is specified. 3.10.00.04_eng
Ramsey Harris [Thu, 8 Aug 2013 16:41:50 +0000 (09:41 -0700)]
Build CMEM library only if platform is specified.

CMEM library is platform specific. You just specify a platform
to build the library and programs that use CMEM.

8 years agoAdded offset pointer support to MmRcp.
Ramsey Harris [Thu, 8 Aug 2013 01:26:51 +0000 (18:26 -0700)]
Added offset pointer support to MmRcp.

New parameter type to support data pointers into managed memory
allocations such that the data pointer is offset from the base
address.

8 years agoMoved drm libraries out of common variable.
Ramsey Harris [Wed, 7 Aug 2013 22:27:55 +0000 (15:27 -0700)]
Moved drm libraries out of common variable.