Code cleanup to remove unused VirtQueue functions on QNX
Signed-off-by: VW <vwan@ti.com>
Signed-off-by: VW <vwan@ti.com>
Update MessageQMulti test to support up to 55 threads
Signed-off-by: VW <vwan@ti.com>
Signed-off-by: VW <vwan@ti.com>
Add INTMEM resource type support in QNX
This commit adds support for the new INTMEM resource type (SDOCM00107479).
For this resource type, we map the entry only for the loader on the host,
without mapping it to the slave MMU.
This commit also removes support of the hard-coded static entries defined
in the address translation table, which was originally there to ensure
slave internal memories are always mapped. To match up with the Linux
implementation we'll now rely on the INTMEM resource type instead.
Note that this does break compatibility with slave executables that were
previously built without the INTMEM resource entries but were relying
on the hard-coded internal memory definitions in the ipc resource manager.
Signed-off-by: VW <vwan@ti.com>
This commit adds support for the new INTMEM resource type (SDOCM00107479).
For this resource type, we map the entry only for the loader on the host,
without mapping it to the slave MMU.
This commit also removes support of the hard-coded static entries defined
in the address translation table, which was originally there to ensure
slave internal memories are always mapped. To match up with the Linux
implementation we'll now rely on the INTMEM resource type instead.
Note that this does break compatibility with slave executables that were
previously built without the INTMEM resource entries but were relying
on the hard-coded internal memory definitions in the ipc resource manager.
Signed-off-by: VW <vwan@ti.com>
Add subtest into rpmsg-rpc-stress test to trigger program-access MMU fault
This commit enhances the rpmsg-rpc-stress test to allow it to trigger MMU
fault via instruction fetch.
Signed-off-by: VW <vwan@ti.com>
This commit enhances the rpmsg-rpc-stress test to allow it to trigger MMU
fault via instruction fetch.
Signed-off-by: VW <vwan@ti.com>
Linux/Android: Option to set LAD working dir permissions
Added an optional flag (-p) to LAD, to allow users to set the permissions
of LAD's working directory at launch.
This is critical, if applications using IPC stack (MessageQ) are executed
in user-space while LAD is started as root. Without proper directory
permissions the user application will be unable to talk to the LAD daemon.
Added an optional flag (-p) to LAD, to allow users to set the permissions
of LAD's working directory at launch.
This is critical, if applications using IPC stack (MessageQ) are executed
in user-space while LAD is started as root. Without proper directory
permissions the user application will be unable to talk to the LAD daemon.
Add Deh/Watchdog support for OMAP5 & DRA7XX remote cores
The ti/deh package supports DSPs and IPUs, although the DSP support
needs some further work (Exception "dump" from SYS/BIOS when watchdog
fires is not valid, all zeroes for now).
The ti/ipc/tests have Deh/Watchdog enabled for IPU on OMAP5 and IPU2
on DRA7XX.
The new content contained herein originally came from:
http://git.omapzoom.org/?p=repo/sysbios-rpmsg.git;a=summary
The repo HEAD at the time of copying was:
commit 18c2b758f0674ee0baf95603248c6303afd9c854
This repo supported Deh/Watchdog for OMAP4/5.
The ti/deh package supports DSPs and IPUs, although the DSP support
needs some further work (Exception "dump" from SYS/BIOS when watchdog
fires is not valid, all zeroes for now).
The ti/ipc/tests have Deh/Watchdog enabled for IPU on OMAP5 and IPU2
on DRA7XX.
The new content contained herein originally came from:
http://git.omapzoom.org/?p=repo/sysbios-rpmsg.git;a=summary
The repo HEAD at the time of copying was:
commit 18c2b758f0674ee0baf95603248c6303afd9c854
This repo supported Deh/Watchdog for OMAP4/5.
NotifySetup_plugHwi() - initialize restore ier mask
On ARP32, when plugging a Hwi, specify the restore ier mask. This is
needed because we use a custom bit mask for the disable ier mask.
On ARP32, when plugging a Hwi, specify the restore ier mask. This is
needed because we use a custom bit mask for the disable ier mask.
Fixed minor typo in comment.
Fix MessageQ to support more than 52 instances in QNX
This fix changes MessageQ to obtain a port number assignment from MessageQCopy
and use it as local queue id as opposed to having MessageQ manage the ids
itself. This ensures the port number to be above 1024, so that it does not
collide with any reserved port such as the one for the Name Service.
This addresses CQ SDOCM00104834.
Signed-off-by: VW <vwan@ti.com>
This fix changes MessageQ to obtain a port number assignment from MessageQCopy
and use it as local queue id as opposed to having MessageQ manage the ids
itself. This ensures the port number to be above 1024, so that it does not
collide with any reserved port such as the one for the Name Service.
This addresses CQ SDOCM00104834.
Signed-off-by: VW <vwan@ti.com>
DRA7XX: Remove hard-coded vring addrs
Replace hard-coded vring addrs with runtime addrs read from
the resource table. This reduces the number of things to change
if the memory map moves around.
Replace hard-coded vring addrs with runtime addrs read from
the resource table. This reduces the number of things to change
if the memory map moves around.
BIOS: Remove dead DRA7XX VirtQueue code
Because BIOS-side virtqueue-based processors never run as the 'host',
half of the protocol is unused. This commit removes that dead code
for the BIOS-side DRA7XX VirtQueue driver.
Because BIOS-side virtqueue-based processors never run as the 'host',
half of the protocol is unused. This commit removes that dead code
for the BIOS-side DRA7XX VirtQueue driver.
OMAP5: Remove hard-coded vring addrs
Replace hard-coded vring addrs with runtime addrs read from
the resource table. This reduces the number of things to change
if the memory map moves around.
Replace hard-coded vring addrs with runtime addrs read from
the resource table. This reduces the number of things to change
if the memory map moves around.
BIOS: Remove dead OMAP5 VirtQueue code
Because BIOS-side virtqueue-based processors never run as the 'host',
half of the protocol is unused. This commit removes that dead code
for the BIOS-side OMAP5 VirtQueue driver.
Because BIOS-side virtqueue-based processors never run as the 'host',
half of the protocol is unused. This commit removes that dead code
for the BIOS-side OMAP5 VirtQueue driver.
Update resource table with physical device address of vrings in QNX
The physical device address of vrings needs to be updated in the
resource table in QNX, after memory has been allocated for these
vrings. This is so that Resource_getVringDA() on the slave side
can return the correct physical device address.
Signed-off-by: VW <vwan@ti.com>
The physical device address of vrings needs to be updated in the
resource table in QNX, after memory has been allocated for these
vrings. This is so that Resource_getVringDA() on the slave side
can return the correct physical device address.
Signed-off-by: VW <vwan@ti.com>
Linux: Use DESTDIR as configure --prefix option
If the user sets DESTDIR (e.g. in products.mak), pass that value
via the --prefix= option to ./configure.
Also relocate the DESTDIR variable definition in products.mak to
reflect it's used outside of QNX.
If the user sets DESTDIR (e.g. in products.mak), pass that value
via the --prefix= option to ./configure.
Also relocate the DESTDIR variable definition in products.mak to
reflect it's used outside of QNX.
Create Keystone platform instances with no external DDR defined
On MAR-based cores (i.e., C6x), SYS/BIOS will, by default, set the
"cacheable" bit for any external memory that it "sees", i.e., any
external memory that is defined for the platform. This happens regardless
of whether or not that memory is used for program placement. This
cacheable-ness is somewhat hidden to the programmer.
In order to offer better control of this, Keystone platform instances are
created with no external memory defined. This allows all MAR pages to be
tagged "non-cached" by default, and the programmer is free to set MAR bits
to their liking.
On MAR-based cores (i.e., C6x), SYS/BIOS will, by default, set the
"cacheable" bit for any external memory that it "sees", i.e., any
external memory that is defined for the platform. This happens regardless
of whether or not that memory is used for program placement. This
cacheable-ness is somewhat hidden to the programmer.
In order to offer better control of this, Keystone platform instances are
created with no external memory defined. This allows all MAR pages to be
tagged "non-cached" by default, and the programmer is free to set MAR bits
to their liking.
MultiProc: API Guide updates (doxygen)
Clarified OS-specific configuration details.
Added some use case descriptions for when
MultiProc_setLocalId() might be used.
Clarified OS-specific configuration details.
Added some use case descriptions for when
MultiProc_setLocalId() might be used.
Linux: Tracing ease of use
Allow end users to enable userspace tracing via an environment
variable (IPC_DEBUG). Setting IPC_DEBUG=1 enables 'some' trace,
setting IPC_DEBUG to 2 (or 3) enables more.
This imitates a popular feature from Codec Engine, details here:
http://processors.wiki.ti.com/index.php/CE_DEBUG
Allow end users to enable userspace tracing via an environment
variable (IPC_DEBUG). Setting IPC_DEBUG=1 enables 'some' trace,
setting IPC_DEBUG to 2 (or 3) enables more.
This imitates a popular feature from Codec Engine, details here:
http://processors.wiki.ti.com/index.php/CE_DEBUG
Linux: Fix a few build warnings
Added a missing header, deleted an unused variable.
Added a missing header, deleted an unused variable.
Remove dead code used for support of slaves with MMU disabled in QNX
This commit removes the SysLink_Override_Params mechanism that is used
to turn on support for slaves with MMU disabled. This mode was never
tested, nor do we anticipate supporting this in the future, given
the benefits of an MMU.
Signed-off-by: VW <vwan@ti.com>
This commit removes the SysLink_Override_Params mechanism that is used
to turn on support for slaves with MMU disabled. This mode was never
tested, nor do we anticipate supporting this in the future, given
the benefits of an MMU.
Signed-off-by: VW <vwan@ti.com>
QNX: Remove dead virtio-related macros
Note virtio in this case is the virtualized platform, not the
protocol rpmsg is built on.
We no longer support OMAP5 or DRA7XX-based virtio platforms,
this commit removes related preprocessor defines set in makefiles
and used throughout the code base.
Note virtio in this case is the virtualized platform, not the
protocol rpmsg is built on.
We no longer support OMAP5 or DRA7XX-based virtio platforms,
this commit removes related preprocessor defines set in makefiles
and used throughout the code base.
QNX: Stop building early for unsupported platforms
Catch an unsupported platform sooner with a simple check.
Without this check, the build proceeds and fails halfway through with
a confusing error - in my case it was when the loader was being built
and some of the required preprocessor defines weren't set.
Catch an unsupported platform sooner with a simple check.
Without this check, the build proceeds and fails halfway through with
a confusing error - in my case it was when the loader was being built
and some of the required preprocessor defines weren't set.
Fixed 'use' help text to add new -t option in ipc_trace_daemon for QNX
Minor update of the help text to add the option, in case the user uses the
'use' command for help.
This addresses CQ SDOCM00107256.
Signed-off-by: VW <vwan@ti.com>
Minor update of the help text to add the option, in case the user uses the
'use' command for help.
This addresses CQ SDOCM00107256.
Signed-off-by: VW <vwan@ti.com>
Add new resource type and corresponding struct for internal memory
A new resource type TYPE_INTMEM is added that allows specifying internal
memory resources that the kernel will map and later on load ELF file
sections.
This new type replaces TYPE_CRASHDUMP, which is not used or supported.
A new resource type TYPE_INTMEM is added that allows specifying internal
memory resources that the kernel will map and later on load ELF file
sections.
This new type replaces TYPE_CRASHDUMP, which is not used or supported.
Fix VirtQueue_getAvailBuf on QNX to avoid race condition
This is to address SDOCM00106156.
In commit c98d2c5624aac20bcdd738f5a54fbddca045fd69, we have fixed a race
condition on the BIOS side by clearing the VRING_USED_F_NO_NOTIFY flag
prior to checking whether there are remaining buffers. We are now doing
the same on the host side.
Note that this code is not currently exercised on the host, but is simply
maintained to ensure that the VirtQueue module is complete in functionality.
Signed-off-by: VW <vwan@ti.com>
This is to address SDOCM00106156.
In commit c98d2c5624aac20bcdd738f5a54fbddca045fd69, we have fixed a race
condition on the BIOS side by clearing the VRING_USED_F_NO_NOTIFY flag
prior to checking whether there are remaining buffers. We are now doing
the same on the host side.
Note that this code is not currently exercised on the host, but is simply
maintained to ensure that the VirtQueue module is complete in functionality.
Signed-off-by: VW <vwan@ti.com>
Linux: Quiet "unused variable" build warning
For Linux-based devices without GateMP support (e.g. OMAP5, TCI6638),
remove an unused variable declaration.
For Linux-based devices without GateMP support (e.g. OMAP5, TCI6638),
remove an unused variable declaration.
Docs: Minor spec clarifications for MmRpc
Clarify that the 'handle' parameter for various MmRpc APIs must
be valid.
Clarify that the 'handle' parameter for various MmRpc APIs must
be valid.
Build: Removed unused ti.sdo.ipc.build pkg
This package is no longer used and can be removed.
This package is no longer used and can be removed.
SDOCM00106949 IPC interrupt preempts itself on ARP32 (EVE)
Changed default interrupt vector to actual values. When creating Hwi
instances, compute a mask which blocks both interrupt vectors. Set
the mask in Hwi create params.
Changed default interrupt vector to actual values. When creating Hwi
instances, compute a mask which blocks both interrupt vectors. Set
the mask in Hwi create params.
SDOCM00106428 Notify mailbox driver support on DRA7xx (DSP, EVE)
New NotifyDriverMbx module; initial implementation of notify mailbox
driver on dsp and eve only. Added support for multiple notify driver
configs in NotifySetup; requires new dispatch isr for notify events.
The isr will dispatch to the appropriate driver (shm or mbx). Improved
the NotifyDriverShm performance because it checks only the mailboxes
which might have raised the given event instead of always checking all
mailboxes. Added ROV view of NotifyDriverMbx. Added a mailbox tab
which shows inbound and outbound mailbox status. Better ISA handling in
source code and script code. Updated Build module with NotifyDriverMbx.c
to include new driver in IPC product libraries for C66 and ARP32.
New NotifyDriverMbx module; initial implementation of notify mailbox
driver on dsp and eve only. Added support for multiple notify driver
configs in NotifySetup; requires new dispatch isr for notify events.
The isr will dispatch to the appropriate driver (shm or mbx). Improved
the NotifyDriverShm performance because it checks only the mailboxes
which might have raised the given event instead of always checking all
mailboxes. Added ROV view of NotifyDriverMbx. Added a mailbox tab
which shows inbound and outbound mailbox status. Better ISA handling in
source code and script code. Updated Build module with NotifyDriverMbx.c
to include new driver in IPC product libraries for C66 and ARP32.
BIOS: NameServerRemoteNotify callback may have uninitialized var
The callback function for NameServerRemoteNotify may end up with an
uninitialized swiHandle. Though this case should never happen, the handle
should be initialized and an assert must be issued if it remains NULL.
This also fixes a Coverity error with the variable.
The callback function for NameServerRemoteNotify may end up with an
uninitialized swiHandle. Though this case should never happen, the handle
should be initialized and an assert must be issued if it remains NULL.
This also fixes a Coverity error with the variable.
BIOS: NameServerRemote must copy names with 1 char less than max
The strncpy length must be max number of characters - 1 bytes. The last
character will be the null termination thus shouldn't be copied. This
fix addresses a Coverity buffer overrun error.
The strncpy length must be max number of characters - 1 bytes. The last
character will be the null termination thus shouldn't be copied. This
fix addresses a Coverity buffer overrun error.
BIOS: NameServerMessageQ names need proper termination
The NameServerMessageQ instanceName and name strings weren't being
properly null terminated when the names were 1 character less than the
maximum size. This addresses the following bug:
SDOCM00106336: NameServerMessageQ copy of name is not copying null
terminated character
The NameServerMessageQ instanceName and name strings weren't being
properly null terminated when the names were 1 character less than the
maximum size. This addresses the following bug:
SDOCM00106336: NameServerMessageQ copy of name is not copying null
terminated character
Remove dead code that appears to be trying to set L1D cache size to 0
The way to set an L1/L2 cache size is through the Build.platformTable
platform instance creation. The dead code that is removed here was not
only trying to change the cache size at too late a time, it was doing
so by setting a local variable that went nowhere.
The way to set an L1/L2 cache size is through the Build.platformTable
platform instance creation. The dead code that is removed here was not
only trying to change the cache size at too late a time, it was doing
so by setting a local variable that went nowhere.
Eliminate need to specify Syslink_Override_Params on QNX
This commit changes Syslink_Override_Params in Platform.c to an empty
string. It removes the need to specify carveouts in the string, which
was only used for verification purposes when there is a slave-side MMU.
Code associated with the verification of the resource table entries
against these carveouts is removed.
This commit also changes the default for mmuEnable to TRUE, since that
is currently the only mode we support.
This addresses CQ SDOCM00105667.
Signed-off-by: VW <vwan@ti.com>
This commit changes Syslink_Override_Params in Platform.c to an empty
string. It removes the need to specify carveouts in the string, which
was only used for verification purposes when there is a slave-side MMU.
Code associated with the verification of the resource table entries
against these carveouts is removed.
This commit also changes the default for mmuEnable to TRUE, since that
is currently the only mode we support.
This addresses CQ SDOCM00105667.
Signed-off-by: VW <vwan@ti.com>
Add timestamp prefix to LOG[0|1|2]() macros
For the timestamp prefix, subtract the start time (which is established
when the logFile is opened) so that the massive "since the epoch" value
is not displayed. For this, subtract only the timeval.tv_sec (seconds)
value so we don't have to worry about the "borrow" that results when
start_tv.tv_usec > tv.tv_usec (essentially, treat start_tv.tv_usec as 0,
which skews this "relative" time ahead by start_tv.tv_usec microseconds).
For the timestamp prefix, subtract the start time (which is established
when the logFile is opened) so that the massive "since the epoch" value
is not displayed. For this, subtract only the timeval.tv_sec (seconds)
value so we don't have to worry about the "borrow" that results when
start_tv.tv_usec > tv.tv_usec (essentially, treat start_tv.tv_usec as 0,
which skews this "relative" time ahead by start_tv.tv_usec microseconds).
Test: Fix NameServerApp config
IpcMgr_ipcStartup() was being added twice to the BIOS startup
function - once in nameserverapp.cfg (which is removed in this
commit) and again in messageq_common.cfg.xs (which is included
by nameserverapp.cfg). In addition to just being wrong, this
resulted in an abort on Keystone 2 devices.
Also, the MessageQ.SetupTransportProxy was errantly not assigned
in the nameserverapp.cfg script. This resulted in MessageQ.xs
pulling in 'default' MessageQ configuration, which pulled in much
more content than was necessary for this test (for example,
TransportShm, which then pulled in GateMP, SharedRegion, etc). By
explicitly assigning MessageQ.SetupTransportProxy to the
ti.ipc.transports.TransportRpmsgSetup module, these extra [unused]
modules are no longer pulled in.
IpcMgr_ipcStartup() was being added twice to the BIOS startup
function - once in nameserverapp.cfg (which is removed in this
commit) and again in messageq_common.cfg.xs (which is included
by nameserverapp.cfg). In addition to just being wrong, this
resulted in an abort on Keystone 2 devices.
Also, the MessageQ.SetupTransportProxy was errantly not assigned
in the nameserverapp.cfg script. This resulted in MessageQ.xs
pulling in 'default' MessageQ configuration, which pulled in much
more content than was necessary for this test (for example,
TransportShm, which then pulled in GateMP, SharedRegion, etc). By
explicitly assigning MessageQ.SetupTransportProxy to the
ti.ipc.transports.TransportRpmsgSetup module, these extra [unused]
modules are no longer pulled in.
Revert "SDOCM00106428 Add notify mailbox driver support on DRA7xx (Part 1)"
This reverts commit 3be15bd0ee6a26a8c1d712e698f4055b94f47043.
This reverts commit 3be15bd0ee6a26a8c1d712e698f4055b94f47043.
Revert "SDOCM00106428 Add notify mailbox driver support on DRA7xx (Part 2)"
This reverts commit 73882d944bb7b1865f4c35e4bdb35c05bc3da9e5.
This reverts commit 73882d944bb7b1865f4c35e4bdb35c05bc3da9e5.
Revert "SDOCM00106428 Add notify mailbox driver support on DRA7xx (Part 3)"
This reverts commit 65a4b382ea3fc702dedc51f02471149e642772b8.
This reverts commit 65a4b382ea3fc702dedc51f02471149e642772b8.
Fix misuse of SET_BIT macro to clear mailbox-interrupt-status-clear registers
The mailbox interrupt handling code in QNX IPC uses the SET_BIT macro to
clear status bits from the MAILBOX_IRQSTATUS_CLR_u registers. This is wrong,
because the macro does as follows:
>#define SET_BIT(num,pos) ((num) |= (1u << (pos)))
It will read the register and end up clearing *ALL* bits that are pending
during the write-back, as opposed to the specific one it needs to clear. If the
host is in the midst of processing an interrupt from a given core when a second
core writes to its (sub)mailbox, the second payload may be lost.
This commit changes the SET_BIT call to a direct register assignment of the
appropriate bit mask.
Signed-off-by: VW <vwan@ti.com>
The mailbox interrupt handling code in QNX IPC uses the SET_BIT macro to
clear status bits from the MAILBOX_IRQSTATUS_CLR_u registers. This is wrong,
because the macro does as follows:
>#define SET_BIT(num,pos) ((num) |= (1u << (pos)))
It will read the register and end up clearing *ALL* bits that are pending
during the write-back, as opposed to the specific one it needs to clear. If the
host is in the midst of processing an interrupt from a given core when a second
core writes to its (sub)mailbox, the second payload may be lost.
This commit changes the SET_BIT call to a direct register assignment of the
appropriate bit mask.
Signed-off-by: VW <vwan@ti.com>
Increase NAMESERVER_GET_TIMEOUT from 20000 to 40000 microseconds
Product testing revealed that a remote core was occasionally taking
slighly longer than 20000 microseconds to respond (in the negative)
to a NameServer_getRemote() query. We're not sure why it's taking
so long in some cases, as normally the remote core will respond in a
few hundred microseconds.
Doubling the timeout will affect the total query time across multiple
remote cores when some of those cores aren't running NameServer, but
this should be OK since it affects "startup" times with MessageQ_open()
and shouldn't affect normal "execute" times.
Product testing revealed that a remote core was occasionally taking
slighly longer than 20000 microseconds to respond (in the negative)
to a NameServer_getRemote() query. We're not sure why it's taking
so long in some cases, as normally the remote core will respond in a
few hundred microseconds.
Doubling the timeout will affect the total query time across multiple
remote cores when some of those cores aren't running NameServer, but
this should be OK since it affects "startup" times with MessageQ_open()
and shouldn't affect normal "execute" times.
Remove duplicated call to GateMP_close in gatempapp on BIOS side
Signed-off-by: VW <vwan@ti.com>
Signed-off-by: VW <vwan@ti.com>
Build: Switch from ?= assignments to =
products.mak should use the [less confusing] = assignments, rather
than the set-if-not-already-set ?= assignment. This helps with user
readability of the assignments.
products.mak should use the [less confusing] = assignments, rather
than the set-if-not-already-set ?= assignment. This helps with user
readability of the assignments.
SDOCM00106664: Reduce slave-side trace from tests
The slave-side trace enabled by the tests is too high. It obfuscates
actual test output, as well as, in at least one case, was slowing
down the slave-side execution enough to cause host-side timeouts
waiting for replies.
This commit changes some Registry-related masks from ALWAYS_ON
to RUNTIME_OFF to help quiet things down.
The slave-side trace enabled by the tests is too high. It obfuscates
actual test output, as well as, in at least one case, was slowing
down the slave-side execution enough to cause host-side timeouts
waiting for replies.
This commit changes some Registry-related masks from ALWAYS_ON
to RUNTIME_OFF to help quiet things down.
Enable gptimers in PD_IPU domain
This commit adds workaround to enable gptimers in PD_IPU domain on Vayu in QNX.
It enables example ex41_forwardmsg to run successfully.
Signed-off-by: VW <vwan@ti.com>
This commit adds workaround to enable gptimers in PD_IPU domain on Vayu in QNX.
It enables example ex41_forwardmsg to run successfully.
Signed-off-by: VW <vwan@ti.com>
SDOCM00106450 HeapMemMP_free fails to cache invalidate freed...
The freed buffer content (after the header) was left in cache. If
buffer content was dirty, it would eventually be evicted with a
write-back possibly overwriting memory in use by a different core,
and cause heap corruption.
The freed buffer content (after the header) was left in cache. If
buffer content was dirty, it would eventually be evicted with a
write-back possibly overwriting memory in use by a different core,
and cause heap corruption.
SDOCM00106428 Add notify mailbox driver support on DRA7xx (Part 3)
Added notify mailbox driver support for ARP32. The IPC interrupt on
arp32 will dispatch to the appropriate driver (shm or mbx). This
improves the NotifyDriverShm performance because it checks only the
mailboxes which might have raised the given event instead of always
checking all mailboxes. Improved ROV view of NotifyDriverMbx. Added
a mailbox tab which shows inbound and outbound mailbox status. Better
ISA handling in source code and script code.
Added notify mailbox driver support for ARP32. The IPC interrupt on
arp32 will dispatch to the appropriate driver (shm or mbx). This
improves the NotifyDriverShm performance because it checks only the
mailboxes which might have raised the given event instead of always
checking all mailboxes. Improved ROV view of NotifyDriverMbx. Added
a mailbox tab which shows inbound and outbound mailbox status. Better
ISA handling in source code and script code.
Add configurable polling interval to ipc_trace_daemon on QNX
This commit adds a command line parameter to ipc_trace_daemon to set the
polling interval. The default is now set to 0.5 sec as the previous
default was too long. This addresses SDOCM00105472.
Signed-off-by: VW <vwan@ti.com>
This commit adds a command line parameter to ipc_trace_daemon to set the
polling interval. The default is now set to 0.5 sec as the previous
default was too long. This addresses SDOCM00105472.
Signed-off-by: VW <vwan@ti.com>
Linux/Qnx: MessageQBench test must check initial MSG put
The MessageQBench test must ensure the initial MessageQ_put during
the applications handshaking returns successful before continuing.
The MessageQBench test must ensure the initial MessageQ_put during
the applications handshaking returns successful before continuing.
Add IPU1 support in QNX
This commit adds support for IPU1 in QNX. It has the current limitation that
the core cannot be put into deep sleep in the idle task, so the function
IpcPower_idle() must be removed from the idle loop. This issue will be fixed
at a later time.
Signed-off-by: VW <vwan@ti.com>
This commit adds support for IPU1 in QNX. It has the current limitation that
the core cannot be put into deep sleep in the idle task, so the function
IpcPower_idle() must be removed from the idle loop. This issue will be fixed
at a later time.
Signed-off-by: VW <vwan@ti.com>
SDOCM00106428 Add notify mailbox driver support on DRA7xx (Part 2)
Updated Build module with NotifyDriverMbx.c to include new driver
in IPC product libraries (C66, M4, ARP32, A15g).
Updated Build module with NotifyDriverMbx.c to include new driver
in IPC product libraries (C66, M4, ARP32, A15g).
VAYU QNX: Prevent race condition when host is slow to clear interrupts from IPU
This commit prevents the same race condition that was fixed in commit id
feb7a8486ed537033c5aed5b170f52f758bddabe, this time for the IPUs as
the other commit only dealt with the DSP.
Signed-off-by: VW <vwan@ti.com>
This commit prevents the same race condition that was fixed in commit id
feb7a8486ed537033c5aed5b170f52f758bddabe, this time for the IPUs as
the other commit only dealt with the DSP.
Signed-off-by: VW <vwan@ti.com>
SDOCM00106428 Add notify mailbox driver support on DRA7xx (Part 1)
New NotifyDriverMbx module; initial implementation of notify mailbox
driver on dsp only. Added support for multiple notify driver configs
in NotifySetup; requires new dispatch isr for notify events.
New NotifyDriverMbx module; initial implementation of notify mailbox
driver on dsp only. Added support for multiple notify driver configs
in NotifySetup; requires new dispatch isr for notify events.
Linux/Qnx: MessageQ msg cannot be freed if put fails
MessageQ msg being put to the transport layer can only be freed
if the msg is successfully placed. Otherwise, it's the responsibility
of the application to free the msg.
MessageQ msg being put to the transport layer can only be freed
if the msg is successfully placed. Otherwise, it's the responsibility
of the application to free the msg.
BIOS: Only build rpmsg libs when useful
Many of the rpmsg-protocol-related IPC packages build for
all targets thrown at them (like good packages should).
However, we know many supported targets will never use the rpmsg
protocol, and we are therefore unnecessarily building libraries
that will never be used.
This commit changes some of the rpmsg-specific packages to not
build for targets that don't have any devices containing an
rpmsg-using HLOS-based host.
Many of the rpmsg-protocol-related IPC packages build for
all targets thrown at them (like good packages should).
However, we know many supported targets will never use the rpmsg
protocol, and we are therefore unnecessarily building libraries
that will never be used.
This commit changes some of the rpmsg-specific packages to not
build for targets that don't have any devices containing an
rpmsg-using HLOS-based host.
Linux: Fix pkg-config dependency name
The name of dependent packages includes the 'lib' prefix - this
fixes pkg-config when run on libtiipc.pc.
The name of dependent packages includes the 'lib' prefix - this
fixes pkg-config when run on libtiipc.pc.
Linux: Fix warnings in LAD for non GateMP builds
To eliminate build warnings in LAD, variables used for GateMP enabled
code need to be encapsulated.
To eliminate build warnings in LAD, variables used for GateMP enabled
code need to be encapsulated.
Linux: Update autotools generated files
Check in autoreconf-generated files after the change from
C66AK2E to 66AK2E.
Check in autoreconf-generated files after the change from
C66AK2E to 66AK2E.
66AK2E: Linux: Remove leading 'C' in device name
The initial Linux support for 66AK2E (commit
f45b1ad1a591b188eb1321102a3b8ed479eec490) went in with
the leading 'C66AK2E' identifier. After review by the MCSDK team,
the leading 'C' was incorrect and removed.
Note that autotools' condition variables must start with a
leading character, so internally the variable 'C66AK2E' is
still used. But the user only sees '66AK2E' when setting
the PLATFORM variable.
The BIOS-side changes are in a separate commit.
The initial Linux support for 66AK2E (commit
f45b1ad1a591b188eb1321102a3b8ed479eec490) went in with
the leading 'C66AK2E' identifier. After review by the MCSDK team,
the leading 'C' was incorrect and removed.
Note that autotools' condition variables must start with a
leading character, so internally the variable 'C66AK2E' is
still used. But the user only sees '66AK2E' when setting
the PLATFORM variable.
The BIOS-side changes are in a separate commit.
66AK2E: BIOS: Remove leading 'C' in device name
The initial support for 66AK2E (commit
867efc6fa15f91639820614f6f9ca6ee6751ffa6) went in with
the 'C66AK2E' identifier. After review by the MCSDK team,
the leading 'C' was incorrect and removed.
The XDC platform and catalog includes this leading 'C', so
most of the internal config-related support did not require
changes.
Finally, this is only the BIOS-side changes. The Linux-side
changes will be done in a subsequent commit.
The initial support for 66AK2E (commit
867efc6fa15f91639820614f6f9ca6ee6751ffa6) went in with
the 'C66AK2E' identifier. After review by the MCSDK team,
the leading 'C' was incorrect and removed.
The XDC platform and catalog includes this leading 'C', so
most of the internal config-related support did not require
changes.
Finally, this is only the BIOS-side changes. The Linux-side
changes will be done in a subsequent commit.
SDOCM00106383: Remove C6x COFF support
C6x COFF support is being [softly] removed from IPC 3.21. This
commit deletes C6x COFF-related variables from products.mak, but
leaves everything else intact. If a user finds they need COFF
support, they can easily re-enable it themselves by setting the
variable(s) removed from products.mak and rebuilding.
Eventually the intent is to remove C6x COFF support altogether -
including the build support in ipc-bios.mak and ipc-bios.bld, and
possibly elsewhere.
C6x COFF support is being [softly] removed from IPC 3.21. This
commit deletes C6x COFF-related variables from products.mak, but
leaves everything else intact. If a user finds they need COFF
support, they can easily re-enable it themselves by setting the
variable(s) removed from products.mak and rebuilding.
Eventually the intent is to remove C6x COFF support altogether -
including the build support in ipc-bios.mak and ipc-bios.bld, and
possibly elsewhere.
BIOS: GateMP host support must ensure maxNameLen is 32
When GateMP host support is enabled, the default GateMP must ensure
the size of the maxNameLen must be at least 32. The size must correspond
to the expected size on the host OS (Linux, Qnx, Android) which is
currently 32.
The default size for maxNameLen on the BIOS-side is 32. Thus this issue
hadn't be encountered.
When GateMP host support is enabled, the default GateMP must ensure
the size of the maxNameLen must be at least 32. The size must correspond
to the expected size on the host OS (Linux, Qnx, Android) which is
currently 32.
The default size for maxNameLen on the BIOS-side is 32. Thus this issue
hadn't be encountered.
Linux/Android: Remove existing response FIFO in LAD
In rare instances when LAD is improperly terminated, the PID-based
response FIFO will not be removed. This will cause startup failures
of subsequent execution of LAD. The existing response FIFO must be
removed before creating new ones with the same PID. (SDOCM00106318)
In rare instances when LAD is improperly terminated, the PID-based
response FIFO will not be removed. This will cause startup failures
of subsequent execution of LAD. The existing response FIFO must be
removed before creating new ones with the same PID. (SDOCM00106318)
Android: Change LAD's working directory
Depending on user privileges when the LAD daemon is started, the
working directory may not be writable. The directory has been moved
to /data/lad. File permissions at this level are easier to dictate
(SDOCM00106314).
Depending on user privileges when the LAD daemon is started, the
working directory may not be writable. The directory has been moved
to /data/lad. File permissions at this level are easier to dictate
(SDOCM00106314).
VirtQueue: Remove "A9" from #defines
Many of our supported devices do not use A9s, so generalize
the definitions that previously used A9 in them.
Many of our supported devices do not use A9s, so generalize
the definitions that previously used A9 in them.
DRA7XX: Remove unnecessary rpmsg-related code
Similar to commit 16adcaad which cleaned up OMAP5 code, this
removes dead code for DRA7XX. Most of the changes remove
untested, and likely broken, non-SMP code.
In at least one case, the code cleanup may fix previously
undiscovered issues. For example, in VirtQueue_isr(), the first
switch() block was [likely inadvertently] skipped for DSP2. There
is no known issue because of this, but now with this cleanup, DSP2
will (and should!) participate in this initial switch statement.
Similar to commit 16adcaad which cleaned up OMAP5 code, this
removes dead code for DRA7XX. Most of the changes remove
untested, and likely broken, non-SMP code.
In at least one case, the code cleanup may fix previously
undiscovered issues. For example, in VirtQueue_isr(), the first
switch() block was [likely inadvertently] skipped for DSP2. There
is no known issue because of this, but now with this cleanup, DSP2
will (and should!) participate in this initial switch statement.
DRA7XX: Use XDC preprocessor definitions
Switch from IPC created preprocessor definitions (set by
package.bld) to standard XDC-provided definitions.
Also remove some minor dead code.
This is just code cleanup, no intended functional change.
Switch from IPC created preprocessor definitions (set by
package.bld) to standard XDC-provided definitions.
Also remove some minor dead code.
This is just code cleanup, no intended functional change.
C66AK2E: BIOS: Fix C66AK2E test
Building on 867efc6fa15f91639820614f6f9ca6ee6751ffa6, this
fixes a test that was failing to build for C66AK2E.
Building on 867efc6fa15f91639820614f6f9ca6ee6751ffa6, this
fixes a test that was failing to build for C66AK2E.
VAYU QNX: Prevent race condition when ARM is slow to handle mailbox interrupts
This patch fixes a race condition where the host side in QNX is slow to clear a
mailbox interrupt. If the slave were to try to send another interrupt before
the ARM has cleared the first one, the code in InterruptDsp_intSend()
will simply drop it. This is bad because on QNX, the code in VirtQueue_ISR
interprets the received arg as the VirtQueue id. Hence if consecutive
messages were sent with different ids, the second message would be missed.
The fix is to poll whenever the mailbox is occupied, and send the message
only when the mailbox is free. (SDOCM00106278)
Signed-off-by: VW <vwan@ti.com>
This patch fixes a race condition where the host side in QNX is slow to clear a
mailbox interrupt. If the slave were to try to send another interrupt before
the ARM has cleared the first one, the code in InterruptDsp_intSend()
will simply drop it. This is bad because on QNX, the code in VirtQueue_ISR
interprets the received arg as the VirtQueue id. Hence if consecutive
messages were sent with different ids, the second message would be missed.
The fix is to poll whenever the mailbox is occupied, and send the message
only when the mailbox is free. (SDOCM00106278)
Signed-off-by: VW <vwan@ti.com>
BIOS: Fix typo in variable name
SZIE? Really? This stuff kills me.
SZIE? Really? This stuff kills me.
Linux: Update autotools generated files
Check in autoreconf-generated files after the pkg-config
changes.
Check in autoreconf-generated files after the pkg-config
changes.
SDOCM00103659: Add pkg-config support
This builds on commit 6348f9de, which added pkg-config support for
the mmrpc lib. This commit adds pkg-config support
for the tiipc and tiipcutils libraries.
Also updates .gitignore to ignore the generated *.pc files.
This builds on commit 6348f9de, which added pkg-config support for
the mmrpc lib. This commit adds pkg-config support
for the tiipc and tiipcutils libraries.
Also updates .gitignore to ignore the generated *.pc files.
DRA7XX: Minor test cfg script refactoring
Only MmServicMgr-using slaves require the
ti.sysbios.xdcruntime.GateThreadSupport Module. This moves
the dependency on that package from the common Dsp_vayu.cfg into
the one MmServiceMgr-based test.
Only MmServicMgr-using slaves require the
ti.sysbios.xdcruntime.GateThreadSupport Module. This moves
the dependency on that package from the common Dsp_vayu.cfg into
the one MmServiceMgr-based test.
DRA7XX: Consolidate DSP1/2 config scripts
Lots of duplication between DRA7XX's ti/ipc/tests/Dsp(1|2).cfg
scripts. This commit merges the two into Dsp_vayu.cfg, which
encapsulates the single "real" difference, which was the
MultiProc config name. It also adjusts users of these Dsp .cfg
scripts to now use the common Dsp_vayu.cfg script.
Lots of duplication between DRA7XX's ti/ipc/tests/Dsp(1|2).cfg
scripts. This commit merges the two into Dsp_vayu.cfg, which
encapsulates the single "real" difference, which was the
MultiProc config name. It also adjusts users of these Dsp .cfg
scripts to now use the common Dsp_vayu.cfg script.
OMAP5: Adjust IPU carveout size and linker map
The sizes for the IPU data section has been reduced, in line
with the changes on the host OS side. There is no change in
the starting addresses of either the DSP or IPU. The linker
memory map file used for building OMAP5 samples has also been
adjusted accordingly.
Signed-off-by: Suman Anna <s-anna@ti.com>
The sizes for the IPU data section has been reduced, in line
with the changes on the host OS side. There is no change in
the starting addresses of either the DSP or IPU. The linker
memory map file used for building OMAP5 samples has also been
adjusted accordingly.
Signed-off-by: Suman Anna <s-anna@ti.com>
DRA7xx: Adjust carveout sizes and addresses
The starting addresses for the resource table carveouts have
been adjusted in line with the changes on the host OS side.
The IPU2 size has been decreased, and the starting addresses
of the vrings have been reshuffled.
The linker memory map has also been adjusted for IPU2. No memory
map changes were made to IPU1 and DSP1 processors even though
the host-side can support a little bit more larger footprint
images - the current memory maps for these processors is a
minimal memory map.
Signed-off-by: Suman Anna <s-anna@ti.com>
The starting addresses for the resource table carveouts have
been adjusted in line with the changes on the host OS side.
The IPU2 size has been decreased, and the starting addresses
of the vrings have been reshuffled.
The linker memory map has also been adjusted for IPU2. No memory
map changes were made to IPU1 and DSP1 processors even though
the host-side can support a little bit more larger footprint
images - the current memory maps for these processors is a
minimal memory map.
Signed-off-by: Suman Anna <s-anna@ti.com>
Vayu: Minor comment wordsmithing
Fix typo, 80 char alignment.
Fix typo, 80 char alignment.
Tests: Remove MPU mapping from gatempapp sample's resource table
The L4_PER mapping entry is split into three individual L4_PERx
entries. This is done to remove any mappings for the MPU-relevant
address spaces into the slave processor MMUs.
This change incorporates the same changes to the gatempapp resource
table as in commit,
e4b6067 "Remoteproc: DRA7xx: Remove MPU mapping from resource table".
Signed-off-by: Suman Anna <s-anna@ti.com>
The L4_PER mapping entry is split into three individual L4_PERx
entries. This is done to remove any mappings for the MPU-relevant
address spaces into the slave processor MMUs.
This change incorporates the same changes to the gatempapp resource
table as in commit,
e4b6067 "Remoteproc: DRA7xx: Remove MPU mapping from resource table".
Signed-off-by: Suman Anna <s-anna@ti.com>
Android: Adds GateMP build support
The necessary build files have been updated to add GateMP for
Android. The functionality has been verified manually using
breakpoints to ensure GateMP APIs are behaving as expected.
The necessary build files have been updated to add GateMP for
Android. The functionality has been verified manually using
breakpoints to ensure GateMP APIs are behaving as expected.
Linux: LAD requires -l option for logging
With the addition of GateMP support, the LAD daemon now processes
arguments differently. An 'l' option is now required to enable
logging. The 'g' option enables GateMP support. A usage output has
been added with an 'h' option.
Examples:
lad_<platform> -h
lad_<platform> -l log.txt
lad_<platform> -g -l log.txt
With the addition of GateMP support, the LAD daemon now processes
arguments differently. An 'l' option is now required to enable
logging. The 'g' option enables GateMP support. A usage output has
been added with an 'h' option.
Examples:
lad_<platform> -h
lad_<platform> -l log.txt
lad_<platform> -g -l log.txt
OMAP5: Minor test cfg cleanup
Minor config refactoring. The GateThreadSupport module is only
needed by grcm users, but was brought in through Dsp.cfg which
is used by non-grcm-using tests. Also, took the opportunity to
fixup some syntax buglets and remove some dead comments.
Minor config refactoring. The GateThreadSupport module is only
needed by grcm users, but was brought in through Dsp.cfg which
is used by non-grcm-using tests. Also, took the opportunity to
fixup some syntax buglets and remove some dead comments.
Linux: Improve MessageQApp cmdline error handling
In the MessageQApp, if an errant 2nd arg is passed on the command
line (e.g. "DSP" instead of "2"), the calculated procId is 0
(which is the host), and HOST<->HOST messaging is attempted. This
isn't supported.
This commit catches that errant cmdline and emits an error.
In the MessageQApp, if an errant 2nd arg is passed on the command
line (e.g. "DSP" instead of "2"), the calculated procId is 0
(which is the host), and HOST<->HOST messaging is attempted. This
isn't supported.
This commit catches that errant cmdline and emits an error.
OMAP5: Remove unnecessary rpmsg-related code
The original OMAP5 code import included support for running the
IPU in non-SMP BIOS. This was untested in the context of IPC 3.x,
and is not supported. The unsupported/dead stuff was obfuscating
the live stuff, so this commit removes it.
There is no intentional change in behavior, other than slight
performance improvement due to small bits of code removal.
The original OMAP5 code import included support for running the
IPU in non-SMP BIOS. This was untested in the context of IPC 3.x,
and is not supported. The unsupported/dead stuff was obfuscating
the live stuff, so this commit removes it.
There is no intentional change in behavior, other than slight
performance improvement due to small bits of code removal.
BIOS: Enable xdc__strict and fix issues
XDC provides a xdc__strict feature. Defining that pre-processor
variable prior to #including <xdc/std.h> will disable deprecated
data types (e.g. Uint32 - note the lowercase 'i') and change
NULL from '0' to '(void *)0'.
This commit throws that xdc__strict definition when building the
BIOS-side code, and fixes issues that were found enabling it.
Interestingly, there were a few bugs that turned up during this
exercise (rare in the wild, but still good cleanup).
XDC provides a xdc__strict feature. Defining that pre-processor
variable prior to #including <xdc/std.h> will disable deprecated
data types (e.g. Uint32 - note the lowercase 'i') and change
NULL from '0' to '(void *)0'.
This commit throws that xdc__strict definition when building the
BIOS-side code, and fixes issues that were found enabling it.
Interestingly, there were a few bugs that turned up during this
exercise (rare in the wild, but still good cleanup).
GateMP: Revert ti_sdo_ipc_GateMP_getSharedAddr
This function was inadvertently modified in a previous commit,
and needs to be reverted back to its original state.
(SDOCM00106117)
Signed-off-by: VW <vwan@ti.com>
This function was inadvertently modified in a previous commit,
and needs to be reverted back to its original state.
(SDOCM00106117)
Signed-off-by: VW <vwan@ti.com>
Linux: Update autotools-generated files
Linux: Fix gateMPApp unconditional build
The tests directory Makefile needs to ensure CMEM_INSTALL_DIR
variable is set before attempting to build the gateMPApp for DRA7XX.
The tests directory Makefile needs to ensure CMEM_INSTALL_DIR
variable is set before attempting to build the gateMPApp for DRA7XX.
Docs: Update MmRpc doxygen documentation
Linux: Update to autotools files for GateMP addition
Linux: Added GateMP support for DRA7XX devices
GateMP support has been added using the device's spinlocks.
To enable GateMP on the host, throw -g option when launching the
LAD daemon as follows:
./lad_dra7xx log.txt -g
To enable GateMP on the slave core, the core must be configured as
the owner of SR0 and GateMP.hostSupport config param must be set
to 'true' as follows:
var GateMP = xdc.useModule('ti.sdo.ipc.GateMP');
GateMP.hostSupport = true;
The slave core with GateMP enabled must the loaded (remoteproc)
prior to the execution of LAD on the host. This adds a restriction
on LAD that wasn't previously there.
Note: Initial validation has only been performed on DRA7XX DSP1.
GateMP support has been added using the device's spinlocks.
To enable GateMP on the host, throw -g option when launching the
LAD daemon as follows:
./lad_dra7xx log.txt -g
To enable GateMP on the slave core, the core must be configured as
the owner of SR0 and GateMP.hostSupport config param must be set
to 'true' as follows:
var GateMP = xdc.useModule('ti.sdo.ipc.GateMP');
GateMP.hostSupport = true;
The slave core with GateMP enabled must the loaded (remoteproc)
prior to the execution of LAD on the host. This adds a restriction
on LAD that wasn't previously there.
Note: Initial validation has only been performed on DRA7XX DSP1.
Linux: Update autotools generated files
Check in autoreconf-generated files for C66AK2E support.
Check in autoreconf-generated files for C66AK2E support.
C66AK2E: Linux: Introduce support for C66AK2E
The C66AK2E device is an A15 + C66 DSP, similar in hardware
to the TCI663X family of devices. This commit adds Linux-side
support.
Note that this commit doesn't update the autotools-generated
files. That will be done in a separate commit.
The C66AK2E device is an A15 + C66 DSP, similar in hardware
to the TCI663X family of devices. This commit adds Linux-side
support.
Note that this commit doesn't update the autotools-generated
files. That will be done in a separate commit.
C66AK2E: BIOS: Introduce support for C66AK2E
The C66AK2E device is an A15 + C66 DSP, similar in hardware
to the TCI663X family of devices. This commit adds BIOS-side
support.
The C66AK2E device is an A15 + C66 DSP, similar in hardware
to the TCI663X family of devices. This commit adds BIOS-side
support.
Linux: Update autotools generated files
Check in autoreconf-generated files.
Check in autoreconf-generated files.
TCI6630: Linux: Introduce support for TCI6630K2L
The TCI6630K2L device is an A15 + 4 C66 DSPs, very similar
to TCH6638K2K (A15 + 8 C66 DSPs). This commit adds
Linux support.
Note that this commit doesn't update the autotools-generated
files. That will be done in a separate commit.
The TCI6630K2L device is an A15 + 4 C66 DSPs, very similar
to TCH6638K2K (A15 + 8 C66 DSPs). This commit adds
Linux support.
Note that this commit doesn't update the autotools-generated
files. That will be done in a separate commit.
TCI6630: BIOS: Introduce support for TCI6630K2L
The TCI6630K2L device is an A15 + 4 C66 DSPs, very similar
to TCI6638K2K (A15 + 8 C66 DSPs). This commit adds
BIOS-side support.
The TCI6630K2L device is an A15 + 4 C66 DSPs, very similar
to TCI6638K2K (A15 + 8 C66 DSPs). This commit adds
BIOS-side support.
Increase the max name length for GateMP's NameServer on QNX to 32
This is to match up with the BIOS side default configuration in GateMP, and to
accommodate for the name of the default gate, which is 17-byte long.
Signed-off-by: VW <vwan@ti.com>
This is to match up with the BIOS side default configuration in GateMP, and to
accommodate for the name of the default gate, which is 17-byte long.
Signed-off-by: VW <vwan@ti.com>
Linux: Update autotools generated files
The autotools generated files have been update to reflect the addition
of a pkgconfig file for the mmrpc library.
Including the generated files in the development branch eliminates the
need for users to have autotools (autoconf, autoamke, and libtool) to
build ipc Linux sources.
The autotools generated files have been update to reflect the addition
of a pkgconfig file for the mmrpc library.
Including the generated files in the development branch eliminates the
need for users to have autotools (autoconf, autoamke, and libtool) to
build ipc Linux sources.
Linux: Add package config information to mmrpc
This patch adds the libmmrpc.pc to package config.
This aides in identifying the correct CFLAGS for any user or mmrpc
as below.
pkg-config --cflags libmmrpc
Using the above command, the applications using libmmrpc can
find the cflags automatically using pkg-config thus avoiding to
explicitly set the path to MmRpc.h
This patch adds the libmmrpc.pc to package config.
This aides in identifying the correct CFLAGS for any user or mmrpc
as below.
pkg-config --cflags libmmrpc
Using the above command, the applications using libmmrpc can
find the cflags automatically using pkg-config thus avoiding to
explicitly set the path to MmRpc.h