summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 7942b6b)
raw | patch | inline | side by side (parent: 7942b6b)
author | Buddy Liong <a0270631@ti.com> | |
Fri, 5 Feb 2016 22:53:27 +0000 (16:53 -0600) | ||
committer | Buddy Liong <a0270631@ti.com> | |
Mon, 2 Oct 2017 15:20:48 +0000 (10:20 -0500) |
Prior to this, DCE Server returns H264D_PutDataFxn() to codec as
soon as put_DataFxn() has been sent to MPU side (libdce client).
This become an issue when codec has sent the last H264D_PutDataFxn()
which will return the VIDDEC3_process call.
On the MPU side, it is still busy processing the put_DataFxn() and
when MPU is receiving VIDDEC3_process, it stops the put_DataFxn() and
there could be one more put_DataFxn that needs to be processed.
Because of this there is an issue of numBlocks corruption.
The solution is to make sure DCE Server doesn't return H264D_PutDataFxn()
to codec unless MPU side (libdce client) has come with the next
put_DataFxn().
Basically DCE Server needs to make sure that MPU side has processed
the data in H264D_PutDataFxn() before return it to codec.
This is track in a variable "putdata_toclient".
When codec returns VIDDEC3_process(), DCE Server needs to set
the variable "putData_endprocess" so that the next put_DataFxn()
will return numBlocks = 0.
This will allow MPU side (libdce client) to stop sending put_DataFxn().
Change-Id: Ied8c03eec8d4934eb1218f8687ad5cff6d17d57f
Signed-off-by: Buddy Liong <a0270631@ti.com>
soon as put_DataFxn() has been sent to MPU side (libdce client).
This become an issue when codec has sent the last H264D_PutDataFxn()
which will return the VIDDEC3_process call.
On the MPU side, it is still busy processing the put_DataFxn() and
when MPU is receiving VIDDEC3_process, it stops the put_DataFxn() and
there could be one more put_DataFxn that needs to be processed.
Because of this there is an issue of numBlocks corruption.
The solution is to make sure DCE Server doesn't return H264D_PutDataFxn()
to codec unless MPU side (libdce client) has come with the next
put_DataFxn().
Basically DCE Server needs to make sure that MPU side has processed
the data in H264D_PutDataFxn() before return it to codec.
This is track in a variable "putdata_toclient".
When codec returns VIDDEC3_process(), DCE Server needs to set
the variable "putData_endprocess" so that the next put_DataFxn()
will return numBlocks = 0.
This will allow MPU side (libdce client) to stop sending put_DataFxn().
Change-Id: Ied8c03eec8d4934eb1218f8687ad5cff6d17d57f
Signed-off-by: Buddy Liong <a0270631@ti.com>
src/ti/framework/dce/dce.c | patch | blob | history |
index 68a9cbc23e900517a8664ba9f661ff6662817df9..ab7de66b416be902177ccc4dc062d2fe121e0c7b 100644 (file)
/* Decoder Server static function declarations */
static VIDDEC3_Handle viddec3_create(Engine_Handle engine, String name, VIDDEC3_Params *params);
static XDAS_Int32 viddec3_control(VIDDEC3_Handle codec,VIDDEC3_Cmd id,VIDDEC3_DynamicParams * dynParams,VIDDEC3_Status * status);
+static XDAS_Int32 viddec3_process(VIDDEC3_Handle codec, XDM2_BufDesc *inBufs, XDM2_BufDesc *outBufs, VIDDEC3_InArgs *inArgs, VIDDEC3_OutArgs *outArgs);
+
static int viddec3_reloc(VIDDEC3_Handle handle, uint8_t *ptr, uint32_t len);
static pthread_mutex_t sync_process_mutex;
Uint32 codec_request;
Uint32 putdata_ready;
Uint32 mpu_crash_indication;
+ Uint32 putdata_toclient;
+ Uint32 putData_endprocess;
} Callback_data;
typedef struct {
[OMAP_DCE_VIDDEC3] =
{
(CreateFxn)viddec3_create, (ControlFxn)viddec3_control,
- (ProcessFxn)VIDDEC3_process, (DeleteFxn)VIDDEC3_delete,
+ (ProcessFxn)viddec3_process, (DeleteFxn)VIDDEC3_delete,
(RelocFxn)viddec3_reloc,
},
};
for (i = 0; i < DIM(c->encode_codec); i++) {
if (c->encode_codec[i] == codec) {
if (c->encode_callback[i].row_mode) {
- c->encode_callback[i].dataSyncHandle = codec;
- c->encode_callback[i].mpu_crash_indication = FALSE;
- dynParams->getDataFxn = (XDM_DataSyncGetFxn) H264E_GetDataFxn;
- dynParams->getDataHandle = codec;
+ if (id == XDM_SETPARAMS) {
+ c->encode_callback[i].dataSyncHandle = codec;
+ c->encode_callback[i].mpu_crash_indication = FALSE;
+ dynParams->getDataFxn = (XDM_DataSyncGetFxn) H264E_GetDataFxn;
+ dynParams->getDataHandle = codec;
+ }
}
}
}
@@ -347,11 +353,13 @@ static XDAS_Int32 viddec3_control(VIDDEC3_Handle codec,VIDDEC3_Cmd id,VIDDEC3_Dy
for (i = 0; i < DIM(c->decode_codec); i++) {
if (c->decode_codec[i] == codec) {
if (c->decode_callback[i].row_mode) {
- DEBUG("Check codec 0x%x", codec);
- c->decode_callback[i].dataSyncHandle = codec;
- c->decode_callback[i].mpu_crash_indication = FALSE;
- dynParams->putDataFxn = (XDM_DataSyncPutFxn) H264D_PutDataFxn;
- dynParams->putDataHandle = codec;
+ DEBUG("Check codec 0x%x control id %d", codec, id);
+ if (id == XDM_SETPARAMS) {
+ c->decode_callback[i].dataSyncHandle = codec;
+ c->decode_callback[i].mpu_crash_indication = FALSE;
+ dynParams->putDataFxn = (XDM_DataSyncPutFxn) H264D_PutDataFxn;
+ dynParams->putDataHandle = codec;
+ }
}
}
}
@@ -361,6 +369,34 @@ static XDAS_Int32 viddec3_control(VIDDEC3_Handle codec,VIDDEC3_Cmd id,VIDDEC3_Dy
return (VIDDEC3_control(codec, id, dynParams, status));
}
+static XDAS_Int32 viddec3_process(VIDDEC3_Handle codec, XDM2_BufDesc *inBufs, XDM2_BufDesc *outBufs, VIDDEC3_InArgs *inArgs, VIDDEC3_OutArgs *outArgs)
+{
+ Client* c;
+ XDAS_Int32 ret;
+
+ c = get_client_instance((Uint32) codec);
+ if (c) {
+ int i;
+ for (i = 0; i < DIM(c->decode_codec); i++) {
+ if (c->decode_codec[i] == codec) {
+ if (c->decode_callback[i].row_mode) {
+ DEBUG("Codec 0x%x", codec);
+ c->decode_callback[i].codec_request = 0;
+ c->decode_callback[i].putdata_toclient = 0;
+ c->decode_callback[i].putData_endprocess = 0;
+ ret = VIDDEC3_process(codec, inBufs, outBufs, inArgs, outArgs);
+
+ // Set flag and signal for put_DataFxn to return.
+ c->decode_callback[i].putData_endprocess = 1;
+ pthread_cond_signal(&(c->decode_callback[i].synch_callback));
+ return (ret);
+ }
+ }
+ }
+ }
+ return (VIDDEC3_process(codec, inBufs, outBufs, inArgs, outArgs));
+}
+
static int videnc2_reloc(VIDENC2_Handle handle, uint8_t *ptr, uint32_t len)
{
return (-1); // Not implemented
if (c->decode_codec[i] == dataSyncHandle) {
pthread_mutex_lock(&(c->decode_callback[i].callback_mutex));
// Found the corresponding entry, check if IVA-HD has already called the callback (codec_request == 1).
- if (c->decode_callback[i].codec_request) {
+
+ if ((c->decode_callback[i].codec_request) && ((c->decode_callback[i].putdata_toclient) == 0)) {
DEBUG("Case#1 put_DataFxn is received while codec has requested first. c->decode_callback[%d].callback_mutex 0x%x",
i, c->decode_callback[i].callback_mutex);
DEBUG("Case#1 c->decode_callback[i].dataSyncDesc 0x%x dataSyncDesc 0x%x", c->decode_callback[i].dataSyncDesc, dataSyncDesc);
dataSyncDesc->varBlockSizesFlag = (c->decode_callback[i].dataSyncDesc)->varBlockSizesFlag;
dataSyncDesc->blockSizes = (c->decode_callback[i].dataSyncDesc)->blockSizes;
- DEBUG("signal the other thread H264D_PutDataFxn to continue");
+ (c->decode_callback[i].putdata_toclient)++;
+ pthread_mutex_unlock(&(c->decode_callback[i].callback_mutex));
+
+ dce_clean(dataSyncDesc);
+ return (0);
+ } else if ((c->decode_callback[i].codec_request) && (c->decode_callback[i].putdata_toclient)) {
+ // Check if put_data_toclient are set; Otherwise send the data to MPU.
+ DEBUG("MPU has received the earlier put_DataFxn from codec on 0x%x", c->decode_codec[i]);
+ (c->decode_callback[i].putdata_toclient)--;
+ DEBUG("Signal thread H264D_PutDataFxn to continue");
pthread_cond_signal(&(c->decode_callback[i].synch_callback));
+ // After signaling H264D_PutDataFxn, it needs to wait for the new data to be returned by codec.
+ }
+
+ // We received put_DataFxn from client, need to wait for data from codec through H264D_PutDataFxn before continuing
+ c->decode_callback[i].putdata_ready = 1;
+ DEBUG("Case#2 put_DataFxn is received. Wait for H264D_PutDataFxn to come; set putdata_ready = 1 c->decode_callback[%d].callback_mutex 0x%x", i, c->decode_callback[i].callback_mutex);
+ DEBUG("Case#2 c->decode_callback[i].dataSyncDesc 0x%x dataSyncDesc 0x%x", c->decode_callback[i].dataSyncDesc, dataSyncDesc);
+ pthread_cond_wait(&(c->decode_callback[i].synch_callback), &(c->decode_callback[i].callback_mutex));
+
+ DEBUG("put_DataFxn FINALLY gets H264D_PutDataFxn, and the data has been provided, continue.");
+ // Signal is received; check if it is from VIDDEC3_process or from H264D_PutDataFxn
+ if (c->decode_callback[i].putData_endprocess ) {
+ dataSyncDesc->numBlocks = 0; // To be returned to MPU side which will be ignored.
} else {
- // We received put_DataFxn from libdce/client, need to hold it until the data
- // is provided by codec through H264D_PutDataFxn before continuing.
- c->decode_callback[i].putdata_ready = 1;
- DEBUG("Case#2 put_DataFxn is received but codec has not requested H264D_PutDataFxn. Wait cond. c->decode_callback[%d].callback_mutex 0x%x", i, c->decode_callback[i].callback_mutex);
- DEBUG("Case#2 c->decode_callback[i].dataSyncDesc 0x%x dataSyncDesc 0x%x", c->decode_callback[i].dataSyncDesc, dataSyncDesc);
- pthread_cond_wait(&(c->decode_callback[i].synch_callback), &(c->decode_callback[i].callback_mutex));
- DEBUG("put_DataFxn FINALLY gets H264D_PutDataFxn, and the data has been provided, continue.");
// Copy the local structure as H264D_PutDataFxn has already stored codec partial decoded data to be sent to MPU side.
dataSyncDesc->size = (c->decode_callback[i].dataSyncDesc)->size;
dataSyncDesc->scatteredBlocksFlag = (c->decode_callback[i].dataSyncDesc)->scatteredBlocksFlag;
dataSyncDesc->numBlocks = (c->decode_callback[i].dataSyncDesc)->numBlocks;
dataSyncDesc->varBlockSizesFlag = (c->decode_callback[i].dataSyncDesc)->varBlockSizesFlag;
dataSyncDesc->blockSizes = (c->decode_callback[i].dataSyncDesc)->blockSizes;
-
- c->decode_callback[i].putdata_ready = 0;
- // After resetting putdata_ready to 0, this function will return to MPU; we can let the codec callback to continue for more data.
- DEBUG("From client dataSyncDesc->size %d ", dataSyncDesc->size);
- DEBUG("From client dataSyncDesc->scatteredBlocksFlag %d ", dataSyncDesc->scatteredBlocksFlag);
- DEBUG("From client dataSyncDesc->baseAddr %d ", dataSyncDesc->baseAddr);
- DEBUG("From client dataSyncDesc->numBlocks %d ", dataSyncDesc->numBlocks);
- DEBUG("From client dataSyncDesc->varBlockSizesFlag %d ", dataSyncDesc->varBlockSizesFlag);
- DEBUG("From client dataSyncDesc->blockSizes %d ", dataSyncDesc->blockSizes);
}
+ c->decode_callback[i].putdata_ready = 0;
+ // After resetting putdata_ready to 0, this function will return to MPU
+ DEBUG("From client dataSyncDesc->size %d ", dataSyncDesc->size);
+ DEBUG("From client dataSyncDesc->scatteredBlocksFlag %d ", dataSyncDesc->scatteredBlocksFlag);
+ DEBUG("From client dataSyncDesc->baseAddr %d ", dataSyncDesc->baseAddr);
+ DEBUG("From client dataSyncDesc->numBlocks %d ", dataSyncDesc->numBlocks);
+ DEBUG("From client dataSyncDesc->varBlockSizesFlag %d ", dataSyncDesc->varBlockSizesFlag);
+ DEBUG("From client dataSyncDesc->blockSizes %d ", dataSyncDesc->blockSizes);
+
+ (c->decode_callback[i].putdata_toclient)++;
pthread_mutex_unlock(&(c->decode_callback[i].callback_mutex));
}
}
/* For low latency instance, need to trigger the flag to callback function so that it will return full numblock*/
for( i = 0; i < DIM(c->decode_codec); i++ ) {
- //DEBUG("c->decode_callback[%d].row_mode %d", i, c->decode_callback[i].row_mode);
if (c->decode_callback[i].row_mode) {
DEBUG("Setting c->decode_callback[%d].mpu_crash_indication = TRUE c->decode_codec[%d].callback_mutex 0x%x", i, i, c->decode_callback[i].callback_mutex);
c->decode_callback[i].mpu_crash_indication = TRUE;
}
for( i = 0; i < DIM(c->encode_codec); i++ ) {
- //DEBUG("c->encode_callback[%d].row_mode %d", i, c->encode_callback[i].row_mode);
if (c->encode_callback[i].row_mode) {
DEBUG("Setting c->encode_callback[%d].mpu_crash_indication = TRUE c->encode_codec[%d].callback_mutex 0x%x", i, i, c->encode_callback[i].callback_mutex);
c->encode_callback[i].mpu_crash_indication = TRUE;
} else {
c->encode_callback[i].codec_request = 1;
+ DEBUG("H264E_GetDataFxn wait Case#1");
// Wait until get_DataFxn is received from MPU client side. Need the information to be passed to codec as currently not available.
pthread_cond_wait(&(c->encode_callback[i].synch_callback), &(c->encode_callback[i].callback_mutex));
if (c->decode_codec[i] == dataSyncHandle) {
pthread_mutex_lock(&(c->decode_callback[i].callback_mutex));
DEBUG("H264D_PutDataFxn dataSyncHandle 0x%x c->decode_codec[%d].callback_mutex 0x%x", dataSyncHandle, i, c->decode_callback[i].callback_mutex);
- // Should be okay to save the data from IVA-HD codec into local structure for put_DataFxn to pick up.
+ c->decode_callback[i].codec_request = 1;
+ // Save the data from IVA-HD codec into local structure for put_DataFxn to pick up.
if (dataSyncHandle == c->decode_callback[i].dataSyncHandle) {
(c->decode_callback[i].dataSyncDesc)->size = dataSyncDesc->size;
(c->decode_callback[i].dataSyncDesc)->scatteredBlocksFlag = dataSyncDesc->scatteredBlocksFlag;
// After storing the data from codec, send thread signal conditional for put_DataFxn to continue passing the codec data to MPU.
pthread_cond_signal(&(c->decode_callback[i].synch_callback));
+
+ DEBUG("H264D_PutDataFxn Case#2 wait on pthread_cond_wait");
+ // After signal put_DataFxn, needs to wait for put_DataFxn return from A15 before returning to codec.
+ pthread_cond_wait(&(c->decode_callback[i].synch_callback), &(c->decode_callback[i].callback_mutex));
} else {
- c->decode_callback[i].codec_request = 1;
DEBUG("H264D_PutDataFxn Case#1 wait on pthread_cond_wait c->decode_codec[%d].callback_mutex 0x%x", i, c->decode_callback[i].callback_mutex);
pthread_cond_wait(&(c->decode_callback[i].synch_callback), &(c->decode_callback[i].callback_mutex));
- c->decode_callback[i].codec_request = 0;
}
}
+ c->decode_callback[i].codec_request = 0;
pthread_mutex_unlock(&(c->decode_callback[i].callback_mutex));
}
}