RVC: Handling M4 message for reverse gear detection master
authorBuddy Liong <a0270631@ti.com>
Tue, 31 Jan 2017 23:01:08 +0000 (17:01 -0600)
committerBuddy Liong <a0270631@ti.com>
Tue, 31 Jan 2017 23:01:08 +0000 (17:01 -0600)
commitd28fce4df2675daf148f8d758b283c88a4f698aa
treeb4d0eabb85225a520f4b14632961f0904d8b4d2f
parent0ec98f95028e6640e38e95e55edfdf5eb9514dca
RVC: Handling M4 message for reverse gear detection

When M4 detects reverse gear, it will send messageQ to HOST (A15).
The message will be used by A15 to set the kernel panic timeout
value. When reverse gear (RVC) is up, then panic timeout should be
set to 0 sec meaning when Android kernel crash, there should not be
recovery as it will affect RVC.
When no reverse gear (RVC is stop), then panic timeout can be set
to any value (default is 5 sec) meaning when Android kernel crash,
recovery should be triggered within the panic timeout value.

Signed-off-by: Buddy Liong <a0270631@ti.com>
appA15HeartBeatHost.c
appA15HeartBeatHost.h