66aa794916ca2737509b6bef8ff13125fd415502
[jacinto-ai/caffe-jacinto.git] / INSTALL.md
1 # Installation
3 To build and test Caffe do
5     make
6     make test
7     make runtest
9 You may need to minimally tinker with paths in `Makefile.config` and maybe the
10 `Makefile` itself.
12 Note that building and running CPU-only works, but GPU tests will naturally
13 fail.
15 We mostly used Ubuntu 12.04 for development, and here we describe the
16 step-to-step guide on installing Caffe on Ubuntu.
18 ## Prerequisites
20 * CUDA
21 * Boost
22 * MKL (but see the boost-eigen branch for a boost/Eigen3 port)
23 * OpenCV
24 * glog, gflags, protobuf, leveldb, snappy
25 * For the Python wrapper: python, numpy (>= 1.7 preferred), and boost_python
26 * For the Matlab wrapper: Matlab with mex
28 Caffe requires the CUDA NVCC compiler to compile its GPU code. To install CUDA, go to the [NVidia CUDA website](https://developer.nvidia.com/cuda-downloads) and follow installation instructions there. Caffe is verified to compile with both CUDA 5.0 and 5.5.
30 Caffe also needs Intel MKL as the backend of its matrix computation and vectorized computations. We are in the process of removing MKL dependency, but for now you will need to have an MKL installation. You can obtain a [trial license](http://software.intel.com/en-us/intel-mkl) or an [academic license](http://software.intel.com/en-us/intel-education-offerings) (if you are a student).
32 If you would like to compile the Python wrapper, you will need to install python, numpy and boost_python. You can either compile them from scratch or use a pre-packaged solution like [Anaconda](https://store.continuum.io/cshop/anaconda/) or [Enthought Canopy](https://www.enthought.com/products/canopy/). Note that if you use the Ubuntu default python, you will need to apt-install the `python-dev` package to have the python headers.
34 If you would like to compile the Matlab wrapper, you will need to install Matlab.
36 You will also need other packages, most of which can be installed via apt-get using:
38     sudo apt-get install libprotobuf-dev libleveldb-dev libsnappy-dev libopencv-dev libboost-all-dev
40 The only exception being the google logging library, which does not exist in the Ubuntu 12.04 repository. To install it, do:
42     wget https://google-glog.googlecode.com/files/glog-0.3.3.tar.gz
43     tar zxvf glog-0.3.3.tar.gz
44     ./configure
45     make && make install
47 After setting all the prerequisites, you should modify the `Makefile.config` file and change the paths to those on your computer.
49 ## Compilation
51 After installing the prerequisites, simply do `make all` to compile Caffe. If you would like to compile the Python and Matlab wrappers, do
53     make pycaffe
54     make matcaffe
56 Optionally, you can run `make distribute` to create a `build` directory that contains all the necessary files, including the headers, compiled shared libraries, and binary files that you can distribute over different machines.
58 To use Caffe with python, you will need to add `/path/to/caffe/python` or `/path/to/caffe/build/python` to your `PYTHONPATH`.
60 Now that you have compiled Caffe, check out the [MNIST demo](mnist.html) and the pretrained [ImageNet example](imagenet.html).