1 // Copyright 2013 Yangqing Jia
3 package caffe;
5 message BlobProto {
6 optional int32 num = 1 [default = 0];
7 optional int32 channels = 2 [default = 0];
8 optional int32 height = 3 [default = 0];
9 optional int32 width = 4 [default = 0];
10 repeated float data = 5 [packed=true];
11 repeated float diff = 6 [packed=true];
12 }
14 message Datum {
15 optional int32 channels = 1;
16 optional int32 height = 2;
17 optional int32 width = 3;
18 // the actual image data, in bytes
19 optional bytes data = 4;
20 optional int32 label = 5;
21 }
23 message FillerParameter {
24 // The filler type. In default we will set it to Gaussian for easy
25 // debugging.
26 optional string type = 1 [default = 'gaussian'];
27 optional float value = 2 [default = 0]; // the value in constant filler
28 optional float min = 3 [default = 0]; // the min value in uniform filler
29 optional float max = 4 [default = 1]; // the max value in uniform filler
30 optional float mean = 5 [default = 0]; // the mean value in gaussian filler
31 optional float std = 6 [default = 1]; // the std value in gaussian filler
32 }
34 message LayerParameter {
35 optional string name = 1; // the layer name
36 optional string type = 2; // the string to specify the layer type
38 // Parameters to specify layers with inner products.
39 optional uint32 num_output = 3; // The number of outputs for the layer
40 optional bool biasterm = 4 [default = true]; // whether to have bias terms
41 optional FillerParameter weight_filler = 5; // The filler for the weight
42 optional FillerParameter bias_filler = 6; // The filler for the bias
44 optional uint32 pad = 7 [default = 0]; // The padding size
45 optional uint32 kernelsize = 8; // The kernel size
46 optional uint32 group = 9 [default = 1]; // The group size for group conv
47 optional uint32 stride = 10 [default = 1]; // The stride
48 enum PoolMethod {
49 MAX = 0;
50 AVE = 1;
51 }
52 optional PoolMethod pool = 11 [default = MAX]; // The pooling method
53 optional float dropout_ratio = 12 [default = 0.5]; // dropout ratio
55 optional uint32 local_size = 13 [default = 5]; // for local response norm
56 optional float alpha = 14 [default = 1.]; // for local response norm
57 optional float beta = 15 [default = 0.75]; // for local response norm
59 // For data layers, specify the data source
60 optional string source = 16;
61 // For datay layers, specify the batch size.
62 optional uint32 batchsize = 17;
64 // The blobs containing the numeric parameters of the layer
65 repeated BlobProto blobs = 50;
66 }
68 message LayerConnection {
69 optional LayerParameter layer = 1; // the layer parameter
70 repeated string bottom = 2; // the name of the bottom blobs
71 repeated string top = 3; // the name of the top blobs
72 }
74 message NetParameter {
75 optional string name = 1; // consider giving the network a name
76 repeated LayerConnection layers = 2; // a bunch of layers.
77 repeated string input = 3; // The input to the network
78 }
80 message SolverParameter {
81 optional float base_lr = 1; // The base learning rate
82 optional int32 display = 2; // display options. 0 = no display
83 optional int32 max_iter = 3; // the maximum number of iterations
84 optional int32 snapshot = 4; // The snapshot interval
85 optional string lr_policy = 5; // The learning rate decay policy.
86 optional float min_lr = 6 [default = 0]; // The mininum learning rate
87 optional float max_lr = 7 [default = 1e10]; // The maximum learning rate
88 optional float gamma = 8; // The parameter to compute the learning rate.
89 optional float power = 9; // The parameter to compute the learning rate.
90 optional float momentum = 10; // The momentum value.
92 optional string snapshot_prefix = 11; // The prefix for the snapshot.
93 }