// Copyright 2013 Yangqing Jia #ifndef CAFFE_COMMON_HPP_ #define CAFFE_COMMON_HPP_ #include #include #include #include // cuda driver types #include #include #include // various checks for different function calls. #define CUDA_CHECK(condition) CHECK_EQ((condition), cudaSuccess) #define CUBLAS_CHECK(condition) CHECK_EQ((condition), CUBLAS_STATUS_SUCCESS) #define CURAND_CHECK(condition) CHECK_EQ((condition), CURAND_STATUS_SUCCESS) #define VSL_CHECK(condition) CHECK_EQ((condition), VSL_STATUS_OK) // After a kernel is executed, this will check the error and if there is one, // exit loudly. #define CUDA_POST_KERNEL_CHECK \ if (cudaSuccess != cudaPeekAtLastError()) \ LOG(FATAL) << "Cuda kernel failed. Error: " \ << cudaGetErrorString(cudaPeekAtLastError()) // Disable the copy and assignment operator for a class. #define DISABLE_COPY_AND_ASSIGN(classname) \ private:\ classname(const classname&);\ classname& operator=(const classname&) // Instantiate a class with float and double specifications. #define INSTANTIATE_CLASS(classname) \ template class classname; \ template class classname // A simple macro to mark codes that are not implemented, so that when the code // is executed we will see a fatal log. #define NOT_IMPLEMENTED LOG(FATAL) << "Not Implemented Yet" namespace caffe { // We will use the boost shared_ptr instead of the new C++11 one mainly // because cuda does not work (at least now) well with C++11 features. using boost::shared_ptr; // We will use 1024 threads per block, which requires cuda sm_2x or above. const int CAFFE_CUDA_NUM_THREADS = 1024; inline int CAFFE_GET_BLOCKS(const int N) { return (N + CAFFE_CUDA_NUM_THREADS - 1) / CAFFE_CUDA_NUM_THREADS; } // A singleton class to hold common caffe stuff, such as the handler that // caffe is going to use for cublas, curand, etc. class Caffe { public: ~Caffe(); inline static Caffe& Get() { if (!singleton_.get()) { singleton_.reset(new Caffe()); } return *singleton_; } enum Brew { CPU, GPU }; enum Phase { TRAIN, TEST }; // The getters for the variables. // Returns the cublas handle. inline static cublasHandle_t cublas_handle() { return Get().cublas_handle_; } // Returns the curand generator. inline static curandGenerator_t curand_generator() { return Get().curand_generator_; } // Returns the MKL random stream. inline static VSLStreamStatePtr vsl_stream() { return Get().vsl_stream_; } // Returns the mode: running on CPU or GPU. inline static Brew mode() { return Get().mode_; } // Returns the phase: TRAIN or TEST. inline static Phase phase() { return Get().phase_; } // The setters for the variables // Sets the mode. It is recommended that you don't change the mode halfway // into the program since that may cause allocation of pinned memory being // freed in a non-pinned way, which may cause problems - I haven't verified // it personally but better to note it here in the header file. inline static void set_mode(Brew mode) { Get().mode_ = mode; } // Sets the phase. inline static void set_phase(Phase phase) { Get().phase_ = phase; } // Sets the random seed of both MKL and curand static void set_random_seed(const unsigned int seed); // Sets the device. Since we have cublas and curand stuff, set device also // requires us to reset those values. static void SetDevice(const int device_id); // Prints the current GPU status. static void DeviceQuery(); protected: cublasHandle_t cublas_handle_; curandGenerator_t curand_generator_; VSLStreamStatePtr vsl_stream_; Brew mode_; Phase phase_; static shared_ptr singleton_; private: // The private constructor to avoid duplicate instantiation. Caffe(); DISABLE_COPY_AND_ASSIGN(Caffe); }; } // namespace caffe #endif // CAFFE_COMMON_HPP_