// Copyright 2013 Yangqing Jia package caffe; message BlobProto { optional int32 num = 1 [default = 0]; optional int32 channels = 2 [default = 0]; optional int32 height = 3 [default = 0]; optional int32 width = 4 [default = 0]; repeated float data = 5 [packed=true]; repeated float diff = 6 [packed=true]; } message Datum { optional int32 channels = 1; optional int32 height = 2; optional int32 width = 3; // the actual image data, in bytes optional bytes data = 4; optional int32 label = 5; } message FillerParameter { // The filler type. In default we will set it to Gaussian for easy // debugging. optional string type = 1 [default = 'gaussian']; optional float value = 2 [default = 0]; // the value in constant filler optional float min = 3 [default = 0]; // the min value in uniform filler optional float max = 4 [default = 1]; // the max value in uniform filler optional float mean = 5 [default = 0]; // the mean value in gaussian filler optional float std = 6 [default = 1]; // the std value in gaussian filler } message LayerParameter { optional string name = 1; // the layer name optional string type = 2; // the string to specify the layer type // Parameters to specify layers with inner products. optional uint32 num_output = 3; // The number of outputs for the layer optional bool biasterm = 4 [default = true]; // whether to have bias terms optional FillerParameter weight_filler = 5; // The filler for the weight optional FillerParameter bias_filler = 6; // The filler for the bias optional uint32 pad = 7 [default = 0]; // The padding size optional uint32 kernelsize = 8; // The kernel size optional uint32 group = 9 [default = 1]; // The group size for group conv optional uint32 stride = 10 [default = 1]; // The stride enum PoolMethod { MAX = 0; AVE = 1; } optional PoolMethod pool = 11 [default = MAX]; // The pooling method optional float dropout_ratio = 12 [default = 0.5]; // dropout ratio optional uint32 local_size = 13 [default = 5]; // for local response norm optional float alpha = 14 [default = 1.]; // for local response norm optional float beta = 15 [default = 0.75]; // for local response norm // For data layers, specify the data source optional string source = 16; // For datay layers, specify the batch size. optional uint32 batchsize = 17; // The blobs containing the numeric parameters of the layer repeated BlobProto blobs = 50; } message LayerConnection { optional LayerParameter layer = 1; // the layer parameter repeated string bottom = 2; // the name of the bottom blobs repeated string top = 3; // the name of the top blobs } message NetParameter { optional string name = 1; // consider giving the network a name repeated LayerConnection layers = 2; // a bunch of layers. repeated string bottom = 3; // The input to the network repeated string top = 4; // The output of the network. } message SolverParameter { optional float base_lr = 1; // The base learning rate optional int32 display = 2; // display options. 0 = no display optional int32 max_iter = 3; // the maximum number of iterations optional int32 snapshot = 4; // The snapshot interval optional string lr_policy = 5; // The learning rate decay policy. optional float min_lr = 6 [default = 0]; // The mininum learning rate optional float max_lr = 7 [default = 1e10]; // The maximum learning rate optional float gamma = 8; // The parameter to compute the learning rate. optional float power = 9; // The parameter to compute the learning rate. optional float momentum = 10; // The momentum value. }