diff --git a/.travis.yml b/.travis.yml
index 37864c16423786d9b73db99800a00b4d481c233c..6478c866904cdd234193d4b53e27b29af1361ffe 100644 (file)
--- a/.travis.yml
+++ b/.travis.yml
-language: cpp
-
-# Cache Ubuntu apt packages.
-cache: apt
+dist: trusty
+sudo: required
-compiler:
- - gcc
-# Disable clang build: doesn't seem to work on Linux.
-# (@jeffdonahue: Travis buildbot's failure behavior is similar to what I see
-# building on Linux.)
-# - clang
+language: cpp
+compiler: gcc
+
+env:
+ global:
+ - NUM_THREADS=8
+ matrix:
+ # Use a build matrix to test many builds in parallel
+ # envvar defaults:
+ # WITH_CMAKE: false
+ # WITH_PYTHON3: false
+ # WITH_CUDA: const true since v0.17
+ # WITH_CUDNN: false
+ - BUILD_NAME="default-make"
+# - BUILD_NAME="python3-make" WITH_PYTHON3=true
+ - BUILD_NAME="cudnn-make" WITH_CUDNN=true
+
+ - BUILD_NAME="default-cmake" WITH_CMAKE=true
+ - BUILD_NAME="python3-cmake" WITH_CMAKE=true WITH_PYTHON3=true
+ - BUILD_NAME="cudnn-cmake" WITH_CMAKE=true WITH_CUDNN=true
+ - BUILD_NAME="cudnn-python3-cmake" WITH_CMAKE=true WITH_CUDNN=true WITH_PYTHON3=true
+
+cache:
+ apt: true
-
before_install:
- - echo $LANG
- - echo $LC_ALL
- - sudo add-apt-repository ppa:ubuntu-sdk-team/ppa -y
- - sudo apt-get -y update
- - sudo apt-get -y install wget git curl python-dev python-numpy libprotobuf-dev libleveldb-dev libsnappy-dev libopencv-dev libboost-all-dev libhdf5-serial-dev protobuf-compiler libatlas-dev libatlas-base-dev bc cmake
+ - source ./scripts/travis/defaults.sh
install:
- - wget https://google-glog.googlecode.com/files/glog-0.3.3.tar.gz -O /tmp/glog-0.3.3.tar.gz && tar -C /tmp -xzvf /tmp/glog-0.3.3.tar.gz && rm /tmp/glog-0.3.3.tar.gz
- - cd /tmp/glog-0.3.3 && ./configure && make -j4 && sudo make install -j4 && cd -
- - wget https://github.com/schuhschuh/gflags/archive/master.zip -O /tmp/gflags-master.zip && pushd /tmp/ && unzip gflags-master.zip && cd gflags-master && mkdir build && cd build && export CXXFLAGS="-fPIC" && cmake .. && make VERBOSE=1 && sudo make install && popd
- - curl http://developer.download.nvidia.com/compute/cuda/repos/ubuntu1204/x86_64/cuda-repo-ubuntu1204_6.0-37_amd64.deb -o /tmp/cuda_install.deb && sudo dpkg -i /tmp/cuda_install.deb && rm /tmp/cuda_install.deb
- - sudo apt-get -y update
- # Install the minimal CUDA subpackages required to test Caffe build.
- # For a full CUDA installation, add 'cuda' to the list of packages.
- - sudo apt-get -y install cuda-core-6-0 cuda-extra-libs-6-0
- # Create CUDA symlink at /usr/local/cuda
- # (This would normally be created by the CUDA installer, but we create it
- # manually since we did a partial installation.)
- - sudo ln -s /usr/local/cuda-6.0 /usr/local/cuda
- - curl https://gitorious.org/mdb/mdb/archive/7f038d0f15bec57b4c07aa3f31cd5564c88a1897.tar.gz -o /tmp/mdb.tar.gz && tar -C /tmp -xzvf /tmp/mdb.tar.gz && rm /tmp/mdb.tar.gz
- - cd /tmp/mdb-mdb/libraries/liblmdb/ && make -j4 && sudo make install -j4 && cd -
+ - sudo -E ./scripts/travis/install-deps.sh
+ - ./scripts/travis/setup-venv.sh ~/venv
+ - source ~/venv/bin/activate
+ - ./scripts/travis/install-python-deps.sh
before_script:
- - mv Makefile.config.example Makefile.config
- - export LD_LIBRARY_PATH=$LD_LIBRARY_PATH:/usr/local/lib
- - export NUM_THREADS=4
+ - ./scripts/travis/configure.sh
script:
- # CMake build.
- - mkdir build
- - cd build
- ## CPU-GPU: build only.
- - cmake -DBUILD_PYTHON=ON -DBUILD_EXAMPLES=ON -DCMAKE_BUILD_TYPE=Release ..
- - make --keep-going --jobs=$NUM_THREADS
- - make clean && rm -rf *
- ## CPU-only: comprehensive
- - cmake -DBUILD_PYTHON=ON -DBUILD_EXAMPLES=ON -DCMAKE_BUILD_TYPE=Release -DCPU_ONLY=ON ..
- - make --keep-going --jobs=$NUM_THREADS
- - make runtest --keep-going --jobs=$NUM_THREADS
- - make lint --jobs=$NUM_THREADS
- - make clean && rm -rf *
- ## Cleaning
- - cd ..
- - rm -r build
-
- # Make build
- ## CPU-GPU: build only.
- - export CPU_ONLY=0
- - make --keep-going --jobs=$NUM_THREADS all
- - make clean
- ## CPU-only: comprehensive.
- - export CPU_ONLY=1
- - make --keep-going --jobs=$NUM_THREADS all test warn lint
- - make runtest
- - make --jobs=$NUM_THREADS all
- - make --jobs=$NUM_THREADS test
- - make --jobs=$NUM_THREADS warn
- - make --jobs=$NUM_THREADS lint
- - make --jobs=$NUM_THREADS pycaffe
+ - ./scripts/travis/build.sh
+ - ./scripts/travis/test.sh
notifications:
# Emails are sent to the committer's git-configured email address by default,