diff --git a/INSTALL.md b/INSTALL.md
index 745f0164c564c44b2204bdf1428615fdacb726bb..f20131cf5560a181649faa0ff537eefebe2cdb88 100644 (file)
--- a/INSTALL.md
+++ b/INSTALL.md
```
* In the Makefile.confg, make the following changes.<br>
-- Since the default opencv version in Anaconda is now 3.x, uncomment the line OPENCV_VERSION := 3<br>
- -- Add additional include folders to the line INCLUDE_DIRS. We need to add the full paths to the directories envs/caffe/include and envs/caffe/include/python2.7 located inside the Anaconda installation.<br>
+ -- Add additional include folders to the line INCLUDE_DIRS. We need to add the full paths to the directories envs/caffe/include envs/caffe/include/python2.7 and envs/caffe/lib/python2.7/site-packages/numpy/core/include located inside the Anaconda installation.<br>
-- Add additional lib folders to the line LIBRARY_DIRS. We need to add the full paths to the directories envs/caffe/lib and envs/caffe/lib/python2.7 located inside the Anaconda installation.<br>
+ * At import time or runtime, if there is an issue in finding shared objects (.so files), we may need to specify additional paths into LD_LIBRARY_PATH. Note: This is required only if there is an issue in finding a .so file. The exact path that we may need to add may also be different.
+ export LD_LIBRARY_PATH=$LD_LIBRARY_PATH:/user/a0393608/files/apps/anaconda3/envs/caffe/lib
+
* After these installations, do cmake and make as explained before.<br>
7. <b>Appendix: Caffe's original instructions </b>