doc update
[jacinto-ai/caffe-jacinto.git] / Makefile.config
index 111bee9928077e97806c231575979f71714084fd..4dff33a559b0fc6837236c8003877bd915737e7c 100644 (file)
-# define third-party library paths
-# CHANGE YOUR CUDA PATH IF IT IS NOT THIS
+## Refer to http://caffe.berkeleyvision.org/installation.html
+# Contributions simplifying and improving our build system are welcome!
+
+# cuDNN acceleration switch (uncomment to build with cuDNN).
+# cuDNN version 6 or higher is required.
+USE_CUDNN := 1
+
+# NCCL acceleration switch (uncomment to build with NCCL)
+# See https://github.com/NVIDIA/nccl
+USE_NCCL := 1
+
+# CPU-only switch (uncomment to build without GPU support).
+# Disables FP16 support.
+# CPU_ONLY := 1
+# Builds tests with 16 bit float support in addition to 32 and 64 bit.
+# TEST_FP16 := 1
+
+# uncomment to disable IO dependencies and corresponding data layers
+# USE_OPENCV := 0
+# USE_LEVELDB := 0
+# USE_LMDB := 0
+
+# Uncomment if you're using OpenCV 3
+# OPENCV_VERSION := 3
+
+# To customize your choice of compiler, uncomment and set the following.
+# N.B. the default for Linux is g++ and the default for OSX is clang++
+# CUSTOM_CXX := g++
+
+# CUDA directory contains bin/ and lib/ directories that we need.
 CUDA_DIR := /usr/local/cuda
-# CHANGE YOUR CUDA ARCH IF IT IS NOT THIS
-CUDA_ARCH := -gencode arch=compute_20,code=sm_20 \
-    -gencode arch=compute_20,code=sm_21 \
-    -gencode arch=compute_30,code=sm_30 \
-    -gencode arch=compute_35,code=sm_35
-# CHANGE YOUR MKL PATH IF IT IS NOT THIS
-MKL_DIR := /opt/intel/mkl
-# CHANGE YOUR MATLAB PATH IF IT IS NOT THIS
-# your mex binary should be located at $(MATLAB_DIR)/bin/mex
-MATLAB_DIR := /usr/local
-# PUT ALL OTHER INCLUDE AND LIB DIRECTORIES HERE
-INCLUDE_DIRS := /usr/local/include /usr/include/python2.7 \
-    /usr/local/lib/python2.7/dist-packages/numpy/core/include
-LIBRARY_DIRS := /usr/lib /usr/local/lib
-
-# DEFINE THE CXX PATH
-CXX=/usr/bin/g++
-
-BUILD_DIR=build
-DISTRIBUTE_DIR=distribute
+# On Ubuntu 14.04, if cuda tools are installed via
+# "sudo apt-get install nvidia-cuda-toolkit" then use this instead:
+# CUDA_DIR := /usr
+
+# CUDA architecture setting: going with all of them.
+CUDA_ARCH :=   -gencode arch=compute_50,code=sm_50 \
+               -gencode arch=compute_52,code=sm_52 \
+               -gencode arch=compute_60,code=sm_60 \
+               -gencode arch=compute_61,code=sm_61 \
+               -gencode arch=compute_61,code=compute_61
+
+# BLAS choice:
+# atlas for ATLAS
+# mkl for MKL
+# open for OpenBlas - default, see https://github.com/xianyi/OpenBLAS
+BLAS := open
+# Custom (MKL/ATLAS/OpenBLAS) include and lib directories.
+BLAS_INCLUDE := /opt/OpenBLAS/include/
+BLAS_LIB := /opt/OpenBLAS/lib/
+
+# Homebrew puts openblas in a directory that is not on the standard search path
+# BLAS_INCLUDE := $(shell brew --prefix openblas)/include
+# BLAS_LIB := $(shell brew --prefix openblas)/lib
+
+# This is required only if you will compile the matlab interface.
+# MATLAB directory should contain the mex binary in /bin.
+# MATLAB_DIR := /usr/local
+# MATLAB_DIR := /Applications/MATLAB_R2012b.app
+
+# NOTE: this is required only if you will compile the python interface.
+# We need to be able to find Python.h and numpy/arrayobject.h.
+PYTHON_INCLUDE := /usr/include/python2.7 \
+               /usr/lib/python2.7/dist-packages/numpy/core/include
+# Anaconda Python distribution is quite popular. Include path:
+# Verify anaconda location, sometimes it's in root.
+# ANACONDA_HOME := $(HOME)/anaconda
+# PYTHON_INCLUDE := $(ANACONDA_HOME)/include \
+               # $(ANACONDA_HOME)/include/python2.7 \
+               # $(ANACONDA_HOME)/lib/python2.7/site-packages/numpy/core/include \
+
+# Uncomment to use Python 3 (default is Python 2)
+# PYTHON_LIBRARIES := boost_python3 python3.5m
+# PYTHON_INCLUDE := /usr/include/python3.5m \
+#                 /usr/lib/python3.5/dist-packages/numpy/core/include
+
+# We need to be able to find libpythonX.X.so or .dylib.
+PYTHON_LIB := /usr/lib
+# PYTHON_LIB := $(ANACONDA_HOME)/lib
+
+# Homebrew installs numpy in a non standard path (keg only)
+# PYTHON_INCLUDE += $(dir $(shell python -c 'import numpy.core; print(numpy.core.__file__)'))/include
+# PYTHON_LIB += $(shell brew --prefix numpy)/lib
+
+# Uncomment to support layers written in Python (will link against Python libs)
+WITH_PYTHON_LAYER := 1
+
+# Whatever else you find you need goes here.
+INCLUDE_DIRS := $(PYTHON_INCLUDE) /usr/local/include /usr/include/hdf5/serial
+LIBRARY_DIRS := $(PYTHON_LIB) /usr/local/lib /usr/lib /usr/lib/x86_64-linux-gnu/hdf5/serial
+
+# If Homebrew is installed at a non standard location (for example your home directory) and you use it for general dependencies
+# INCLUDE_DIRS += $(shell brew --prefix)/include
+# LIBRARY_DIRS += $(shell brew --prefix)/lib
+
+# Uncomment to use `pkg-config` to specify OpenCV library paths.
+# (Usually not necessary -- OpenCV libraries are normally installed in one of the above $LIBRARY_DIRS.)
+# USE_PKG_CONFIG := 1
+
+BUILD_DIR := build
+DISTRIBUTE_DIR := distribute
+
+# Uncomment for debugging. Does not work on OSX due to https://github.com/BVLC/caffe/issues/171
+# DEBUG := 1
+
+# The ID of the GPU that 'make runtest' will use to run unit tests.
+TEST_GPUID := 0
+
+# enable pretty build (comment to see full commands)
+Q ?= @
+
+# shared object suffix name to differentiate branches
+LIBRARY_NAME_SUFFIX := -nv