summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 7453bbf)
raw | patch | inline | side by side (parent: 7453bbf)
author | mhouston <mhouston@nvidia.com> | |
Tue, 18 Aug 2015 22:29:26 +0000 (15:29 -0700) | ||
committer | mhouston <mhouston@nvidia.com> | |
Tue, 18 Aug 2015 22:29:26 +0000 (15:29 -0700) |
docs/multigpu.md | patch | blob | history |
diff --git a/docs/multigpu.md b/docs/multigpu.md
index 4b20234741768b06b00356fc916bc3ae56b4ade8..01cfb8938b57d3105fd4d9f5721bd60772de685a 100644 (file)
--- a/docs/multigpu.md
+++ b/docs/multigpu.md
Current implementation has a "soft" assumption that the devices being used are homogeneous. In practice, any devices of the same general class should work together, but performance and total size is limited by the smallest device being used. e.g. if you combine a TitanX and a GTX980, peformance will be limited by the 980. Mixing vastly different levels of boards, e.g. Kepler and Fermi, is not supported.
+"nvidia-smi topo -m" will show you the connectivity matrix. You can do P2P through PCIe bridges, but not across socket level links at this time, e.g. across CPU sockets on a multi-socket motherboard.
+
# Scaling Performance
Performance is **heavily** dependent on the PCIe topology of the system, the configuration of the neural network you are training, and the speed of each of the layers. Systems like the DIGITS DevBox have an optimized PCIe topology (X99-E WS chipset). In general, scaling on 2 GPUs tends to be ~1.8X on average for networks like AlexNet, CaffeNet, VGG, GoogleNet. 4 GPUs begins to have falloff in scaling. Generally with "weak scaling" where the batchsize increases with the number of GPUs you will see 3.5x scaling or so. With "strong scaling", the system can become communication bound, especially with layer performance optimizations like those in [cuDNNv3](http://nvidia.com/cudnn), and you will likely see closer to mid 2.x scaling in performance. Networks that have heavy computation compared to the number of parameters tend to have the best scaling performance.
\ No newline at end of file