author | Evan Shelhamer <shelhamer@imaginarynumber.net> | |
Fri, 15 May 2015 01:42:02 +0000 (18:42 -0700) | ||
committer | Evan Shelhamer <shelhamer@imaginarynumber.net> | |
Fri, 15 May 2015 01:42:02 +0000 (18:42 -0700) |
Update docs for ND blobs (#1970) and layer type is a string (#1694)
1 | 2 | |||
---|---|---|---|---|
docs/tutorial/layers.md | patch | | diff1 | | diff2 | | blob | history |
diff --cc docs/tutorial/layers.md
index c4529e6afc08033212d7ee4c643ebafeee9baa69,74d236c1194313ad7bbde796472e6207b20f8007..ff2ee491244ec5691f4ed7eb80602539931a2921
+++ b/docs/tutorial/layers.md
#### Flattening
- The `FLATTEN` layer is a utility layer that flattens an input of shape `n * c * h * w` to a simple vector output of shape `n * (c*h*w) * 1 * 1`.
+ The `Flatten` layer is a utility layer that flattens an input of shape `n * c * h * w` to a simple vector output of shape `n * (c*h*w)`
+#### Reshape
+
+* Layer type: `Reshape`
+* Implementation: `./src/caffe/layers/reshape_layer.cpp`
+* Parameters (`ReshapeParameter reshape_param`)
+ - Optional: (also see detailed description below)
+ - `shape`
+
+* Input
+ - a single blob with arbitrary dimensions
+* Output
+ - the same blob, with modified dimensions, as specified by `reshape_param`
+
+* Sample
+
+ layer {
+ name: "reshape"
+ type: "Reshape"
+ bottom: "input"
+ top: "output"
+ reshape_param {
+ shape {
+ dim: 0 # copy the dimension from below
+ dim: 2
+ dim: 3
+ dim: -1 # infer it from the other dimensions
+ }
+ }
+ }
+
+The `Reshape` layer can be used to change the dimensions of its input, without changing its data. Just like the `Flatten` layer, only the dimensions are changed; no data is copied in the process.
+
+Output dimensions are specified by the `ReshapeParam` proto. Positive numbers are used directly, setting the corresponding dimension of the output blob. In addition, two special values are accepted for any of the target dimension values:
+
+* **0** means "copy the respective dimension of the bottom layer". That is, if the bottom has 2 as its 1st dimension, the top will have 2 as its 1st dimension as well, given `dim: 0` as the 1st target dimension.
+* **-1** stands for "infer this from the other dimensions". This behavior is similar to that of -1 in *numpy*'s or `[]` for *MATLAB*'s reshape: this dimension is calculated to keep the overall element count the same as in the bottom layer. At most one -1 can be used in a reshape operation.
+
+As another example, specifying `reshape_param { shape { dim: 0 dim: -1 } }` makes the layer behave in exactly the same way as the `Flatten` layer.
+
#### Concatenation
- * LayerType: `CONCAT`
+ * Layer type: `Concat`
* CPU implementation: `./src/caffe/layers/concat_layer.cpp`
* CUDA GPU implementation: `./src/caffe/layers/concat_layer.cu`
* Parameters (`ConcatParameter concat_param`)