[jacinto-ai/pytorch-jacinto-ai-devkit.git] / modules / pytorch_jacinto_ai / vision / datasets / kinetics.py
1 from .video_utils import VideoClips
2 from .utils import list_dir
3 from .folder import make_dataset
4 from .vision import VisionDataset
7 class Kinetics400(VisionDataset):
8 """
9 `Kinetics-400 <https://deepmind.com/research/open-source/open-source-datasets/kinetics/>`_
10 dataset.
12 Kinetics-400 is an action recognition video dataset.
13 This dataset consider every video as a collection of video clips of fixed size, specified
14 by ``frames_per_clip``, where the step in frames between each clip is given by
15 ``step_between_clips``.
17 To give an example, for 2 videos with 10 and 15 frames respectively, if ``frames_per_clip=5``
18 and ``step_between_clips=5``, the dataset size will be (2 + 3) = 5, where the first two
19 elements will come from video 1, and the next three elements from video 2.
20 Note that we drop clips which do not have exactly ``frames_per_clip`` elements, so not all
21 frames in a video might be present.
23 Internally, it uses a VideoClips object to handle clip creation.
25 Args:
26 root (string): Root directory of the Kinetics-400 Dataset.
27 frames_per_clip (int): number of frames in a clip
28 step_between_clips (int): number of frames between each clip
29 transform (callable, optional): A function/transform that takes in a TxHxWxC video
30 and returns a transformed version.
32 Returns:
33 video (Tensor[T, H, W, C]): the `T` video frames
34 audio(Tensor[K, L]): the audio frames, where `K` is the number of channels
35 and `L` is the number of points
36 label (int): class of the video clip
37 """
39 def __init__(self, root, frames_per_clip, step_between_clips=1, transform=None):
40 super(Kinetics400, self).__init__(root)
41 extensions = ('avi',)
43 classes = list(sorted(list_dir(root)))
44 class_to_idx = {classes[i]: i for i in range(len(classes))}
45 self.samples = make_dataset(self.root, class_to_idx, extensions, is_valid_file=None)
46 self.classes = classes
47 video_list = [x[0] for x in self.samples]
48 self.video_clips = VideoClips(video_list, frames_per_clip, step_between_clips)
49 self.transform = transform
51 def __len__(self):
52 return self.video_clips.num_clips()
54 def __getitem__(self, idx):
55 video, audio, info, video_idx = self.video_clips.get_clip(idx)
56 label = self.samples[video_idx][1]
58 if self.transform is not None:
59 video = self.transform(video)
61 return video, audio, label