1 #!/usr/bin/env python
3 import sys
4 import os
5 import cv2
6 import argparse
7 import datetime
8 import numpy as np
10 ################################
11 from pytorch_jacinto_ai.xnn.utils import str2bool
12 parser = argparse.ArgumentParser()
13 parser.add_argument('--save_path', type=str, default=None, help='checkpoint save folder')
14 parser.add_argument('--gpus', type=int, nargs='*', default=None, help='Base learning rate')
15 parser.add_argument('--batch_size', type=int, default=None, help='Batch size')
16 parser.add_argument('--model_name', type=str, default=None, help='model name')
17 parser.add_argument('--dataset_name', type=str, default=None, help='dataset name')
18 parser.add_argument('--data_path', type=str, default=None, help='data path')
19 parser.add_argument('--epoch_size', type=float, default=None, help='epoch size. using a fraction will reduce the data used for one epoch')
20 parser.add_argument('--img_resize', type=int, nargs=2, default=None, help='img_resize size. for training this will be modified according to rand_scale')
21 parser.add_argument('--rand_scale', type=float, nargs=2, default=None, help='random scale factors for training')
22 parser.add_argument('--rand_crop', type=int, nargs=2, default=None, help='random crop for training')
23 parser.add_argument('--output_size', type=int, nargs=2, default=None, help='output size of the evaluation - prediction/groundtruth. this is not used while training as it blows up memory requirement')
24 parser.add_argument('--quantize', type=str2bool, default=None, help='Quantize the model')
25 #parser.add_argument('--model_surgery', type=str, default=None, choices=[None, 'pact2'], help='whether to transform the model after defining')
26 parser.add_argument('--pretrained', type=str, default=None, help='pretrained model')
27 parser.add_argument('--bitwidth_weights', type=int, default=None, help='bitwidth for weight quantization')
28 parser.add_argument('--bitwidth_activations', type=int, default=None, help='bitwidth for activation quantization')
29 cmds = parser.parse_args()
31 ################################
32 # taken care first, since this has to be done before importing pytorch
33 if 'gpus' in vars(cmds):
34 value = getattr(cmds, 'gpus')
35 if (value is not None) and ("CUDA_VISIBLE_DEVICES" not in os.environ):
36 os.environ["CUDA_VISIBLE_DEVICES"] = ','.join([str(v) for v in value])
37 #
38 #
40 # to avoid hangs in data loader with multi threads
41 # this was observed after using cv2 image processing functions
42 # https://github.com/pytorch/pytorch/issues/1355
43 cv2.setNumThreads(0)
46 ################################
47 #import of torch should be after CUDA_VISIBLE_DEVICES for it to take effect
48 import torch
49 from pytorch_jacinto_ai.engine import infer_pixel2pixel
51 # Create the parse and set default arguments
52 args = infer_pixel2pixel.get_config()
55 #Modify arguments
56 args.model_name = "deeplabv3lite_mobilenetv2_tv" #"deeplabv3lite_mobilenetv2_relu" #"deeplabv3lite_mobilenetv2_relu_x1p5" #"deeplabv3plus"
58 args.dataset_name = 'a2d2_segmentation_measure' #'tiad_segmentation_infer' #'cityscapes_segmentation_infer' #'tiad_segmentation' #'cityscapes_segmentation_measure'
60 #args.save_path = './data/checkpoints'
61 args.data_path = '/data/ssd/datasets/a2d2_v2/' #'./data/datasets/cityscapes/data' #'/data/hdd/datasets/cityscapes_leftImg8bit_sequence_trainvaltest/' #'./data/datasets/cityscapes/data' #'./data/tiad/data/demoVideo/sequence0021' #'./data/tiad/data/demoVideo/sequence0025' #'./data/tiad/data/demoVideo/sequence0001_2017'
62 #args.pretrained = './data/modelzoo/semantic_segmentation/cityscapes/deeplabv3lite-mobilenetv2/cityscapes_segmentation_deeplabv3lite-mobilenetv2_2019-06-26-08-59-32.pth'
63 #args.pretrained = './data/checkpoints/tiad_segmentation/2019-10-18_00-50-03_tiad_segmentation_deeplabv3lite_mobilenetv2_ericsun_resize768x384_traincrop768x384_float/checkpoint.pth.tar'
65 args.pretrained = '/data/files/work/bitbucket_TI/pytorch-jacinto-models/data/checkpoints/a2d2_segmentation/2020-01-25_13-06-18_a2d2_segmentation_deeplabv3lite_mobilenetv2_tv_resize768x384_traincrop768x384/training/model_best_ep172.pth.tar'
67 args.model_config.input_channels = (3,)
68 args.model_config.output_type = ['segmentation']
69 args.model_config.output_channels = None
70 args.losses = [['segmentation_loss']]
71 args.metrics = [['segmentation_metrics']]
73 args.frame_IOU = False # Print mIOU for each frame
74 args.shuffle = False
76 args.num_images = 30000 # Max number of images to run inference on
77 #args.blend = [False]
78 #'color', 'blend'
79 args.viz_op_type = ['color']
80 args.visualize_gt = False
81 args.car_mask = False # False #True
82 args.label = [True] # False #True
83 args.label_infer = [True]
84 args.palette = True
85 args.start_img_index = 0
86 args.end_img_index = 0
87 args.create_video = True # True #False
88 args.depth = [False]
90 args.epoch_size = 0 #0 #0.5
91 args.iter_size = 1 #2
93 args.batch_size = 1 #80 #12 #16 #32 #64
94 args.img_resize = (384, 768) #(256,512) #(512,512) # #(1024, 2048) #(512,1024) #(720, 1280)
96 args.output_size = (1208, 1920) #(1024, 2048)
97 #args.rand_scale = (1.0, 2.0) #(1.0,2.0) #(1.0,1.5) #(1.0,1.25)
99 args.quantize = True
101 args.depth = [False]
102 args.quantize = False
103 args.histogram_range = True
105 #args.image_prenorm=False
106 #args.image_mean = [0]
107 #args.image_scale = [1.0]
108 #args.image_prenorm = False
109 #args.image_mean = [123.675, 116.28, 103.53]
110 #args.image_scale = [0.017125, 0.017507, 0.017429]
111 #args.image_mean = [0] # image mean for input image normalization
112 #args.image_scale = [1.0] # image scaling/mult for input iamge normalization
114 #save modified files after last commit
115 #args.save_mod_files = True
117 args.gpu_mode = True
118 args.write_layer_ip_op = False
119 args.generate_onnx = True
121 ################################
122 for key in vars(cmds):
123 if key == 'gpus':
124 pass # already taken care above, since this has to be done before importing pytorch
125 elif hasattr(args, key):
126 value = getattr(cmds, key)
127 if value != 'None' and value is not None:
128 setattr(args, key, value)
129 else:
130 assert False, f'invalid argument {key}'
131 #
133 ################################
134 #Run the test
135 infer_pixel2pixel.main(args)