# Jacinto-AI-DevKit (PyTorch)
###### Notice:
- If you have not visited our landing page in github, please do so: [https://github.com/TexasInstruments/jacinto-ai-devkit](https://github.com/TexasInstruments/jacinto-ai-devkit)
- **Issue Tracker for jacinto-ai-devkit:** You can file issues or ask questions at **e2e**: [https://e2e.ti.com/support/processors/f/791/tags/jacinto_2D00_ai_2D00_devkit](https://e2e.ti.com/support/processors/f/791/tags/jacinto_2D00_ai_2D00_devkit). While creating a new issue kindly include **jacinto-ai-devkit** in the tags (as you create a new issue, there is a space to enter tags, at the bottom of the page).
- **Issue Tracker for TIDL:** [https://e2e.ti.com/support/processors/f/791/tags/TIDL](https://e2e.ti.com/support/processors/f/791/tags/TIDL). Please include the tag **TIDL** (as you create a new issue, there is a space to enter tags, at the bottom of the page).
- If you do not get a reply within two days, please contact us at: jacinto-ai-devkit@list.ti.com
### Deep Learning Models / Training / Calibration & Quantization - Using PyTorch
This code provides a set of low complexity deep learning examples and models for low power embedded systems. Low power embedded systems often requires balancing of complexity and accuracy. This is a tough task and requires significant amount of expertise and experimentation. We call this process **complexity optimization**. In addition we would like to bridge the gap between Deep Learning training frameworks and real-time embedded inference by providing ready to use examples and enable **ease of use**. Scripts for training, validation, complexity analysis are also provided.
This code also includes tools for **Quantization Aware Training** that can output an 8-bit Quantization friendly model - these tools can be used to improve the quantized accuracy and bring it near floating point accuracy. For more details, please refer to the section on [Quantization](docs/Quantization.md).
**Several of these models have been verified to work on [TI's Jacinto7 Automotive Processors](http://www.ti.com/processors/automotive-processors/tdax-adas-socs/overview.html).** These tools and software are primarily intended as examples for learning and research.
## Installation Instructions
- These instructions are for installation on **Ubuntu 18.04**.
- Install Anaconda with Python 3.7 or higher from https://www.anaconda.com/distribution/
- After installation, make sure that your python is indeed Anaconda Python 3.7 or higher by typing:
```
python --version
```
- Clone this repository into your local folder
- Execute the following shell script to install the dependencies:
```
./setup.sh
```
## Examples
The following examples are currently available. Click on each of the links below to go into the full description of the example.
* Image Classification
* [**Image Classification**](docs/Image_Classification.md)
* Pixel2Pixel prediction
* [**Semantic Segmentation**](docs/Semantic_Segmentation.md)
* [Depth Estimation](docs/Depth_Estimation.md)
* [Motion Segmentation](docs/Motion_Segmentation.md)
* Multi Task Estimation - coming soon..
* Object Detection
* Object Detection - coming soon..
* Object Keypoint Estimation - coming soon..
* [**Quantization**](docs/Quantization.md)
Some of the common training and validation commands are provided in shell scripts (.sh files) in the root folder.
## Additional Information
For information on other similar devkits, please visit:
- Landing Page: [https://github.com/TexasInstruments/jacinto-ai-devkit](https://github.com/TexasInstruments/jacinto-ai-devkit)
- Actual Git Repositories: [https://git.ti.com/jacinto-ai-devkit](https://git.ti.com/jacinto-ai-devkit)
## Acknowledgements
Our source code uses parts of the following open source projects. We would like to sincerely thank their authors for making their code bases publicly available.
|Module/Functionality |Parts of the code borrowed/modified from |
|----------------------------------|-------------------------------------------------------------------------------------|
|Datasets, Models |https://github.com/pytorch/vision, https://github.com/ansleliu/LightNet |
|Training, Validation Engine/Loops |https://github.com/pytorch/examples, https://github.com/ClementPinard/FlowNetPytorch |
|Object Detection |https://github.com/open-mmlab/mmdetection |
## License
Please see the [LICENSE](./LICENSE) file for more information about the license under which this code is made available.