1 /*
2 * fs/signalfd.c
3 *
4 * Copyright (C) 2003 Linus Torvalds
5 *
6 * Mon Mar 5, 2007: Davide Libenzi <davidel@xmailserver.org>
7 * Changed ->read() to return a siginfo strcture instead of signal number.
8 * Fixed locking in ->poll().
9 * Added sighand-detach notification.
10 * Added fd re-use in sys_signalfd() syscall.
11 * Now using anonymous inode source.
12 * Thanks to Oleg Nesterov for useful code review and suggestions.
13 * More comments and suggestions from Arnd Bergmann.
14 * Sat May 19, 2007: Davi E. M. Arnaut <davi@haxent.com.br>
15 * Retrieve multiple signals with one read() call
16 * Sun Jul 15, 2007: Davide Libenzi <davidel@xmailserver.org>
17 * Attach to the sighand only during read() and poll().
18 */
20 #include <linux/file.h>
21 #include <linux/poll.h>
22 #include <linux/init.h>
23 #include <linux/fs.h>
24 #include <linux/sched.h>
25 #include <linux/slab.h>
26 #include <linux/kernel.h>
27 #include <linux/signal.h>
28 #include <linux/list.h>
29 #include <linux/anon_inodes.h>
30 #include <linux/signalfd.h>
31 #include <linux/syscalls.h>
32 #include <linux/proc_fs.h>
33 #include <linux/compat.h>
35 void signalfd_cleanup(struct sighand_struct *sighand)
36 {
37 wait_queue_head_t *wqh = &sighand->signalfd_wqh;
38 /*
39 * The lockless check can race with remove_wait_queue() in progress,
40 * but in this case its caller should run under rcu_read_lock() and
41 * sighand_cachep is SLAB_DESTROY_BY_RCU, we can safely return.
42 */
43 if (likely(!waitqueue_active(wqh)))
44 return;
46 /* wait_queue_t->func(POLLFREE) should do remove_wait_queue() */
47 wake_up_poll(wqh, POLLHUP | POLLFREE);
48 }
50 struct signalfd_ctx {
51 sigset_t sigmask;
52 };
54 static int signalfd_release(struct inode *inode, struct file *file)
55 {
56 kfree(file->private_data);
57 return 0;
58 }
60 static unsigned int signalfd_poll(struct file *file, poll_table *wait)
61 {
62 struct signalfd_ctx *ctx = file->private_data;
63 unsigned int events = 0;
65 poll_wait(file, ¤t->sighand->signalfd_wqh, wait);
67 spin_lock_irq(¤t->sighand->siglock);
68 if (next_signal(¤t->pending, &ctx->sigmask) ||
69 next_signal(¤t->signal->shared_pending,
70 &ctx->sigmask))
71 events |= POLLIN;
72 spin_unlock_irq(¤t->sighand->siglock);
74 return events;
75 }
77 /*
78 * Copied from copy_siginfo_to_user() in kernel/signal.c
79 */
80 static int signalfd_copyinfo(struct signalfd_siginfo __user *uinfo,
81 siginfo_t const *kinfo)
82 {
83 long err;
85 BUILD_BUG_ON(sizeof(struct signalfd_siginfo) != 128);
87 /*
88 * Unused members should be zero ...
89 */
90 err = __clear_user(uinfo, sizeof(*uinfo));
92 /*
93 * If you change siginfo_t structure, please be sure
94 * this code is fixed accordingly.
95 */
96 err |= __put_user(kinfo->si_signo, &uinfo->ssi_signo);
97 err |= __put_user(kinfo->si_errno, &uinfo->ssi_errno);
98 err |= __put_user((short) kinfo->si_code, &uinfo->ssi_code);
99 switch (kinfo->si_code & __SI_MASK) {
100 case __SI_KILL:
101 err |= __put_user(kinfo->si_pid, &uinfo->ssi_pid);
102 err |= __put_user(kinfo->si_uid, &uinfo->ssi_uid);
103 break;
104 case __SI_TIMER:
105 err |= __put_user(kinfo->si_tid, &uinfo->ssi_tid);
106 err |= __put_user(kinfo->si_overrun, &uinfo->ssi_overrun);
107 err |= __put_user((long) kinfo->si_ptr, &uinfo->ssi_ptr);
108 err |= __put_user(kinfo->si_int, &uinfo->ssi_int);
109 break;
110 case __SI_POLL:
111 err |= __put_user(kinfo->si_band, &uinfo->ssi_band);
112 err |= __put_user(kinfo->si_fd, &uinfo->ssi_fd);
113 break;
114 case __SI_FAULT:
115 err |= __put_user((long) kinfo->si_addr, &uinfo->ssi_addr);
116 #ifdef __ARCH_SI_TRAPNO
117 err |= __put_user(kinfo->si_trapno, &uinfo->ssi_trapno);
118 #endif
119 #ifdef BUS_MCEERR_AO
120 /*
121 * Other callers might not initialize the si_lsb field,
122 * so check explicitly for the right codes here.
123 */
124 if (kinfo->si_code == BUS_MCEERR_AR ||
125 kinfo->si_code == BUS_MCEERR_AO)
126 err |= __put_user((short) kinfo->si_addr_lsb,
127 &uinfo->ssi_addr_lsb);
128 #endif
129 break;
130 case __SI_CHLD:
131 err |= __put_user(kinfo->si_pid, &uinfo->ssi_pid);
132 err |= __put_user(kinfo->si_uid, &uinfo->ssi_uid);
133 err |= __put_user(kinfo->si_status, &uinfo->ssi_status);
134 err |= __put_user(kinfo->si_utime, &uinfo->ssi_utime);
135 err |= __put_user(kinfo->si_stime, &uinfo->ssi_stime);
136 break;
137 case __SI_RT: /* This is not generated by the kernel as of now. */
138 case __SI_MESGQ: /* But this is */
139 err |= __put_user(kinfo->si_pid, &uinfo->ssi_pid);
140 err |= __put_user(kinfo->si_uid, &uinfo->ssi_uid);
141 err |= __put_user((long) kinfo->si_ptr, &uinfo->ssi_ptr);
142 err |= __put_user(kinfo->si_int, &uinfo->ssi_int);
143 break;
144 default:
145 /*
146 * This case catches also the signals queued by sigqueue().
147 */
148 err |= __put_user(kinfo->si_pid, &uinfo->ssi_pid);
149 err |= __put_user(kinfo->si_uid, &uinfo->ssi_uid);
150 err |= __put_user((long) kinfo->si_ptr, &uinfo->ssi_ptr);
151 err |= __put_user(kinfo->si_int, &uinfo->ssi_int);
152 break;
153 }
155 return err ? -EFAULT: sizeof(*uinfo);
156 }
158 static ssize_t signalfd_dequeue(struct signalfd_ctx *ctx, siginfo_t *info,
159 int nonblock)
160 {
161 ssize_t ret;
162 DECLARE_WAITQUEUE(wait, current);
164 spin_lock_irq(¤t->sighand->siglock);
165 ret = dequeue_signal(current, &ctx->sigmask, info);
166 switch (ret) {
167 case 0:
168 if (!nonblock)
169 break;
170 ret = -EAGAIN;
171 default:
172 spin_unlock_irq(¤t->sighand->siglock);
173 return ret;
174 }
176 add_wait_queue(¤t->sighand->signalfd_wqh, &wait);
177 for (;;) {
178 set_current_state(TASK_INTERRUPTIBLE);
179 ret = dequeue_signal(current, &ctx->sigmask, info);
180 if (ret != 0)
181 break;
182 if (signal_pending(current)) {
183 ret = -ERESTARTSYS;
184 break;
185 }
186 spin_unlock_irq(¤t->sighand->siglock);
187 schedule();
188 spin_lock_irq(¤t->sighand->siglock);
189 }
190 spin_unlock_irq(¤t->sighand->siglock);
192 remove_wait_queue(¤t->sighand->signalfd_wqh, &wait);
193 __set_current_state(TASK_RUNNING);
195 return ret;
196 }
198 /*
199 * Returns a multiple of the size of a "struct signalfd_siginfo", or a negative
200 * error code. The "count" parameter must be at least the size of a
201 * "struct signalfd_siginfo".
202 */
203 static ssize_t signalfd_read(struct file *file, char __user *buf, size_t count,
204 loff_t *ppos)
205 {
206 struct signalfd_ctx *ctx = file->private_data;
207 struct signalfd_siginfo __user *siginfo;
208 int nonblock = file->f_flags & O_NONBLOCK;
209 ssize_t ret, total = 0;
210 siginfo_t info;
212 count /= sizeof(struct signalfd_siginfo);
213 if (!count)
214 return -EINVAL;
216 siginfo = (struct signalfd_siginfo __user *) buf;
217 do {
218 ret = signalfd_dequeue(ctx, &info, nonblock);
219 if (unlikely(ret <= 0))
220 break;
221 ret = signalfd_copyinfo(siginfo, &info);
222 if (ret < 0)
223 break;
224 siginfo++;
225 total += ret;
226 nonblock = 1;
227 } while (--count);
229 return total ? total: ret;
230 }
232 #ifdef CONFIG_PROC_FS
233 static int signalfd_show_fdinfo(struct seq_file *m, struct file *f)
234 {
235 struct signalfd_ctx *ctx = f->private_data;
236 sigset_t sigmask;
238 sigmask = ctx->sigmask;
239 signotset(&sigmask);
240 render_sigset_t(m, "sigmask:\t", &sigmask);
242 return 0;
243 }
244 #endif
246 static const struct file_operations signalfd_fops = {
247 #ifdef CONFIG_PROC_FS
248 .show_fdinfo = signalfd_show_fdinfo,
249 #endif
250 .release = signalfd_release,
251 .poll = signalfd_poll,
252 .read = signalfd_read,
253 .llseek = noop_llseek,
254 };
256 SYSCALL_DEFINE4(signalfd4, int, ufd, sigset_t __user *, user_mask,
257 size_t, sizemask, int, flags)
258 {
259 sigset_t sigmask;
260 struct signalfd_ctx *ctx;
262 /* Check the SFD_* constants for consistency. */
263 BUILD_BUG_ON(SFD_CLOEXEC != O_CLOEXEC);
264 BUILD_BUG_ON(SFD_NONBLOCK != O_NONBLOCK);
266 if (flags & ~(SFD_CLOEXEC | SFD_NONBLOCK))
267 return -EINVAL;
269 if (sizemask != sizeof(sigset_t) ||
270 copy_from_user(&sigmask, user_mask, sizeof(sigmask)))
271 return -EINVAL;
272 sigdelsetmask(&sigmask, sigmask(SIGKILL) | sigmask(SIGSTOP));
273 signotset(&sigmask);
275 if (ufd == -1) {
276 ctx = kmalloc(sizeof(*ctx), GFP_KERNEL);
277 if (!ctx)
278 return -ENOMEM;
280 ctx->sigmask = sigmask;
282 /*
283 * When we call this, the initialization must be complete, since
284 * anon_inode_getfd() will install the fd.
285 */
286 ufd = anon_inode_getfd("[signalfd]", &signalfd_fops, ctx,
287 O_RDWR | (flags & (O_CLOEXEC | O_NONBLOCK)));
288 if (ufd < 0)
289 kfree(ctx);
290 } else {
291 struct fd f = fdget(ufd);
292 if (!f.file)
293 return -EBADF;
294 ctx = f.file->private_data;
295 if (f.file->f_op != &signalfd_fops) {
296 fdput(f);
297 return -EINVAL;
298 }
299 spin_lock_irq(¤t->sighand->siglock);
300 ctx->sigmask = sigmask;
301 spin_unlock_irq(¤t->sighand->siglock);
303 wake_up(¤t->sighand->signalfd_wqh);
304 fdput(f);
305 }
307 return ufd;
308 }
310 SYSCALL_DEFINE3(signalfd, int, ufd, sigset_t __user *, user_mask,
311 size_t, sizemask)
312 {
313 return sys_signalfd4(ufd, user_mask, sizemask, 0);
314 }
316 #ifdef CONFIG_COMPAT
317 COMPAT_SYSCALL_DEFINE4(signalfd4, int, ufd,
318 const compat_sigset_t __user *,sigmask,
319 compat_size_t, sigsetsize,
320 int, flags)
321 {
322 compat_sigset_t ss32;
323 sigset_t tmp;
324 sigset_t __user *ksigmask;
326 if (sigsetsize != sizeof(compat_sigset_t))
327 return -EINVAL;
328 if (copy_from_user(&ss32, sigmask, sizeof(ss32)))
329 return -EFAULT;
330 sigset_from_compat(&tmp, &ss32);
331 ksigmask = compat_alloc_user_space(sizeof(sigset_t));
332 if (copy_to_user(ksigmask, &tmp, sizeof(sigset_t)))
333 return -EFAULT;
335 return sys_signalfd4(ufd, ksigmask, sizeof(sigset_t), flags);
336 }
338 COMPAT_SYSCALL_DEFINE3(signalfd, int, ufd,
339 const compat_sigset_t __user *,sigmask,
340 compat_size_t, sigsetsize)
341 {
342 return compat_sys_signalfd4(ufd, sigmask, sigsetsize, 0);
343 }
344 #endif