]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - keystone-linux/linux.git/blob - samples/Kconfig
Merge branch 'release' of git://git.kernel.org/pub/scm/linux/kernel/git/rzhang/linux
[keystone-linux/linux.git] / samples / Kconfig
1 menuconfig SAMPLES
2         bool "Sample kernel code"
3         help
4           You can build and test sample kernel code here.
6 if SAMPLES
8 config SAMPLE_TRACE_EVENTS
9         tristate "Build trace_events examples -- loadable modules only"
10         depends on EVENT_TRACING && m
11         help
12           This build trace event example modules.
14 config SAMPLE_KOBJECT
15         tristate "Build kobject examples -- loadable modules only"
16         depends on m
17         help
18           This config option will allow you to build a number of
19           different kobject sample modules showing how to use kobjects,
20           ksets, and ktypes properly.
22           If in doubt, say "N" here.
24 config SAMPLE_KPROBES
25         tristate "Build kprobes examples -- loadable modules only"
26         depends on KPROBES && m
27         help
28           This build several kprobes example modules.
30 config SAMPLE_KRETPROBES
31         tristate "Build kretprobes example -- loadable modules only"
32         default m
33         depends on SAMPLE_KPROBES && KRETPROBES
35 config SAMPLE_HW_BREAKPOINT
36         tristate "Build kernel hardware breakpoint examples -- loadable module only"
37         depends on HAVE_HW_BREAKPOINT && m
38         help
39           This builds kernel hardware breakpoint example modules.
41 config SAMPLE_KFIFO
42         tristate "Build kfifo examples -- loadable modules only"
43         depends on m
44         help
45           This config option will allow you to build a number of
46           different kfifo sample modules showing how to use the
47           generic kfifo API.
49           If in doubt, say "N" here.
51 config SAMPLE_KDB
52         tristate "Build kdb command example -- loadable modules only"
53         depends on KGDB_KDB && m
54         help
55           Build an example of how to dynamically add the hello
56           command to the kdb shell.
58 config SAMPLE_RPMSG_CLIENT
59         tristate "Build rpmsg client sample -- loadable modules only"
60         depends on RPMSG && m
61         help
62           Build an rpmsg client sample driver, which demonstrates how
63           to communicate with an AMP-configured remote processor over
64           the rpmsg bus.
66 endif # SAMPLES