1 menuconfig SAMPLES
2 bool "Sample kernel code"
3 help
4 You can build and test sample kernel code here.
6 if SAMPLES
8 config SAMPLE_TRACE_EVENTS
9 tristate "Build trace_events examples -- loadable modules only"
10 depends on EVENT_TRACING && m
11 help
12 This build trace event example modules.
14 config SAMPLE_KOBJECT
15 tristate "Build kobject examples -- loadable modules only"
16 depends on m
17 help
18 This config option will allow you to build a number of
19 different kobject sample modules showing how to use kobjects,
20 ksets, and ktypes properly.
22 If in doubt, say "N" here.
24 config SAMPLE_KPROBES
25 tristate "Build kprobes examples -- loadable modules only"
26 depends on KPROBES && m
27 help
28 This build several kprobes example modules.
30 config SAMPLE_KRETPROBES
31 tristate "Build kretprobes example -- loadable modules only"
32 default m
33 depends on SAMPLE_KPROBES && KRETPROBES
35 config SAMPLE_HW_BREAKPOINT
36 tristate "Build kernel hardware breakpoint examples -- loadable module only"
37 depends on HAVE_HW_BREAKPOINT && m
38 help
39 This builds kernel hardware breakpoint example modules.
41 config SAMPLE_KFIFO
42 tristate "Build kfifo examples -- loadable modules only"
43 depends on m
44 help
45 This config option will allow you to build a number of
46 different kfifo sample modules showing how to use the
47 generic kfifo API.
49 If in doubt, say "N" here.
51 config SAMPLE_KDB
52 tristate "Build kdb command example -- loadable modules only"
53 depends on KGDB_KDB && m
54 help
55 Build an example of how to dynamically add the hello
56 command to the kdb shell.
58 config SAMPLE_RPMSG_CLIENT
59 tristate "Build rpmsg client sample -- loadable modules only"
60 depends on RPMSG && m
61 help
62 Build an rpmsg client sample driver, which demonstrates how
63 to communicate with an AMP-configured remote processor over
64 the rpmsg bus.
66 endif # SAMPLES