1 #!/bin/sh
2 # Copyright (C) Martin Schlemmer <azarah@nosferatu.za.org>
3 # Copyright (C) 2006 Sam Ravnborg <sam@ravnborg.org>
4 #
5 # Released under the terms of the GNU GPL
6 #
7 # Generate a cpio packed initramfs. It uses gen_init_cpio to generate
8 # the cpio archive, and then compresses it.
9 # The script may also be used to generate the inputfile used for gen_init_cpio
10 # This script assumes that gen_init_cpio is located in usr/ directory
12 # error out on errors
13 set -e
15 usage() {
16 cat << EOF
17 Usage:
18 $0 [-o <file>] [-u <uid>] [-g <gid>] {-d | <cpio_source>} ...
19 -o <file> Create compressed initramfs file named <file> using
20 gen_init_cpio and compressor depending on the extension
21 -u <uid> User ID to map to user ID 0 (root).
22 <uid> is only meaningful if <cpio_source> is a
23 directory. "squash" forces all files to uid 0.
24 -g <gid> Group ID to map to group ID 0 (root).
25 <gid> is only meaningful if <cpio_source> is a
26 directory. "squash" forces all files to gid 0.
27 <cpio_source> File list or directory for cpio archive.
28 If <cpio_source> is a .cpio file it will be used
29 as direct input to initramfs.
30 -d Output the default cpio list.
32 All options except -o and -l may be repeated and are interpreted
33 sequentially and immediately. -u and -g states are preserved across
34 <cpio_source> options so an explicit "-u 0 -g 0" is required
35 to reset the root/group mapping.
36 EOF
37 }
39 # awk style field access
40 # $1 - field number; rest is argument string
41 field() {
42 shift $1 ; echo $1
43 }
45 list_default_initramfs() {
46 # echo usr/kinit/kinit
47 :
48 }
50 default_initramfs() {
51 cat <<-EOF >> ${output}
52 # This is a very simple, default initramfs
54 dir /dev 0755 0 0
55 nod /dev/console 0600 0 0 c 5 1
56 dir /root 0700 0 0
57 # file /kinit usr/kinit/kinit 0755 0 0
58 # slink /init kinit 0755 0 0
59 EOF
60 }
62 filetype() {
63 local argv1="$1"
65 # symlink test must come before file test
66 if [ -L "${argv1}" ]; then
67 echo "slink"
68 elif [ -f "${argv1}" ]; then
69 echo "file"
70 elif [ -d "${argv1}" ]; then
71 echo "dir"
72 elif [ -b "${argv1}" -o -c "${argv1}" ]; then
73 echo "nod"
74 elif [ -p "${argv1}" ]; then
75 echo "pipe"
76 elif [ -S "${argv1}" ]; then
77 echo "sock"
78 else
79 echo "invalid"
80 fi
81 return 0
82 }
84 list_print_mtime() {
85 :
86 }
88 print_mtime() {
89 local my_mtime="0"
91 if [ -e "$1" ]; then
92 my_mtime=$(find "$1" -printf "%T@\n" | sort -r | head -n 1)
93 fi
95 echo "# Last modified: ${my_mtime}" >> ${output}
96 echo "" >> ${output}
97 }
99 list_parse() {
100 [ ! -L "$1" ] && echo "$1 \\" || :
101 }
103 # for each file print a line in following format
104 # <filetype> <name> <path to file> <octal mode> <uid> <gid>
105 # for links, devices etc the format differs. See gen_init_cpio for details
106 parse() {
107 local location="$1"
108 local name="/${location#${srcdir}}"
109 # change '//' into '/'
110 name=$(echo "$name" | sed -e 's://*:/:g')
111 local mode="$2"
112 local uid="$3"
113 local gid="$4"
114 local ftype=$(filetype "${location}")
115 # remap uid/gid to 0 if necessary
116 [ "$root_uid" = "squash" ] && uid=0 || [ "$uid" -eq "$root_uid" ] && uid=0
117 [ "$root_gid" = "squash" ] && gid=0 || [ "$gid" -eq "$root_gid" ] && gid=0
118 local str="${mode} ${uid} ${gid}"
120 [ "${ftype}" = "invalid" ] && return 0
121 [ "${location}" = "${srcdir}" ] && return 0
123 case "${ftype}" in
124 "file")
125 str="${ftype} ${name} ${location} ${str}"
126 ;;
127 "nod")
128 local dev=`LC_ALL=C ls -l "${location}"`
129 local maj=`field 5 ${dev}`
130 local min=`field 6 ${dev}`
131 maj=${maj%,}
133 [ -b "${location}" ] && dev="b" || dev="c"
135 str="${ftype} ${name} ${str} ${dev} ${maj} ${min}"
136 ;;
137 "slink")
138 local target=`readlink "${location}"`
139 str="${ftype} ${name} ${target} ${str}"
140 ;;
141 *)
142 str="${ftype} ${name} ${str}"
143 ;;
144 esac
146 echo "${str}" >> ${output}
148 return 0
149 }
151 unknown_option() {
152 printf "ERROR: unknown option \"$arg\"\n" >&2
153 printf "If the filename validly begins with '-', " >&2
154 printf "then it must be prefixed\n" >&2
155 printf "by './' so that it won't be interpreted as an option." >&2
156 printf "\n" >&2
157 usage >&2
158 exit 1
159 }
161 list_header() {
162 :
163 }
165 header() {
166 printf "\n#####################\n# $1\n" >> ${output}
167 }
169 # process one directory (incl sub-directories)
170 dir_filelist() {
171 ${dep_list}header "$1"
173 srcdir=$(echo "$1" | sed -e 's://*:/:g')
174 dirlist=$(find "${srcdir}" -printf "%p %m %U %G\n")
176 # If $dirlist is only one line, then the directory is empty
177 if [ "$(echo "${dirlist}" | wc -l)" -gt 1 ]; then
178 ${dep_list}print_mtime "$1"
180 echo "${dirlist}" | \
181 while read x; do
182 ${dep_list}parse ${x}
183 done
184 fi
185 }
187 # if only one file is specified and it is .cpio file then use it direct as fs
188 # if a directory is specified then add all files in given direcotry to fs
189 # if a regular file is specified assume it is in gen_initramfs format
190 input_file() {
191 source="$1"
192 if [ -f "$1" ]; then
193 ${dep_list}header "$1"
194 is_cpio="$(echo "$1" | sed 's/^.*\.cpio\(\..*\)\?/cpio/')"
195 if [ $2 -eq 0 -a ${is_cpio} = "cpio" ]; then
196 cpio_file=$1
197 echo "$1" | grep -q '^.*\.cpio\..*' && is_cpio_compressed="compressed"
198 [ ! -z ${dep_list} ] && echo "$1"
199 return 0
200 fi
201 if [ -z ${dep_list} ]; then
202 print_mtime "$1" >> ${output}
203 cat "$1" >> ${output}
204 else
205 echo "$1 \\"
206 cat "$1" | while read type dir file perm ; do
207 if [ "$type" = "file" ]; then
208 echo "$file \\";
209 fi
210 done
211 fi
212 elif [ -d "$1" ]; then
213 dir_filelist "$1"
214 else
215 echo " ${prog}: Cannot open '$1'" >&2
216 exit 1
217 fi
218 }
220 prog=$0
221 root_uid=0
222 root_gid=0
223 dep_list=
224 cpio_file=
225 cpio_list=
226 output="/dev/stdout"
227 output_file=""
228 is_cpio_compressed=
229 compr="gzip -n -9 -f"
231 arg="$1"
232 case "$arg" in
233 "-l") # files included in initramfs - used by kbuild
234 dep_list="list_"
235 echo "deps_initramfs := $0 \\"
236 shift
237 ;;
238 "-o") # generate compressed cpio image named $1
239 shift
240 output_file="$1"
241 cpio_list="$(mktemp ${TMPDIR:-/tmp}/cpiolist.XXXXXX)"
242 output=${cpio_list}
243 echo "$output_file" | grep -q "\.gz$" && compr="gzip -n -9 -f"
244 echo "$output_file" | grep -q "\.bz2$" && compr="bzip2 -9 -f"
245 echo "$output_file" | grep -q "\.lzma$" && compr="lzma -9 -f"
246 echo "$output_file" | grep -q "\.xz$" && \
247 compr="xz --check=crc32 --lzma2=dict=1MiB"
248 echo "$output_file" | grep -q "\.lzo$" && compr="lzop -9 -f"
249 echo "$output_file" | grep -q "\.cpio$" && compr="cat"
250 shift
251 ;;
252 esac
253 while [ $# -gt 0 ]; do
254 arg="$1"
255 shift
256 case "$arg" in
257 "-u") # map $1 to uid=0 (root)
258 root_uid="$1"
259 shift
260 ;;
261 "-g") # map $1 to gid=0 (root)
262 root_gid="$1"
263 shift
264 ;;
265 "-d") # display default initramfs list
266 default_list="$arg"
267 ${dep_list}default_initramfs
268 ;;
269 "-h")
270 usage
271 exit 0
272 ;;
273 *)
274 case "$arg" in
275 "-"*)
276 unknown_option
277 ;;
278 *) # input file/dir - process it
279 input_file "$arg" "$#"
280 ;;
281 esac
282 ;;
283 esac
284 done
286 # If output_file is set we will generate cpio archive and compress it
287 # we are careful to delete tmp files
288 if [ ! -z ${output_file} ]; then
289 if [ -z ${cpio_file} ]; then
290 timestamp=
291 if test -n "$KBUILD_BUILD_TIMESTAMP"; then
292 timestamp="$(date -d"$KBUILD_BUILD_TIMESTAMP" +%s || :)"
293 if test -n "$timestamp"; then
294 timestamp="-t $timestamp"
295 fi
296 fi
297 cpio_tfile="$(mktemp ${TMPDIR:-/tmp}/cpiofile.XXXXXX)"
298 usr/gen_init_cpio $timestamp ${cpio_list} > ${cpio_tfile}
299 else
300 cpio_tfile=${cpio_file}
301 fi
302 rm ${cpio_list}
303 if [ "${is_cpio_compressed}" = "compressed" ]; then
304 cat ${cpio_tfile} > ${output_file}
305 else
306 (cat ${cpio_tfile} | ${compr} - > ${output_file}) \
307 || (rm -f ${output_file} ; false)
308 fi
309 [ -z ${cpio_file} ] && rm ${cpio_tfile}
310 fi
311 exit 0