/* * Sample kfifo int type implementation * * Copyright (C) 2010 Stefani Seibold * * Released under the GPL version 2 only. * */ #include #include #include #include #include /* * This module shows how to create a int type fifo. */ /* fifo size in elements (ints) */ #define FIFO_SIZE 32 /* name of the proc entry */ #define PROC_FIFO "int-fifo" /* lock for procfs read access */ static DEFINE_MUTEX(read_lock); /* lock for procfs write access */ static DEFINE_MUTEX(write_lock); /* * define DYNAMIC in this example for a dynamically allocated fifo. * * Otherwise the fifo storage will be a part of the fifo structure. */ #if 0 #define DYNAMIC #endif #ifdef DYNAMIC static DECLARE_KFIFO_PTR(test, int); #else static DEFINE_KFIFO(test, int, FIFO_SIZE); #endif static const int expected_result[FIFO_SIZE] = { 3, 4, 5, 6, 7, 8, 9, 0, 1, 20, 21, 22, 23, 24, 25, 26, 27, 28, 29, 30, 31, 32, 33, 34, 35, 36, 37, 38, 39, 40, 41, 42, }; static int __init testfunc(void) { int buf[6]; int i, j; unsigned int ret; printk(KERN_INFO "int fifo test start\n"); /* put values into the fifo */ for (i = 0; i != 10; i++) kfifo_put(&test, &i); /* show the number of used elements */ printk(KERN_INFO "fifo len: %u\n", kfifo_len(&test)); /* get max of 2 elements from the fifo */ ret = kfifo_out(&test, buf, 2); printk(KERN_INFO "ret: %d\n", ret); /* and put it back to the end of the fifo */ ret = kfifo_in(&test, buf, ret); printk(KERN_INFO "ret: %d\n", ret); /* skip first element of the fifo */ printk(KERN_INFO "skip 1st element\n"); kfifo_skip(&test); /* put values into the fifo until is full */ for (i = 20; kfifo_put(&test, &i); i++) ; printk(KERN_INFO "queue len: %u\n", kfifo_len(&test)); /* show the first value without removing from the fifo */ if (kfifo_peek(&test, &i)) printk(KERN_INFO "%d\n", i); /* check the correctness of all values in the fifo */ j = 0; while (kfifo_get(&test, &i)) { printk(KERN_INFO "item = %d\n", i); if (i != expected_result[j++]) { printk(KERN_WARNING "value mismatch: test failed\n"); return -EIO; } } if (j != ARRAY_SIZE(expected_result)) { printk(KERN_WARNING "size mismatch: test failed\n"); return -EIO; } printk(KERN_INFO "test passed\n"); return 0; } static ssize_t fifo_write(struct file *file, const char __user *buf, size_t count, loff_t *ppos) { int ret; unsigned int copied; if (mutex_lock_interruptible(&write_lock)) return -ERESTARTSYS; ret = kfifo_from_user(&test, buf, count, &copied); mutex_unlock(&write_lock); return ret ? ret : copied; } static ssize_t fifo_read(struct file *file, char __user *buf, size_t count, loff_t *ppos) { int ret; unsigned int copied; if (mutex_lock_interruptible(&read_lock)) return -ERESTARTSYS; ret = kfifo_to_user(&test, buf, count, &copied); mutex_unlock(&read_lock); return ret ? ret : copied; } static const struct file_operations fifo_fops = { .owner = THIS_MODULE, .read = fifo_read, .write = fifo_write, .llseek = noop_llseek, }; static int __init example_init(void) { #ifdef DYNAMIC int ret; ret = kfifo_alloc(&test, FIFO_SIZE, GFP_KERNEL); if (ret) { printk(KERN_ERR "error kfifo_alloc\n"); return ret; } #endif if (testfunc() < 0) { #ifdef DYNAMIC kfifo_free(&test); #endif return -EIO; } if (proc_create(PROC_FIFO, 0, NULL, &fifo_fops) == NULL) { #ifdef DYNAMIC kfifo_free(&test); #endif return -ENOMEM; } return 0; } static void __exit example_exit(void) { remove_proc_entry(PROC_FIFO, NULL); #ifdef DYNAMIC kfifo_free(&test); #endif } module_init(example_init); module_exit(example_exit); MODULE_LICENSE("GPL"); MODULE_AUTHOR("Stefani Seibold ");