]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - keystone-linux/linux.git/commit
genirq: Sanitize spurious interrupt detection of threaded irqs
authorThomas Gleixner <tglx@linutronix.de>
Thu, 7 Mar 2013 13:53:45 +0000 (14:53 +0100)
committerGreg Kroah-Hartman <gregkh@linuxfoundation.org>
Tue, 1 Jul 2014 03:09:45 +0000 (20:09 -0700)
commit72aeabd74a7154d560efcd14afa0244f4393cf8b
tree8f3fd2d8cfda305a185b156f1276b74f2f239b2d
parent1790b2dd037e286b2b01c6254081cf349b72a003
genirq: Sanitize spurious interrupt detection of threaded irqs

commit 1e77d0a1ed7417d2a5a52a7b8d32aea1833faa6c upstream.

Till reported that the spurious interrupt detection of threaded
interrupts is broken in two ways:

- note_interrupt() is called for each action thread of a shared
  interrupt line. That's wrong as we are only interested whether none
  of the device drivers felt responsible for the interrupt, but by
  calling multiple times for a single interrupt line we account
  IRQ_NONE even if one of the drivers felt responsible.

- note_interrupt() when called from the thread handler is not
  serialized. That leaves the members of irq_desc which are used for
  the spurious detection unprotected.

To solve this we need to defer the spurious detection of a threaded
interrupt to the next hardware interrupt context where we have
implicit serialization.

If note_interrupt is called with action_ret == IRQ_WAKE_THREAD, we
check whether the previous interrupt requested a deferred check. If
not, we request a deferred check for the next hardware interrupt and
return.

If set, we check whether one of the interrupt threads signaled
success. Depending on this information we feed the result into the
spurious detector.

If one primary handler of a shared interrupt returns IRQ_HANDLED we
disable the deferred check of irq threads on the same line, as we have
found at least one device driver who cared.

Reported-by: Till Straumann <strauman@slac.stanford.edu>
Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
Tested-by: Austin Schuh <austin@peloton-tech.com>
Cc: Oliver Hartkopp <socketcan@hartkopp.net>
Cc: Wolfgang Grandegger <wg@grandegger.com>
Cc: Pavel Pisa <pisa@cmp.felk.cvut.cz>
Cc: Marc Kleine-Budde <mkl@pengutronix.de>
Cc: linux-can@vger.kernel.org
Link: http://lkml.kernel.org/r/alpine.LFD.2.02.1303071450130.22263@ionos
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
include/linux/irqdesc.h
kernel/irq/manage.c
kernel/irq/spurious.c