summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 216c4a7)
raw | patch | inline | side by side (parent: 216c4a7)
author | Paul Moore <pmoore@redhat.com> | |
Wed, 4 Dec 2013 21:10:51 +0000 (16:10 -0500) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Fri, 20 Dec 2013 15:45:09 +0000 (07:45 -0800) |
commit 446b802437f285de68ffb8d6fac3c44c3cab5b04 upstream.
In selinux_ip_postroute() we perform access checks based on the
packet's security label. For locally generated traffic we get the
packet's security label from the associated socket; this works in all
cases except for TCP SYN-ACK packets. In the case of SYN-ACK packet's
the correct security label is stored in the connection's request_sock,
not the server's socket. Unfortunately, at the point in time when
selinux_ip_postroute() is called we can't query the request_sock
directly, we need to recreate the label using the same logic that
originally labeled the associated request_sock.
See the inline comments for more explanation.
Reported-by: Janak Desai <Janak.Desai@gtri.gatech.edu>
Tested-by: Janak Desai <Janak.Desai@gtri.gatech.edu>
Signed-off-by: Paul Moore <pmoore@redhat.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
In selinux_ip_postroute() we perform access checks based on the
packet's security label. For locally generated traffic we get the
packet's security label from the associated socket; this works in all
cases except for TCP SYN-ACK packets. In the case of SYN-ACK packet's
the correct security label is stored in the connection's request_sock,
not the server's socket. Unfortunately, at the point in time when
selinux_ip_postroute() is called we can't query the request_sock
directly, we need to recreate the label using the same logic that
originally labeled the associated request_sock.
See the inline comments for more explanation.
Reported-by: Janak Desai <Janak.Desai@gtri.gatech.edu>
Tested-by: Janak Desai <Janak.Desai@gtri.gatech.edu>
Signed-off-by: Paul Moore <pmoore@redhat.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
security/selinux/hooks.c | patch | blob | history |
index 27860faab12efab846a66a4cc401fd525ed7046d..5e58d7dd7b69882b5f734dc4f62e3d0b338fb4d2 100644 (file)
--- a/security/selinux/hooks.c
+++ b/security/selinux/hooks.c
@@ -3737,6 +3737,30 @@ static int selinux_skb_peerlbl_sid(struct sk_buff *skb, u16 family, u32 *sid)
return 0;
}
+/**
+ * selinux_conn_sid - Determine the child socket label for a connection
+ * @sk_sid: the parent socket's SID
+ * @skb_sid: the packet's SID
+ * @conn_sid: the resulting connection SID
+ *
+ * If @skb_sid is valid then the user:role:type information from @sk_sid is
+ * combined with the MLS information from @skb_sid in order to create
+ * @conn_sid. If @skb_sid is not valid then then @conn_sid is simply a copy
+ * of @sk_sid. Returns zero on success, negative values on failure.
+ *
+ */
+static int selinux_conn_sid(u32 sk_sid, u32 skb_sid, u32 *conn_sid)
+{
+ int err = 0;
+
+ if (skb_sid != SECSID_NULL)
+ err = security_sid_mls_copy(sk_sid, skb_sid, conn_sid);
+ else
+ *conn_sid = sk_sid;
+
+ return err;
+}
+
/* socket security operations */
static int socket_sockcreate_sid(const struct task_security_struct *tsec,
struct sk_security_struct *sksec = sk->sk_security;
int err;
u16 family = sk->sk_family;
- u32 newsid;
+ u32 connsid;
u32 peersid;
/* handle mapped IPv4 packets arriving via IPv6 sockets */
err = selinux_skb_peerlbl_sid(skb, family, &peersid);
if (err)
return err;
- if (peersid == SECSID_NULL) {
- req->secid = sksec->sid;
- req->peer_secid = SECSID_NULL;
- } else {
- err = security_sid_mls_copy(sksec->sid, peersid, &newsid);
- if (err)
- return err;
- req->secid = newsid;
- req->peer_secid = peersid;
- }
+ err = selinux_conn_sid(sksec->sid, peersid, &connsid);
+ if (err)
+ return err;
+ req->secid = connsid;
+ req->peer_secid = peersid;
return selinux_netlbl_inet_conn_request(req, family);
}
if (!secmark_active && !peerlbl_active)
return NF_ACCEPT;
- /* if the packet is being forwarded then get the peer label from the
- * packet itself; otherwise check to see if it is from a local
- * application or the kernel, if from an application get the peer label
- * from the sending socket, otherwise use the kernel's sid */
sk = skb->sk;
if (sk == NULL) {
+ /* Without an associated socket the packet is either coming
+ * from the kernel or it is being forwarded; check the packet
+ * to determine which and if the packet is being forwarded
+ * query the packet directly to determine the security label. */
if (skb->skb_iif) {
secmark_perm = PACKET__FORWARD_OUT;
if (selinux_skb_peerlbl_sid(skb, family, &peer_sid))
secmark_perm = PACKET__SEND;
peer_sid = SECINITSID_KERNEL;
}
+ } else if (sk->sk_state == TCP_LISTEN) {
+ /* Locally generated packet but the associated socket is in the
+ * listening state which means this is a SYN-ACK packet. In
+ * this particular case the correct security label is assigned
+ * to the connection/request_sock but unfortunately we can't
+ * query the request_sock as it isn't queued on the parent
+ * socket until after the SYN-ACK packet is sent; the only
+ * viable choice is to regenerate the label like we do in
+ * selinux_inet_conn_request(). See also selinux_ip_output()
+ * for similar problems. */
+ u32 skb_sid;
+ struct sk_security_struct *sksec = sk->sk_security;
+ if (selinux_skb_peerlbl_sid(skb, family, &skb_sid))
+ return NF_DROP;
+ if (selinux_conn_sid(sksec->sid, skb_sid, &peer_sid))
+ return NF_DROP;
+ secmark_perm = PACKET__SEND;
} else {
+ /* Locally generated packet, fetch the security label from the
+ * associated socket. */
struct sk_security_struct *sksec = sk->sk_security;
peer_sid = sksec->sid;
secmark_perm = PACKET__SEND;