summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 3ca6968)
raw | patch | inline | side by side (parent: 3ca6968)
author | Jacob Keller <jacob.e.keller@intel.com> | |
Fri, 6 Jun 2014 21:36:39 +0000 (14:36 -0700) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Mon, 7 Jul 2014 01:54:15 +0000 (18:54 -0700) |
commit 8401aa1f59975c03eeebd3ac6d264cbdfe9af5de upstream.
Update the SubmittingPatches process to include howto about the new
'Fixes:' tag to be used when a patch fixes an issue in a previous commit
(found by git-bisect for example).
Signed-off-by: Jacob Keller <jacob.e.keller@intel.com>
Tested-by: Aaron Brown <aaron.f.brown@intel.com>
Signed-off-by: Jeff Kirsher <jeffrey.t.kirsher@intel.com>
Cc: Randy Dunlap <rdunlap@infradead.org>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Update the SubmittingPatches process to include howto about the new
'Fixes:' tag to be used when a patch fixes an issue in a previous commit
(found by git-bisect for example).
Signed-off-by: Jacob Keller <jacob.e.keller@intel.com>
Tested-by: Aaron Brown <aaron.f.brown@intel.com>
Signed-off-by: Jeff Kirsher <jeffrey.t.kirsher@intel.com>
Cc: Randy Dunlap <rdunlap@infradead.org>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Documentation/SubmittingPatches | patch | blob | history |
index 6e97e73d87b507a996767c82bbf0fb6237bf7617..4dbba7e100a1a9ea231afa6fb85b95d170143ee7 100644 (file)
then only post say 15 or so at a time and wait for review and integration.
+If your patch fixes a bug in a specific commit, e.g. you found an issue using
+git-bisect, please use the 'Fixes:' tag with the first 12 characters of the
+SHA-1 ID, and the one line summary.
+Example:
+
+ Fixes: e21d2170f366 ("video: remove unnecessary platform_set_drvdata()")
+
+The following git-config settings can be used to add a pretty format for
+outputting the above style in the git log or git show commands
+
+ [core]
+ abbrev = 12
+ [pretty]
+ fixes = Fixes: %h (\"%s\")
4) Style check your changes.
have been included in the discussion
-14) Using Reported-by:, Tested-by:, Reviewed-by: and Suggested-by:
+14) Using Reported-by:, Tested-by:, Reviewed-by:, Suggested-by: and Fixes:
If this patch fixes a problem reported by somebody else, consider adding a
Reported-by: tag to credit the reporter for their contribution. Please
idea reporters, they will, hopefully, be inspired to help us again in the
future.
+A Fixes: tag indicates that the patch fixes an issue in a previous commit. It
+is used to make it easy to determine where a bug originated, which can help
+review a bug fix. This tag also assists the stable kernel team in determining
+which stable kernel versions should receive your fix. This is the preferred
+method for indicating a bug fixed by the patch. See #2 above for more details.
+
15) The canonical patch format