]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - keystone-linux/linux.git/commitdiff
tracing: Fix wraparound problems in "uptime" trace clock
authorTony Luck <tony.luck@intel.com>
Fri, 18 Jul 2014 18:43:01 +0000 (11:43 -0700)
committerGreg Kroah-Hartman <gregkh@linuxfoundation.org>
Thu, 31 Jul 2014 19:53:49 +0000 (12:53 -0700)
commit 58d4e21e50ff3cc57910a8abc20d7e14375d2f61 upstream.

The "uptime" trace clock added in:

    commit 8aacf017b065a805d27467843490c976835eb4a5
    tracing: Add "uptime" trace clock that uses jiffies

has wraparound problems when the system has been up more
than 1 hour 11 minutes and 34 seconds. It converts jiffies
to nanoseconds using:
        (u64)jiffies_to_usecs(jiffy) * 1000ULL
but since jiffies_to_usecs() only returns a 32-bit value, it
truncates at 2^32 microseconds.  An additional problem on 32-bit
systems is that the argument is "unsigned long", so fixing the
return value only helps until 2^32 jiffies (49.7 days on a HZ=1000
system).

Avoid these problems by using jiffies_64 as our basis, and
not converting to nanoseconds (we do convert to clock_t because
user facing API must not be dependent on internal kernel
HZ values).

Link: http://lkml.kernel.org/p/99d63c5bfe9b320a3b428d773825a37095bf6a51.1405708254.git.tony.luck@intel.com
Fixes: 8aacf017b065 "tracing: Add "uptime" trace clock that uses jiffies"
Signed-off-by: Tony Luck <tony.luck@intel.com>
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
kernel/trace/trace.c
kernel/trace/trace_clock.c

index 98a830d079b964e447a65f41a0aab6388add98e6..18cdf91b2f853d34ab09c1ae90f1d7c0ba2e300a 100644 (file)
@@ -741,7 +741,7 @@ static struct {
        { trace_clock_local,    "local",        1 },
        { trace_clock_global,   "global",       1 },
        { trace_clock_counter,  "counter",      0 },
-       { trace_clock_jiffies,  "uptime",       1 },
+       { trace_clock_jiffies,  "uptime",       0 },
        { trace_clock,          "perf",         1 },
        ARCH_TRACE_CLOCKS
 };
index 26dc348332b798eeb43a77cf2d89357512d9e8c0..57b67b1f24d1a141f88163c385e62be25cd275cf 100644 (file)
@@ -59,13 +59,14 @@ u64 notrace trace_clock(void)
 
 /*
  * trace_jiffy_clock(): Simply use jiffies as a clock counter.
+ * Note that this use of jiffies_64 is not completely safe on
+ * 32-bit systems. But the window is tiny, and the effect if
+ * we are affected is that we will have an obviously bogus
+ * timestamp on a trace event - i.e. not life threatening.
  */
 u64 notrace trace_clock_jiffies(void)
 {
-       u64 jiffy = jiffies - INITIAL_JIFFIES;
-
-       /* Return nsecs */
-       return (u64)jiffies_to_usecs(jiffy) * 1000ULL;
+       return jiffies_64_to_clock_t(jiffies_64 - INITIAL_JIFFIES);
 }
 
 /*