summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 7a147e0)
raw | patch | inline | side by side (parent: 7a147e0)
author | Johannes Weiner <hannes@cmpxchg.org> | |
Thu, 12 Sep 2013 22:13:44 +0000 (15:13 -0700) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Fri, 21 Nov 2014 17:22:56 +0000 (09:22 -0800) |
commit 3812c8c8f3953921ef18544110dafc3505c1ac62 upstream.
The memcg OOM handling is incredibly fragile and can deadlock. When a
task fails to charge memory, it invokes the OOM killer and loops right
there in the charge code until it succeeds. Comparably, any other task
that enters the charge path at this point will go to a waitqueue right
then and there and sleep until the OOM situation is resolved. The problem
is that these tasks may hold filesystem locks and the mmap_sem; locks that
the selected OOM victim may need to exit.
For example, in one reported case, the task invoking the OOM killer was
about to charge a page cache page during a write(), which holds the
i_mutex. The OOM killer selected a task that was just entering truncate()
and trying to acquire the i_mutex:
OOM invoking task:
mem_cgroup_handle_oom+0x241/0x3b0
mem_cgroup_cache_charge+0xbe/0xe0
add_to_page_cache_locked+0x4c/0x140
add_to_page_cache_lru+0x22/0x50
grab_cache_page_write_begin+0x8b/0xe0
ext3_write_begin+0x88/0x270
generic_file_buffered_write+0x116/0x290
__generic_file_aio_write+0x27c/0x480
generic_file_aio_write+0x76/0xf0 # takes ->i_mutex
do_sync_write+0xea/0x130
vfs_write+0xf3/0x1f0
sys_write+0x51/0x90
system_call_fastpath+0x18/0x1d
OOM kill victim:
do_truncate+0x58/0xa0 # takes i_mutex
do_last+0x250/0xa30
path_openat+0xd7/0x440
do_filp_open+0x49/0xa0
do_sys_open+0x106/0x240
sys_open+0x20/0x30
system_call_fastpath+0x18/0x1d
The OOM handling task will retry the charge indefinitely while the OOM
killed task is not releasing any resources.
A similar scenario can happen when the kernel OOM killer for a memcg is
disabled and a userspace task is in charge of resolving OOM situations.
In this case, ALL tasks that enter the OOM path will be made to sleep on
the OOM waitqueue and wait for userspace to free resources or increase
the group's limit. But a userspace OOM handler is prone to deadlock
itself on the locks held by the waiting tasks. For example one of the
sleeping tasks may be stuck in a brk() call with the mmap_sem held for
writing but the userspace handler, in order to pick an optimal victim,
may need to read files from /proc/<pid>, which tries to acquire the same
mmap_sem for reading and deadlocks.
This patch changes the way tasks behave after detecting a memcg OOM and
makes sure nobody loops or sleeps with locks held:
1. When OOMing in a user fault, invoke the OOM killer and restart the
fault instead of looping on the charge attempt. This way, the OOM
victim can not get stuck on locks the looping task may hold.
2. When OOMing in a user fault but somebody else is handling it
(either the kernel OOM killer or a userspace handler), don't go to
sleep in the charge context. Instead, remember the OOMing memcg in
the task struct and then fully unwind the page fault stack with
-ENOMEM. pagefault_out_of_memory() will then call back into the
memcg code to check if the -ENOMEM came from the memcg, and then
either put the task to sleep on the memcg's OOM waitqueue or just
restart the fault. The OOM victim can no longer get stuck on any
lock a sleeping task may hold.
Debugged by Michal Hocko.
Signed-off-by: Johannes Weiner <hannes@cmpxchg.org>
Reported-by: azurIt <azurit@pobox.sk>
Acked-by: Michal Hocko <mhocko@suse.cz>
Cc: David Rientjes <rientjes@google.com>
Cc: KAMEZAWA Hiroyuki <kamezawa.hiroyu@jp.fujitsu.com>
Cc: KOSAKI Motohiro <kosaki.motohiro@jp.fujitsu.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Cong Wang <xiyou.wangcong@gmail.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
The memcg OOM handling is incredibly fragile and can deadlock. When a
task fails to charge memory, it invokes the OOM killer and loops right
there in the charge code until it succeeds. Comparably, any other task
that enters the charge path at this point will go to a waitqueue right
then and there and sleep until the OOM situation is resolved. The problem
is that these tasks may hold filesystem locks and the mmap_sem; locks that
the selected OOM victim may need to exit.
For example, in one reported case, the task invoking the OOM killer was
about to charge a page cache page during a write(), which holds the
i_mutex. The OOM killer selected a task that was just entering truncate()
and trying to acquire the i_mutex:
OOM invoking task:
mem_cgroup_handle_oom+0x241/0x3b0
mem_cgroup_cache_charge+0xbe/0xe0
add_to_page_cache_locked+0x4c/0x140
add_to_page_cache_lru+0x22/0x50
grab_cache_page_write_begin+0x8b/0xe0
ext3_write_begin+0x88/0x270
generic_file_buffered_write+0x116/0x290
__generic_file_aio_write+0x27c/0x480
generic_file_aio_write+0x76/0xf0 # takes ->i_mutex
do_sync_write+0xea/0x130
vfs_write+0xf3/0x1f0
sys_write+0x51/0x90
system_call_fastpath+0x18/0x1d
OOM kill victim:
do_truncate+0x58/0xa0 # takes i_mutex
do_last+0x250/0xa30
path_openat+0xd7/0x440
do_filp_open+0x49/0xa0
do_sys_open+0x106/0x240
sys_open+0x20/0x30
system_call_fastpath+0x18/0x1d
The OOM handling task will retry the charge indefinitely while the OOM
killed task is not releasing any resources.
A similar scenario can happen when the kernel OOM killer for a memcg is
disabled and a userspace task is in charge of resolving OOM situations.
In this case, ALL tasks that enter the OOM path will be made to sleep on
the OOM waitqueue and wait for userspace to free resources or increase
the group's limit. But a userspace OOM handler is prone to deadlock
itself on the locks held by the waiting tasks. For example one of the
sleeping tasks may be stuck in a brk() call with the mmap_sem held for
writing but the userspace handler, in order to pick an optimal victim,
may need to read files from /proc/<pid>, which tries to acquire the same
mmap_sem for reading and deadlocks.
This patch changes the way tasks behave after detecting a memcg OOM and
makes sure nobody loops or sleeps with locks held:
1. When OOMing in a user fault, invoke the OOM killer and restart the
fault instead of looping on the charge attempt. This way, the OOM
victim can not get stuck on locks the looping task may hold.
2. When OOMing in a user fault but somebody else is handling it
(either the kernel OOM killer or a userspace handler), don't go to
sleep in the charge context. Instead, remember the OOMing memcg in
the task struct and then fully unwind the page fault stack with
-ENOMEM. pagefault_out_of_memory() will then call back into the
memcg code to check if the -ENOMEM came from the memcg, and then
either put the task to sleep on the memcg's OOM waitqueue or just
restart the fault. The OOM victim can no longer get stuck on any
lock a sleeping task may hold.
Debugged by Michal Hocko.
Signed-off-by: Johannes Weiner <hannes@cmpxchg.org>
Reported-by: azurIt <azurit@pobox.sk>
Acked-by: Michal Hocko <mhocko@suse.cz>
Cc: David Rientjes <rientjes@google.com>
Cc: KAMEZAWA Hiroyuki <kamezawa.hiroyu@jp.fujitsu.com>
Cc: KOSAKI Motohiro <kosaki.motohiro@jp.fujitsu.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Cong Wang <xiyou.wangcong@gmail.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
index 2c911c95b1ac17304e39969a3d70cc55a6d0a9f2..64591ffc2e2cbe71cc5ee248b9576a9107376ad2 100644 (file)
*
* Toggle whether a failed memcg charge should invoke the OOM killer
* or just return -ENOMEM. Returns the previous toggle state.
+ *
+ * NOTE: Any path that enables the OOM killer before charging must
+ * call mem_cgroup_oom_synchronize() afterward to finalize the
+ * OOM handling and clean up.
*/
static inline bool mem_cgroup_toggle_oom(bool new)
{
WARN_ON(old == false);
}
+static inline bool task_in_memcg_oom(struct task_struct *p)
+{
+ return p->memcg_oom.in_memcg_oom;
+}
+
+bool mem_cgroup_oom_synchronize(void);
+
#ifdef CONFIG_MEMCG_SWAP
extern int do_swap_account;
#endif
{
}
+static inline bool task_in_memcg_oom(struct task_struct *p)
+{
+ return false;
+}
+
+static inline bool mem_cgroup_oom_synchronize(void)
+{
+ return false;
+}
+
static inline void mem_cgroup_inc_page_stat(struct page *page,
enum mem_cgroup_page_stat_item idx)
{
diff --git a/include/linux/sched.h b/include/linux/sched.h
index 42a58ce480bcf466537e3361cd0b475dec32d972..a1b7e6ee453b1f17c2a10c162fb7e27330304ace 100644 (file)
--- a/include/linux/sched.h
+++ b/include/linux/sched.h
unsigned int memcg_kmem_skip_account;
struct memcg_oom_info {
unsigned int may_oom:1;
+ unsigned int in_memcg_oom:1;
+ unsigned int oom_locked:1;
+ int wakeups;
+ struct mem_cgroup *wait_on_memcg;
} memcg_oom;
#endif
#ifdef CONFIG_HAVE_HW_BREAKPOINT
diff --git a/mm/memcontrol.c b/mm/memcontrol.c
index 333bb91ee3f2026d0960df62d66b27eefd7b4ce8..7849660665d711f1eedfe97c5ebd66975afa34cb 100644 (file)
--- a/mm/memcontrol.c
+++ b/mm/memcontrol.c
bool oom_lock;
atomic_t under_oom;
+ atomic_t oom_wakeups;
atomic_t refcnt;
static void memcg_wakeup_oom(struct mem_cgroup *memcg)
{
+ atomic_inc(&memcg->oom_wakeups);
/* for filtering, pass "memcg" as argument. */
__wake_up(&memcg_oom_waitq, TASK_NORMAL, 0, memcg);
}
}
/*
- * try to call OOM killer. returns false if we should exit memory-reclaim loop.
+ * try to call OOM killer
*/
-static bool mem_cgroup_handle_oom(struct mem_cgroup *memcg, gfp_t mask,
- int order)
+static void mem_cgroup_oom(struct mem_cgroup *memcg, gfp_t mask, int order)
{
- struct oom_wait_info owait;
bool locked;
+ int wakeups;
- owait.memcg = memcg;
- owait.wait.flags = 0;
- owait.wait.func = memcg_oom_wake_function;
- owait.wait.private = current;
- INIT_LIST_HEAD(&owait.wait.task_list);
+ if (!current->memcg_oom.may_oom)
+ return;
+
+ current->memcg_oom.in_memcg_oom = 1;
/*
* As with any blocking lock, a contender needs to start
* otherwise it can miss the wakeup from the unlock and sleep
* indefinitely. This is just open-coded because our locking
* is so particular to memcg hierarchies.
- *
- * Even if signal_pending(), we can't quit charge() loop without
- * accounting. So, UNINTERRUPTIBLE is appropriate. But SIGKILL
- * under OOM is always welcomed, use TASK_KILLABLE here.
*/
- prepare_to_wait(&memcg_oom_waitq, &owait.wait, TASK_KILLABLE);
+ wakeups = atomic_read(&memcg->oom_wakeups);
mem_cgroup_mark_under_oom(memcg);
locked = mem_cgroup_oom_trylock(memcg);
if (locked && !memcg->oom_kill_disable) {
mem_cgroup_unmark_under_oom(memcg);
- finish_wait(&memcg_oom_waitq, &owait.wait);
mem_cgroup_out_of_memory(memcg, mask, order);
+ mem_cgroup_oom_unlock(memcg);
+ /*
+ * There is no guarantee that an OOM-lock contender
+ * sees the wakeups triggered by the OOM kill
+ * uncharges. Wake any sleepers explicitely.
+ */
+ memcg_oom_recover(memcg);
} else {
- schedule();
- mem_cgroup_unmark_under_oom(memcg);
- finish_wait(&memcg_oom_waitq, &owait.wait);
+ /*
+ * A system call can just return -ENOMEM, but if this
+ * is a page fault and somebody else is handling the
+ * OOM already, we need to sleep on the OOM waitqueue
+ * for this memcg until the situation is resolved.
+ * Which can take some time because it might be
+ * handled by a userspace task.
+ *
+ * However, this is the charge context, which means
+ * that we may sit on a large call stack and hold
+ * various filesystem locks, the mmap_sem etc. and we
+ * don't want the OOM handler to deadlock on them
+ * while we sit here and wait. Store the current OOM
+ * context in the task_struct, then return -ENOMEM.
+ * At the end of the page fault handler, with the
+ * stack unwound, pagefault_out_of_memory() will check
+ * back with us by calling
+ * mem_cgroup_oom_synchronize(), possibly putting the
+ * task to sleep.
+ */
+ current->memcg_oom.oom_locked = locked;
+ current->memcg_oom.wakeups = wakeups;
+ css_get(&memcg->css);
+ current->memcg_oom.wait_on_memcg = memcg;
}
+}
+
+/**
+ * mem_cgroup_oom_synchronize - complete memcg OOM handling
+ *
+ * This has to be called at the end of a page fault if the the memcg
+ * OOM handler was enabled and the fault is returning %VM_FAULT_OOM.
+ *
+ * Memcg supports userspace OOM handling, so failed allocations must
+ * sleep on a waitqueue until the userspace task resolves the
+ * situation. Sleeping directly in the charge context with all kinds
+ * of locks held is not a good idea, instead we remember an OOM state
+ * in the task and mem_cgroup_oom_synchronize() has to be called at
+ * the end of the page fault to put the task to sleep and clean up the
+ * OOM state.
+ *
+ * Returns %true if an ongoing memcg OOM situation was detected and
+ * finalized, %false otherwise.
+ */
+bool mem_cgroup_oom_synchronize(void)
+{
+ struct oom_wait_info owait;
+ struct mem_cgroup *memcg;
+
+ /* OOM is global, do not handle */
+ if (!current->memcg_oom.in_memcg_oom)
+ return false;
+
+ /*
+ * We invoked the OOM killer but there is a chance that a kill
+ * did not free up any charges. Everybody else might already
+ * be sleeping, so restart the fault and keep the rampage
+ * going until some charges are released.
+ */
+ memcg = current->memcg_oom.wait_on_memcg;
+ if (!memcg)
+ goto out;
+
+ if (test_thread_flag(TIF_MEMDIE) || fatal_signal_pending(current))
+ goto out_memcg;
+
+ owait.memcg = memcg;
+ owait.wait.flags = 0;
+ owait.wait.func = memcg_oom_wake_function;
+ owait.wait.private = current;
+ INIT_LIST_HEAD(&owait.wait.task_list);
- if (locked) {
+ prepare_to_wait(&memcg_oom_waitq, &owait.wait, TASK_KILLABLE);
+ /* Only sleep if we didn't miss any wakeups since OOM */
+ if (atomic_read(&memcg->oom_wakeups) == current->memcg_oom.wakeups)
+ schedule();
+ finish_wait(&memcg_oom_waitq, &owait.wait);
+out_memcg:
+ mem_cgroup_unmark_under_oom(memcg);
+ if (current->memcg_oom.oom_locked) {
mem_cgroup_oom_unlock(memcg);
/*
* There is no guarantee that an OOM-lock contender
*/
memcg_oom_recover(memcg);
}
-
- if (test_thread_flag(TIF_MEMDIE) || fatal_signal_pending(current))
- return false;
- /* Give chance to dying process */
- schedule_timeout_uninterruptible(1);
+ css_put(&memcg->css);
+ current->memcg_oom.wait_on_memcg = NULL;
+out:
+ current->memcg_oom.in_memcg_oom = 0;
return true;
}
CHARGE_RETRY, /* need to retry but retry is not bad */
CHARGE_NOMEM, /* we can't do more. return -ENOMEM */
CHARGE_WOULDBLOCK, /* GFP_WAIT wasn't set and no enough res. */
- CHARGE_OOM_DIE, /* the current is killed because of OOM */
};
static int mem_cgroup_do_charge(struct mem_cgroup *memcg, gfp_t gfp_mask,
unsigned int nr_pages, unsigned int min_pages,
- bool oom_check)
+ bool invoke_oom)
{
unsigned long csize = nr_pages * PAGE_SIZE;
struct mem_cgroup *mem_over_limit;
if (mem_cgroup_wait_acct_move(mem_over_limit))
return CHARGE_RETRY;
- /* If we don't need to call oom-killer at el, return immediately */
- if (!oom_check || !current->memcg_oom.may_oom)
- return CHARGE_NOMEM;
- /* check OOM */
- if (!mem_cgroup_handle_oom(mem_over_limit, gfp_mask, get_order(csize)))
- return CHARGE_OOM_DIE;
+ if (invoke_oom)
+ mem_cgroup_oom(mem_over_limit, gfp_mask, get_order(csize));
- return CHARGE_RETRY;
+ return CHARGE_NOMEM;
}
/*
}
do {
- bool oom_check;
+ bool invoke_oom = oom && !nr_oom_retries;
/* If killed, bypass charge */
if (fatal_signal_pending(current)) {
goto bypass;
}
- oom_check = false;
- if (oom && !nr_oom_retries) {
- oom_check = true;
- nr_oom_retries = MEM_CGROUP_RECLAIM_RETRIES;
- }
-
- ret = mem_cgroup_do_charge(memcg, gfp_mask, batch, nr_pages,
- oom_check);
+ ret = mem_cgroup_do_charge(memcg, gfp_mask, batch,
+ nr_pages, invoke_oom);
switch (ret) {
case CHARGE_OK:
break;
css_put(&memcg->css);
goto nomem;
case CHARGE_NOMEM: /* OOM routine works */
- if (!oom) {
+ if (!oom || invoke_oom) {
css_put(&memcg->css);
goto nomem;
}
- /* If oom, we never return -ENOMEM */
nr_oom_retries--;
break;
- case CHARGE_OOM_DIE: /* Killed by OOM Killer */
- css_put(&memcg->css);
- goto bypass;
}
} while (ret != CHARGE_OK);
diff --git a/mm/memory.c b/mm/memory.c
index 59f450c5c0a3d8f87577021805f2f61a651ab10d..c4ce987745e41ea200076a7ce04a06b94091f6b6 100644 (file)
--- a/mm/memory.c
+++ b/mm/memory.c
if (flags & FAULT_FLAG_USER)
mem_cgroup_disable_oom();
+ if (WARN_ON(task_in_memcg_oom(current) && !(ret & VM_FAULT_OOM)))
+ mem_cgroup_oom_synchronize();
+
return ret;
}
diff --git a/mm/oom_kill.c b/mm/oom_kill.c
index f104c7e9f61efa4cfd61d4c6af544b1eabf2806b..1a582e3aee3eb700004dd93b95cd66dee8928d0e 100644 (file)
--- a/mm/oom_kill.c
+++ b/mm/oom_kill.c
*/
void pagefault_out_of_memory(void)
{
- struct zonelist *zonelist = node_zonelist(first_online_node,
- GFP_KERNEL);
+ struct zonelist *zonelist;
+ if (mem_cgroup_oom_synchronize())
+ return;
+
+ zonelist = node_zonelist(first_online_node, GFP_KERNEL);
if (try_set_zonelist_oom(zonelist, GFP_KERNEL)) {
out_of_memory(NULL, 0, 0, NULL, false);
clear_zonelist_oom(zonelist, GFP_KERNEL);