shared_mem: Update device-tree parsing to accomodate @Addr
[keystone-linux/mpm-transport.git] / .gitignore
1 #
2 # NOTE! Don't add files that are generated in specific
3 # subdirectories here. Add them in the ".gitignore" file
4 # in that subdirectory instead.
5 #
6 # NOTE! Please use 'git ls-files -i --exclude-standard'
7 # command after changing this file, to see if there are
8 # any tracked files which get ignored after the change.
9 #
10 # Normal rules
11 #
12 .*
13 *.o
14 *.o.*
15 *.a
16 *.s
17 *.ko
18 *.so
19 *.so.dbg
20 *.mod.c
21 modules.builtin
22 *.elf
23 *.out
25 #
26 # Top-level generic files
27 #
28 /jtest
29 /mpmsrv
30 /src/ridl/GCC_LNX/
32 #
33 # git files that we don't want to ignore even it they are dot-files
34 #
35 !.gitignore
36 !.mailmap
38 # stgit generated dirs
39 patches-*
41 # cscope files
42 cscope.*
43 ncscope.*
45 #*.orig
46 *~
47 \#*#