1 #
2 # (C) Copyright 2000-2012
3 # Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4 #
5 # See file CREDITS for list of people who contributed to this
6 # project.
7 #
8 # This program is free software; you can redistribute it and/or
9 # modify it under the terms of the GNU General Public License as
10 # published by the Free Software Foundatio; either version 2 of
11 # the License, or (at your option) any later version.
12 #
13 # This program is distributed in the hope that it will be useful,
14 # but WITHOUT ANY WARRANTY; without even the implied warranty of
15 # MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 # GNU General Public License for more details.
17 #
18 # You should have received a copy of the GNU General Public License
19 # along with this program; if not, write to the Free Software
20 # Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 # MA 02111-1307 USA
22 #
24 VERSION = 2013
25 PATCHLEVEL = 01
26 SUBLEVEL =
27 EXTRAVERSION =
28 ifneq "$(SUBLEVEL)" ""
29 U_BOOT_VERSION = $(VERSION).$(PATCHLEVEL).$(SUBLEVEL)$(EXTRAVERSION)
30 else
31 U_BOOT_VERSION = $(VERSION).$(PATCHLEVEL)$(EXTRAVERSION)
32 endif
33 TIMESTAMP_FILE = $(obj)include/generated/timestamp_autogenerated.h
34 VERSION_FILE = $(obj)include/generated/version_autogenerated.h
36 HOSTARCH := $(shell uname -m | \
37 sed -e s/i.86/x86/ \
38 -e s/sun4u/sparc64/ \
39 -e s/arm.*/arm/ \
40 -e s/sa110/arm/ \
41 -e s/ppc64/powerpc/ \
42 -e s/ppc/powerpc/ \
43 -e s/macppc/powerpc/\
44 -e s/sh.*/sh/)
46 HOSTOS := $(shell uname -s | tr '[:upper:]' '[:lower:]' | \
47 sed -e 's/\(cygwin\).*/cygwin/')
49 # Set shell to bash if possible, otherwise fall back to sh
50 SHELL := $(shell if [ -x "$$BASH" ]; then echo $$BASH; \
51 else if [ -x /bin/bash ]; then echo /bin/bash; \
52 else echo sh; fi; fi)
54 export HOSTARCH HOSTOS SHELL
56 # Deal with colliding definitions from tcsh etc.
57 VENDOR=
59 #########################################################################
60 # Allow for silent builds
61 ifeq (,$(findstring s,$(MAKEFLAGS)))
62 XECHO = echo
63 else
64 XECHO = :
65 endif
67 #########################################################################
68 #
69 # U-boot build supports producing a object files to the separate external
70 # directory. Two use cases are supported:
71 #
72 # 1) Add O= to the make command line
73 # 'make O=/tmp/build all'
74 #
75 # 2) Set environement variable BUILD_DIR to point to the desired location
76 # 'export BUILD_DIR=/tmp/build'
77 # 'make'
78 #
79 # The second approach can also be used with a MAKEALL script
80 # 'export BUILD_DIR=/tmp/build'
81 # './MAKEALL'
82 #
83 # Command line 'O=' setting overrides BUILD_DIR environent variable.
84 #
85 # When none of the above methods is used the local build is performed and
86 # the object files are placed in the source directory.
87 #
89 ifdef O
90 ifeq ("$(origin O)", "command line")
91 BUILD_DIR := $(O)
92 endif
93 endif
95 # Call a source code checker (by default, "sparse") as part of the
96 # C compilation.
97 #
98 # Use 'make C=1' to enable checking of re-compiled files.
99 #
100 # See the linux kernel file "Documentation/sparse.txt" for more details,
101 # including where to get the "sparse" utility.
103 ifdef C
104 ifeq ("$(origin C)", "command line")
105 CHECKSRC := $(C)
106 endif
107 endif
108 ifndef CHECKSRC
109 CHECKSRC = 0
110 endif
111 export CHECKSRC
113 ifneq ($(BUILD_DIR),)
114 saved-output := $(BUILD_DIR)
116 # Attempt to create a output directory.
117 $(shell [ -d ${BUILD_DIR} ] || mkdir -p ${BUILD_DIR})
119 # Verify if it was successful.
120 BUILD_DIR := $(shell cd $(BUILD_DIR) && /bin/pwd)
121 $(if $(BUILD_DIR),,$(error output directory "$(saved-output)" does not exist))
122 endif # ifneq ($(BUILD_DIR),)
124 OBJTREE := $(if $(BUILD_DIR),$(BUILD_DIR),$(CURDIR))
125 SPLTREE := $(OBJTREE)/spl
126 SRCTREE := $(CURDIR)
127 TOPDIR := $(SRCTREE)
128 LNDIR := $(OBJTREE)
129 export TOPDIR SRCTREE OBJTREE SPLTREE
131 MKCONFIG := $(SRCTREE)/mkconfig
132 export MKCONFIG
134 ifneq ($(OBJTREE),$(SRCTREE))
135 REMOTE_BUILD := 1
136 export REMOTE_BUILD
137 endif
139 # $(obj) and (src) are defined in config.mk but here in main Makefile
140 # we also need them before config.mk is included which is the case for
141 # some targets like unconfig, clean, clobber, distclean, etc.
142 ifneq ($(OBJTREE),$(SRCTREE))
143 obj := $(OBJTREE)/
144 src := $(SRCTREE)/
145 else
146 obj :=
147 src :=
148 endif
149 export obj src
151 # Make sure CDPATH settings don't interfere
152 unexport CDPATH
154 #########################################################################
156 # The "tools" are needed early, so put this first
157 # Don't include stuff already done in $(LIBS)
158 # The "examples" conditionally depend on U-Boot (say, when USE_PRIVATE_LIBGCC
159 # is "yes"), so compile examples after U-Boot is compiled.
160 SUBDIR_TOOLS = tools
161 SUBDIR_EXAMPLES = examples/standalone examples/api
162 SUBDIRS = $(SUBDIR_TOOLS)
164 .PHONY : $(SUBDIRS) $(VERSION_FILE) $(TIMESTAMP_FILE)
166 ifeq ($(obj)include/config.mk,$(wildcard $(obj)include/config.mk))
168 # Include autoconf.mk before config.mk so that the config options are available
169 # to all top level build files. We need the dummy all: target to prevent the
170 # dependency target in autoconf.mk.dep from being the default.
171 all:
172 sinclude $(obj)include/autoconf.mk.dep
173 sinclude $(obj)include/autoconf.mk
175 ifndef CONFIG_SANDBOX
176 SUBDIRS += $(SUBDIR_EXAMPLES)
177 endif
179 # load ARCH, BOARD, and CPU configuration
180 include $(obj)include/config.mk
181 export ARCH CPU BOARD VENDOR SOC
183 # set default to nothing for native builds
184 ifeq ($(HOSTARCH),$(ARCH))
185 CROSS_COMPILE ?=
186 endif
188 # load other configuration
189 include $(TOPDIR)/config.mk
191 # If board code explicitly specified LDSCRIPT or CONFIG_SYS_LDSCRIPT, use
192 # that (or fail if absent). Otherwise, search for a linker script in a
193 # standard location.
195 LDSCRIPT_MAKEFILE_DIR = $(dir $(LDSCRIPT))
197 ifndef LDSCRIPT
198 #LDSCRIPT := $(TOPDIR)/board/$(BOARDDIR)/u-boot.lds.debug
199 ifdef CONFIG_SYS_LDSCRIPT
200 # need to strip off double quotes
201 LDSCRIPT := $(subst ",,$(CONFIG_SYS_LDSCRIPT))
202 endif
203 endif
205 # If there is no specified link script, we look in a number of places for it
206 ifndef LDSCRIPT
207 ifeq ($(CONFIG_NAND_U_BOOT),y)
208 LDSCRIPT := $(TOPDIR)/board/$(BOARDDIR)/u-boot-nand.lds
209 ifeq ($(wildcard $(LDSCRIPT)),)
210 LDSCRIPT := $(TOPDIR)/$(CPUDIR)/u-boot-nand.lds
211 endif
212 endif
213 ifeq ($(wildcard $(LDSCRIPT)),)
214 LDSCRIPT := $(TOPDIR)/board/$(BOARDDIR)/u-boot.lds
215 endif
216 ifeq ($(wildcard $(LDSCRIPT)),)
217 LDSCRIPT := $(TOPDIR)/$(CPUDIR)/u-boot.lds
218 endif
219 ifeq ($(wildcard $(LDSCRIPT)),)
220 LDSCRIPT := $(TOPDIR)/arch/$(ARCH)/cpu/u-boot.lds
221 # We don't expect a Makefile here
222 LDSCRIPT_MAKEFILE_DIR =
223 endif
224 ifeq ($(wildcard $(LDSCRIPT)),)
225 $(error could not find linker script)
226 endif
227 endif
229 #########################################################################
230 # U-Boot objects....order is important (i.e. start must be first)
232 OBJS = $(CPUDIR)/start.o
233 ifeq ($(CPU),x86)
234 RESET_OBJS-$(CONFIG_X86_NO_RESET_VECTOR) += $(CPUDIR)/start16.o
235 RESET_OBJS-$(CONFIG_X86_NO_RESET_VECTOR) += $(CPUDIR)/resetvec.o
236 endif
237 ifeq ($(CPU),ppc4xx)
238 OBJS += $(CPUDIR)/resetvec.o
239 endif
240 ifeq ($(CPU),mpc85xx)
241 OBJS += $(CPUDIR)/resetvec.o
242 endif
244 OBJS := $(addprefix $(obj),$(OBJS) $(RESET_OBJS-))
246 HAVE_VENDOR_COMMON_LIB = $(if $(wildcard board/$(VENDOR)/common/Makefile),y,n)
248 LIBS-y += lib/libgeneric.o
249 LIBS-y += lib/lzma/liblzma.o
250 LIBS-y += lib/lzo/liblzo.o
251 LIBS-y += lib/zlib/libz.o
252 LIBS-$(CONFIG_TIZEN) += lib/tizen/libtizen.o
253 LIBS-$(HAVE_VENDOR_COMMON_LIB) += board/$(VENDOR)/common/lib$(VENDOR).o
254 LIBS-y += $(CPUDIR)/lib$(CPU).o
255 ifdef SOC
256 LIBS-y += $(CPUDIR)/$(SOC)/lib$(SOC).o
257 endif
258 ifeq ($(CPU),ixp)
259 LIBS-y += drivers/net/npe/libnpe.o
260 endif
261 LIBS-$(CONFIG_OF_EMBED) += dts/libdts.o
262 LIBS-y += arch/$(ARCH)/lib/lib$(ARCH).o
263 LIBS-y += fs/libfs.o \
264 fs/cbfs/libcbfs.o \
265 fs/cramfs/libcramfs.o \
266 fs/ext4/libext4fs.o \
267 fs/fat/libfat.o \
268 fs/fdos/libfdos.o \
269 fs/jffs2/libjffs2.o \
270 fs/reiserfs/libreiserfs.o \
271 fs/ubifs/libubifs.o \
272 fs/yaffs2/libyaffs2.o \
273 fs/zfs/libzfs.o
274 LIBS-y += net/libnet.o
275 LIBS-y += disk/libdisk.o
276 LIBS-y += drivers/bios_emulator/libatibiosemu.o
277 LIBS-y += drivers/block/libblock.o
278 LIBS-$(CONFIG_BOOTCOUNT_LIMIT) += drivers/bootcount/libbootcount.o
279 LIBS-y += drivers/dma/libdma.o
280 LIBS-y += drivers/fpga/libfpga.o
281 LIBS-y += drivers/gpio/libgpio.o
282 LIBS-y += drivers/hwmon/libhwmon.o
283 LIBS-y += drivers/i2c/libi2c.o
284 LIBS-y += drivers/input/libinput.o
285 LIBS-y += drivers/misc/libmisc.o
286 LIBS-y += drivers/mmc/libmmc.o
287 LIBS-y += drivers/mtd/libmtd.o
288 LIBS-y += drivers/mtd/nand/libnand.o
289 LIBS-y += drivers/mtd/onenand/libonenand.o
290 LIBS-y += drivers/mtd/ubi/libubi.o
291 LIBS-y += drivers/mtd/spi/libspi_flash.o
292 LIBS-y += drivers/net/libnet.o
293 LIBS-y += drivers/net/phy/libphy.o
294 LIBS-y += drivers/pci/libpci.o
295 LIBS-y += drivers/pcmcia/libpcmcia.o
296 LIBS-y += drivers/power/libpower.o \
297 drivers/power/fuel_gauge/libfuel_gauge.o \
298 drivers/power/pmic/libpmic.o \
299 drivers/power/battery/libbattery.o
300 LIBS-y += drivers/spi/libspi.o
301 LIBS-y += drivers/dfu/libdfu.o
302 ifeq ($(CPU),mpc83xx)
303 LIBS-y += drivers/qe/libqe.o
304 LIBS-y += arch/powerpc/cpu/mpc8xxx/ddr/libddr.o
305 LIBS-y += arch/powerpc/cpu/mpc8xxx/lib8xxx.o
306 endif
307 ifeq ($(CPU),mpc85xx)
308 LIBS-y += drivers/qe/libqe.o
309 LIBS-y += drivers/net/fm/libfm.o
310 LIBS-y += arch/powerpc/cpu/mpc8xxx/ddr/libddr.o
311 LIBS-y += arch/powerpc/cpu/mpc8xxx/lib8xxx.o
312 endif
313 ifeq ($(CPU),mpc86xx)
314 LIBS-y += arch/powerpc/cpu/mpc8xxx/ddr/libddr.o
315 LIBS-y += arch/powerpc/cpu/mpc8xxx/lib8xxx.o
316 endif
317 LIBS-y += drivers/rtc/librtc.o
318 LIBS-y += drivers/serial/libserial.o
319 LIBS-y += drivers/sound/libsound.o
320 LIBS-$(CONFIG_GENERIC_LPC_TPM) += drivers/tpm/libtpm.o
321 LIBS-y += drivers/twserial/libtws.o
322 LIBS-y += drivers/usb/eth/libusb_eth.o
323 LIBS-y += drivers/usb/gadget/libusb_gadget.o
324 LIBS-y += drivers/usb/host/libusb_host.o
325 LIBS-y += drivers/usb/musb/libusb_musb.o
326 LIBS-y += drivers/usb/musb-new/libusb_musb-new.o
327 LIBS-y += drivers/usb/phy/libusb_phy.o
328 LIBS-y += drivers/usb/ulpi/libusb_ulpi.o
329 LIBS-y += drivers/video/libvideo.o
330 LIBS-y += drivers/watchdog/libwatchdog.o
331 LIBS-y += common/libcommon.o
332 LIBS-y += lib/libfdt/libfdt.o
333 LIBS-y += api/libapi.o
334 LIBS-y += post/libpost.o
335 LIBS-y += test/libtest.o
336 LIBS-y += drivers/rapidio/librio.o
338 ifneq ($(CONFIG_AM33XX)$(CONFIG_OMAP34XX)$(CONFIG_OMAP44XX)$(CONFIG_OMAP54XX),)
339 LIBS-y += $(CPUDIR)/omap-common/libomap-common.o
340 endif
342 ifneq (,$(filter $(SOC), mx25 mx27 mx5 mx6 mx31 mx35))
343 LIBS-y += arch/$(ARCH)/imx-common/libimx-common.o
344 endif
346 ifeq ($(SOC),s5pc1xx)
347 LIBS-y += $(CPUDIR)/s5p-common/libs5p-common.o
348 endif
349 ifeq ($(SOC),exynos)
350 LIBS-y += $(CPUDIR)/s5p-common/libs5p-common.o
351 endif
352 ifeq ($(SOC),tegra20)
353 LIBS-y += arch/$(ARCH)/cpu/$(SOC)-common/lib$(SOC)-common.o
354 LIBS-y += arch/$(ARCH)/cpu/tegra-common/libcputegra-common.o
355 LIBS-y += $(CPUDIR)/tegra-common/libtegra-common.o
356 endif
358 LIBS := $(addprefix $(obj),$(sort $(LIBS-y)))
359 .PHONY : $(LIBS)
361 LIBBOARD = board/$(BOARDDIR)/lib$(BOARD).o
362 LIBBOARD := $(addprefix $(obj),$(LIBBOARD))
364 # Add GCC lib
365 ifdef USE_PRIVATE_LIBGCC
366 ifeq ("$(USE_PRIVATE_LIBGCC)", "yes")
367 PLATFORM_LIBGCC = $(OBJTREE)/arch/$(ARCH)/lib/libgcc.o
368 else
369 PLATFORM_LIBGCC = -L $(USE_PRIVATE_LIBGCC) -lgcc
370 endif
371 else
372 PLATFORM_LIBGCC := -L $(shell dirname `$(CC) $(CFLAGS) -print-libgcc-file-name`) -lgcc
373 endif
374 PLATFORM_LIBS += $(PLATFORM_LIBGCC)
375 export PLATFORM_LIBS
377 # Special flags for CPP when processing the linker script.
378 # Pass the version down so we can handle backwards compatibility
379 # on the fly.
380 LDPPFLAGS += \
381 -include $(TOPDIR)/include/u-boot/u-boot.lds.h \
382 -DCPUDIR=$(CPUDIR) \
383 $(shell $(LD) --version | \
384 sed -ne 's/GNU ld version \([0-9][0-9]*\)\.\([0-9][0-9]*\).*/-DLD_MAJOR=\1 -DLD_MINOR=\2/p')
386 __OBJS := $(subst $(obj),,$(OBJS))
387 __LIBS := $(subst $(obj),,$(LIBS)) $(subst $(obj),,$(LIBBOARD))
389 #########################################################################
390 #########################################################################
392 ifneq ($(CONFIG_BOARD_SIZE_LIMIT),)
393 BOARD_SIZE_CHECK = \
394 @actual=`wc -c $@ | awk '{print $$1}'`; \
395 limit=`printf "%d" $(CONFIG_BOARD_SIZE_LIMIT)`; \
396 if test $$actual -gt $$limit; then \
397 echo "$@ exceeds file size limit:" >&2 ; \
398 echo " limit: $$limit bytes" >&2 ; \
399 echo " actual: $$actual bytes" >&2 ; \
400 echo " excess: $$((actual - limit)) bytes" >&2; \
401 exit 1; \
402 fi
403 else
404 BOARD_SIZE_CHECK =
405 endif
407 # Always append ALL so that arch config.mk's can add custom ones
408 ALL-y += $(obj)u-boot.srec $(obj)u-boot.bin $(obj)System.map
410 ALL-$(CONFIG_NAND_U_BOOT) += $(obj)u-boot-nand.bin
411 ALL-$(CONFIG_ONENAND_U_BOOT) += $(obj)u-boot-onenand.bin
412 ALL-$(CONFIG_SPL) += $(obj)spl/u-boot-spl.bin
413 ALL-$(CONFIG_SPL) += $(obj)$(subst ",,$(CONFIG_SPL_TARGET))
414 ALL-$(CONFIG_OF_SEPARATE) += $(obj)u-boot.dtb $(obj)u-boot-dtb.bin
416 # enable combined SPL/u-boot/dtb rules for tegra
417 ifeq ($(SOC),tegra20)
418 ifeq ($(CONFIG_OF_SEPARATE),y)
419 ALL-y += $(obj)u-boot-dtb-tegra.bin
420 else
421 ALL-y += $(obj)u-boot-nodtb-tegra.bin
422 endif
423 endif
425 all: $(ALL-y) $(SUBDIR_EXAMPLES)
427 $(obj)u-boot.dtb: $(obj)u-boot
428 $(MAKE) -C dts binary
429 mv $(obj)dts/dt.dtb $@
431 $(obj)u-boot-dtb.bin: $(obj)u-boot.bin $(obj)u-boot.dtb
432 cat $^ >$@
434 $(obj)u-boot.hex: $(obj)u-boot
435 $(OBJCOPY) ${OBJCFLAGS} -O ihex $< $@
437 $(obj)u-boot.srec: $(obj)u-boot
438 $(OBJCOPY) -O srec $< $@
440 $(obj)u-boot.bin: $(obj)u-boot
441 $(OBJCOPY) ${OBJCFLAGS} -O binary $< $@
442 $(BOARD_SIZE_CHECK)
444 $(obj)u-boot.ldr: $(obj)u-boot
445 $(CREATE_LDR_ENV)
446 $(LDR) -T $(CONFIG_BFIN_CPU) -c $@ $< $(LDR_FLAGS)
447 $(BOARD_SIZE_CHECK)
449 $(obj)u-boot.ldr.hex: $(obj)u-boot.ldr
450 $(OBJCOPY) ${OBJCFLAGS} -O ihex $< $@ -I binary
452 $(obj)u-boot.ldr.srec: $(obj)u-boot.ldr
453 $(OBJCOPY) ${OBJCFLAGS} -O srec $< $@ -I binary
455 #
456 # U-Boot entry point, needed for booting of full-blown U-Boot
457 # from the SPL U-Boot version.
458 #
459 ifndef CONFIG_SYS_UBOOT_START
460 CONFIG_SYS_UBOOT_START := 0
461 endif
463 $(obj)u-boot.img: $(obj)u-boot.bin
464 $(obj)tools/mkimage -A $(ARCH) -T firmware -C none \
465 -O u-boot -a $(CONFIG_SYS_TEXT_BASE) \
466 -e $(CONFIG_SYS_UBOOT_START) \
467 -n $(shell sed -n -e 's/.*U_BOOT_VERSION//p' $(VERSION_FILE) | \
468 sed -e 's/"[ ]*$$/ for $(BOARD) board"/') \
469 -d $< $@
471 $(obj)u-boot.imx: $(obj)u-boot.bin
472 $(obj)tools/mkimage -n $(CONFIG_IMX_CONFIG) -T imximage \
473 -e $(CONFIG_SYS_TEXT_BASE) -d $< $@
475 $(obj)u-boot.kwb: $(obj)u-boot.bin
476 $(obj)tools/mkimage -n $(CONFIG_SYS_KWD_CONFIG) -T kwbimage \
477 -a $(CONFIG_SYS_TEXT_BASE) -e $(CONFIG_SYS_TEXT_BASE) -d $< $@
479 $(obj)u-boot.pbl: $(obj)u-boot.bin
480 $(obj)tools/mkimage -n $(CONFIG_PBLRCW_CONFIG) \
481 -R $(CONFIG_PBLPBI_CONFIG) -T pblimage \
482 -d $< $@
484 $(obj)u-boot.sha1: $(obj)u-boot.bin
485 $(obj)tools/ubsha1 $(obj)u-boot.bin
487 $(obj)u-boot.dis: $(obj)u-boot
488 $(OBJDUMP) -d $< > $@
490 $(obj)u-boot-with-spl.bin: $(obj)spl/u-boot-spl.bin $(obj)u-boot.bin
491 $(OBJCOPY) ${OBJCFLAGS} --pad-to=$(PAD_TO) -O binary $(obj)spl/u-boot-spl $(obj)spl/u-boot-spl-pad.bin
492 cat $(obj)spl/u-boot-spl-pad.bin $(obj)u-boot.bin > $@
493 rm $(obj)spl/u-boot-spl-pad.bin
495 $(obj)u-boot.ubl: $(obj)u-boot-with-spl.bin
496 $(obj)tools/mkimage -n $(UBL_CONFIG) -T ublimage \
497 -e $(CONFIG_SYS_TEXT_BASE) -d $< $(obj)u-boot.ubl
499 $(obj)u-boot.ais: $(obj)spl/u-boot-spl.bin $(obj)u-boot.img
500 $(obj)tools/mkimage -s -n $(if $(CONFIG_AIS_CONFIG_FILE),$(CONFIG_AIS_CONFIG_FILE),"/dev/null") \
501 -T aisimage \
502 -e $(CONFIG_SPL_TEXT_BASE) \
503 -d $(obj)spl/u-boot-spl.bin \
504 $(obj)spl/u-boot-spl.ais
505 $(OBJCOPY) ${OBJCFLAGS} -I binary \
506 --pad-to=$(CONFIG_SPL_MAX_SIZE) -O binary \
507 $(obj)spl/u-boot-spl.ais $(obj)spl/u-boot-spl-pad.ais
508 cat $(obj)spl/u-boot-spl-pad.ais $(obj)u-boot.img > \
509 $(obj)u-boot.ais
511 # Specify the target for use in elftosb call
512 ELFTOSB_TARGET-$(CONFIG_MX28) = imx28
514 $(obj)u-boot.sb: $(obj)u-boot.bin $(obj)spl/u-boot-spl.bin
515 elftosb -zf $(ELFTOSB_TARGET-y) -c $(TOPDIR)/$(CPUDIR)/$(SOC)/u-boot-$(ELFTOSB_TARGET-y).bd \
516 -o $(obj)u-boot.sb
518 # On x600 (SPEAr600) U-Boot is appended to U-Boot SPL.
519 # Both images are created using mkimage (crc etc), so that the ROM
520 # bootloader can check its integrity. Padding needs to be done to the
521 # SPL image (with mkimage header) and not the binary. Otherwise the resulting image
522 # which is loaded/copied by the ROM bootloader to SRAM doesn't fit.
523 # The resulting image containing both U-Boot images is called u-boot.spr
524 $(obj)u-boot.spr: $(obj)u-boot.img $(obj)spl/u-boot-spl.bin
525 $(obj)tools/mkimage -A $(ARCH) -T firmware -C none \
526 -a $(CONFIG_SPL_TEXT_BASE) -e $(CONFIG_SPL_TEXT_BASE) -n XLOADER \
527 -d $(obj)spl/u-boot-spl.bin $(obj)spl/u-boot-spl.img
528 tr "\000" "\377" < /dev/zero | dd ibs=1 count=$(CONFIG_SPL_PAD_TO) \
529 of=$(obj)spl/u-boot-spl-pad.img 2>/dev/null
530 dd if=$(obj)spl/u-boot-spl.img of=$(obj)spl/u-boot-spl-pad.img \
531 conv=notrunc 2>/dev/null
532 cat $(obj)spl/u-boot-spl-pad.img $(obj)u-boot.img > $@
534 $(obj)u-boot-spi.gph: $(obj)u-boot.img $(obj)spl/u-boot-spl.bin
535 $(obj)tools/mkimage -A $(ARCH) -T gpimage -C none \
536 -a $(CONFIG_SPL_TEXT_BASE) -e $(CONFIG_SPL_TEXT_BASE) \
537 -n SPL -d $(obj)spl/u-boot-spl.bin $(obj)spl/u-boot-spl.gph
538 $(OBJCOPY) ${OBJCFLAGS} -I binary \
539 --pad-to=$(CONFIG_SPL_PAD_TO) --gap-fill=0 -O binary \
540 $(obj)spl/u-boot-spl.gph $(obj)spl/u-boot-spl-pad.gph
541 cat $(obj)spl/u-boot-spl-pad.gph $(obj)u-boot.img > $@
543 $(obj)u-boot-nand.gph: $(obj)u-boot.bin
544 $(obj)tools/mkimage -A $(ARCH) -T gpimage -C none \
545 -a $(CONFIG_SYS_TEXT_BASE) -e $(CONFIG_SYS_TEXT_BASE) \
546 -n U-Boot -d $(obj)u-boot.bin $(obj)gph-u-boot.bin
547 @dd if=/dev/zero of=$(obj)zero.bin bs=8 count=1 2>/dev/null
548 @cat $(obj)gph-u-boot.bin $(obj)zero.bin > $@
549 @rm $(obj)zero.bin
551 ifeq ($(SOC),tegra20)
552 ifeq ($(CONFIG_OF_SEPARATE),y)
553 nodtb=dtb
554 dtbfile=$(obj)u-boot.dtb
555 else
556 nodtb=nodtb
557 dtbfile=
558 endif
560 $(obj)u-boot-$(nodtb)-tegra.bin: $(obj)spl/u-boot-spl.bin $(obj)u-boot.bin $(dtbfile)
561 $(OBJCOPY) ${OBJCFLAGS} --pad-to=$(CONFIG_SYS_TEXT_BASE) -O binary $(obj)spl/u-boot-spl $(obj)spl/u-boot-spl-pad.bin
562 cat $(obj)spl/u-boot-spl-pad.bin $(obj)u-boot.bin $(dtbfile) > $@
563 rm $(obj)spl/u-boot-spl-pad.bin
564 endif
566 $(obj)u-boot-img.bin: $(obj)spl/u-boot-spl.bin $(obj)u-boot.img
567 cat $(obj)spl/u-boot-spl.bin $(obj)u-boot.img > $@
569 ifeq ($(CONFIG_SANDBOX),y)
570 GEN_UBOOT = \
571 cd $(LNDIR) && $(CC) $(SYMS) -T $(obj)u-boot.lds \
572 -Wl,--start-group $(__LIBS) -Wl,--end-group \
573 $(PLATFORM_LIBS) -Wl,-Map -Wl,u-boot.map -o u-boot
574 else
575 GEN_UBOOT = \
576 UNDEF_LST=`$(OBJDUMP) -x $(LIBBOARD) $(LIBS) | \
577 sed -n -e 's/.*\($(SYM_PREFIX)_u_boot_list_.*\)/-u\1/p'|sort|uniq`;\
578 cd $(LNDIR) && $(LD) $(LDFLAGS) $(LDFLAGS_$(@F)) \
579 $$UNDEF_LST $(__OBJS) \
580 --start-group $(__LIBS) --end-group $(PLATFORM_LIBS) \
581 -Map u-boot.map -o u-boot
582 endif
584 $(obj)u-boot: depend \
585 $(SUBDIR_TOOLS) $(OBJS) $(LIBBOARD) $(LIBS) $(LDSCRIPT) $(obj)u-boot.lds
586 $(GEN_UBOOT)
587 ifeq ($(CONFIG_KALLSYMS),y)
588 smap=`$(call SYSTEM_MAP,$(obj)u-boot) | \
589 awk '$$2 ~ /[tTwW]/ {printf $$1 $$3 "\\\\000"}'` ; \
590 $(CC) $(CFLAGS) -DSYSTEM_MAP="\"$${smap}\"" \
591 -c common/system_map.c -o $(obj)common/system_map.o
592 $(GEN_UBOOT) $(obj)common/system_map.o
593 endif
595 $(OBJS): depend
596 $(MAKE) -C $(CPUDIR) $(if $(REMOTE_BUILD),$@,$(notdir $@))
598 $(LIBS): depend $(SUBDIR_TOOLS)
599 $(MAKE) -C $(dir $(subst $(obj),,$@))
601 $(LIBBOARD): depend $(LIBS)
602 $(MAKE) -C $(dir $(subst $(obj),,$@))
604 $(SUBDIRS): depend
605 $(MAKE) -C $@ all
607 $(SUBDIR_EXAMPLES): $(obj)u-boot
609 $(LDSCRIPT): depend
610 $(MAKE) -C $(dir $@) $(notdir $@)
612 # The following line expands into whole rule which generates u-boot.lst,
613 # the file containing u-boots LG-array linker section. This is included into
614 # $(LDSCRIPT). The function make_u_boot_list is defined in helper.mk file.
615 $(eval $(call make_u_boot_list, $(obj)include/u-boot.lst, $(LIBBOARD) $(LIBS)))
616 $(obj)u-boot.lds: $(LDSCRIPT) $(obj)include/u-boot.lst
617 $(CPP) $(CPPFLAGS) $(LDPPFLAGS) -ansi -D__ASSEMBLY__ -P - <$< >$@
619 nand_spl: $(TIMESTAMP_FILE) $(VERSION_FILE) depend
620 $(MAKE) -C nand_spl/board/$(BOARDDIR) all
622 $(obj)u-boot-nand.bin: nand_spl $(obj)u-boot.bin
623 cat $(obj)nand_spl/u-boot-spl-16k.bin $(obj)u-boot.bin > $(obj)u-boot-nand.bin
625 $(obj)spl/u-boot-spl.bin: $(SUBDIR_TOOLS) depend
626 $(MAKE) -C spl all
628 updater:
629 $(MAKE) -C tools/updater all
631 # Explicitly make _depend in subdirs containing multiple targets to prevent
632 # parallel sub-makes creating .depend files simultaneously.
633 depend dep: $(TIMESTAMP_FILE) $(VERSION_FILE) \
634 $(obj)include/autoconf.mk \
635 $(obj)include/generated/generic-asm-offsets.h \
636 $(obj)include/generated/asm-offsets.h
637 for dir in $(SUBDIRS) $(CPUDIR) $(LDSCRIPT_MAKEFILE_DIR) ; do \
638 $(MAKE) -C $$dir _depend ; done
640 TAG_SUBDIRS = $(SUBDIRS)
641 TAG_SUBDIRS += $(dir $(__LIBS))
642 TAG_SUBDIRS += include
644 FIND := find
645 FINDFLAGS := -L
647 checkstack:
648 $(CROSS_COMPILE)objdump -d $(obj)u-boot \
649 `$(FIND) $(obj) -name u-boot-spl -print` | \
650 perl $(src)tools/checkstack.pl $(ARCH)
652 tags ctags:
653 ctags -w -o $(obj)ctags `$(FIND) $(FINDFLAGS) $(TAG_SUBDIRS) \
654 -name '*.[chS]' -print`
656 etags:
657 etags -a -o $(obj)etags `$(FIND) $(FINDFLAGS) $(TAG_SUBDIRS) \
658 -name '*.[chS]' -print`
659 cscope:
660 $(FIND) $(FINDFLAGS) $(TAG_SUBDIRS) -name '*.[chS]' -print > \
661 cscope.files
662 cscope -b -q -k
664 SYSTEM_MAP = \
665 $(NM) $1 | \
666 grep -v '\(compiled\)\|\(\.o$$\)\|\( [aUw] \)\|\(\.\.ng$$\)\|\(LASH[RL]DI\)' | \
667 LC_ALL=C sort
668 $(obj)System.map: $(obj)u-boot
669 @$(call SYSTEM_MAP,$<) > $(obj)System.map
671 checkthumb:
672 @if test $(call cc-version) -lt 0404; then \
673 echo -n '*** Your GCC does not produce working '; \
674 echo 'binaries in THUMB mode.'; \
675 echo '*** Your board is configured for THUMB mode.'; \
676 false; \
677 fi
679 # GCC 3.x is reported to have problems generating the type of relocation
680 # that U-Boot wants.
681 # See http://lists.denx.de/pipermail/u-boot/2012-September/135156.html
682 checkgcc4:
683 @if test $(call cc-version) -lt 0400; then \
684 echo -n '*** Your GCC is too old, please upgrade to GCC 4.x or newer'; \
685 false; \
686 fi
688 #
689 # Auto-generate the autoconf.mk file (which is included by all makefiles)
690 #
691 # This target actually generates 2 files; autoconf.mk and autoconf.mk.dep.
692 # the dep file is only include in this top level makefile to determine when
693 # to regenerate the autoconf.mk file.
694 $(obj)include/autoconf.mk.dep: $(obj)include/config.h include/common.h
695 @$(XECHO) Generating $@ ; \
696 set -e ; \
697 : Generate the dependancies ; \
698 $(CC) -x c -DDO_DEPS_ONLY -M $(CFLAGS) $(CPPFLAGS) \
699 -MQ $(obj)include/autoconf.mk include/common.h > $@
701 $(obj)include/autoconf.mk: $(obj)include/config.h
702 @$(XECHO) Generating $@ ; \
703 set -e ; \
704 : Extract the config macros ; \
705 $(CPP) $(CFLAGS) -DDO_DEPS_ONLY -dM include/common.h | \
706 sed -n -f tools/scripts/define2mk.sed > $@.tmp && \
707 mv $@.tmp $@
709 $(obj)include/generated/generic-asm-offsets.h: $(obj)include/autoconf.mk.dep \
710 $(obj)lib/asm-offsets.s
711 @$(XECHO) Generating $@
712 tools/scripts/make-asm-offsets $(obj)lib/asm-offsets.s $@
714 $(obj)lib/asm-offsets.s: $(obj)include/autoconf.mk.dep \
715 $(src)lib/asm-offsets.c
716 @mkdir -p $(obj)lib
717 $(CC) -DDO_DEPS_ONLY \
718 $(CFLAGS) $(CFLAGS_$(BCURDIR)/$(@F)) $(CFLAGS_$(BCURDIR)) \
719 -o $@ $(src)lib/asm-offsets.c -c -S
721 $(obj)include/generated/asm-offsets.h: $(obj)include/autoconf.mk.dep \
722 $(obj)$(CPUDIR)/$(SOC)/asm-offsets.s
723 @$(XECHO) Generating $@
724 tools/scripts/make-asm-offsets $(obj)$(CPUDIR)/$(SOC)/asm-offsets.s $@
726 $(obj)$(CPUDIR)/$(SOC)/asm-offsets.s: $(obj)include/autoconf.mk.dep
727 @mkdir -p $(obj)$(CPUDIR)/$(SOC)
728 if [ -f $(src)$(CPUDIR)/$(SOC)/asm-offsets.c ];then \
729 $(CC) -DDO_DEPS_ONLY \
730 $(CFLAGS) $(CFLAGS_$(BCURDIR)/$(@F)) $(CFLAGS_$(BCURDIR)) \
731 -o $@ $(src)$(CPUDIR)/$(SOC)/asm-offsets.c -c -S; \
732 else \
733 touch $@; \
734 fi
736 #########################################################################
737 else # !config.mk
738 all $(obj)u-boot.hex $(obj)u-boot.srec $(obj)u-boot.bin \
739 $(obj)u-boot.img $(obj)u-boot.dis $(obj)u-boot \
740 $(filter-out tools,$(SUBDIRS)) \
741 updater depend dep tags ctags etags cscope $(obj)System.map:
742 @echo "System not configured - see README" >&2
743 @ exit 1
745 tools: $(VERSION_FILE) $(TIMESTAMP_FILE)
746 $(MAKE) -C $@ all
747 endif # config.mk
749 $(VERSION_FILE):
750 @mkdir -p $(dir $(VERSION_FILE))
751 @( localvers='$(shell $(TOPDIR)/tools/setlocalversion $(TOPDIR))' ; \
752 printf '#define PLAIN_VERSION "%s%s"\n' \
753 "$(U_BOOT_VERSION)" "$${localvers}" ; \
754 printf '#define U_BOOT_VERSION "U-Boot %s%s"\n' \
755 "$(U_BOOT_VERSION)" "$${localvers}" ; \
756 ) > $@.tmp
757 @( printf '#define CC_VERSION_STRING "%s"\n' \
758 '$(shell $(CC) --version | head -n 1)' )>> $@.tmp
759 @( printf '#define LD_VERSION_STRING "%s"\n' \
760 '$(shell $(LD) -v | head -n 1)' )>> $@.tmp
761 @cmp -s $@ $@.tmp && rm -f $@.tmp || mv -f $@.tmp $@
763 $(TIMESTAMP_FILE):
764 @mkdir -p $(dir $(TIMESTAMP_FILE))
765 @LC_ALL=C date +'#define U_BOOT_DATE "%b %d %C%y"' > $@.tmp
766 @LC_ALL=C date +'#define U_BOOT_TIME "%T"' >> $@.tmp
767 @cmp -s $@ $@.tmp && rm -f $@.tmp || mv -f $@.tmp $@
769 easylogo env gdb:
770 $(MAKE) -C tools/$@ all MTD_VERSION=${MTD_VERSION}
771 gdbtools: gdb
773 xmldocs pdfdocs psdocs htmldocs mandocs: tools/kernel-doc/docproc
774 $(MAKE) U_BOOT_VERSION=$(U_BOOT_VERSION) -C doc/DocBook/ $@
776 tools-all: easylogo env gdb $(VERSION_FILE) $(TIMESTAMP_FILE)
777 $(MAKE) -C tools HOST_TOOLS_ALL=y
779 .PHONY : CHANGELOG
780 CHANGELOG:
781 git log --no-merges U-Boot-1_1_5.. | \
782 unexpand -a | sed -e 's/\s\s*$$//' > $@
784 include/license.h: tools/bin2header COPYING
785 cat COPYING | gzip -9 -c | ./tools/bin2header license_gzip > include/license.h
786 #########################################################################
788 unconfig:
789 @rm -f $(obj)include/config.h $(obj)include/config.mk \
790 $(obj)board/*/config.tmp $(obj)board/*/*/config.tmp \
791 $(obj)include/autoconf.mk $(obj)include/autoconf.mk.dep
793 %_config:: unconfig
794 @$(MKCONFIG) -A $(@:_config=)
796 sinclude $(obj).boards.depend
797 $(obj).boards.depend: boards.cfg
798 @awk '(NF && $$1 !~ /^#/) { print $$1 ": " $$1 "_config; $$(MAKE)" }' $< > $@
800 #
801 # Functions to generate common board directory names
802 #
803 lcname = $(shell echo $(1) | sed -e 's/\(.*\)_config/\L\1/')
804 ucname = $(shell echo $(1) | sed -e 's/\(.*\)_config/\U\1/')
806 #########################################################################
807 ## ARM1176 Systems
808 #########################################################################
809 smdk6400_noUSB_config \
810 smdk6400_config : unconfig
811 @mkdir -p $(obj)include $(obj)board/samsung/smdk6400
812 @mkdir -p $(obj)nand_spl/board/samsung/smdk6400
813 @echo "#define CONFIG_NAND_U_BOOT" > $(obj)include/config.h
814 @echo "CONFIG_NAND_U_BOOT = y" >> $(obj)include/config.mk
815 @if [ -z "$(findstring smdk6400_noUSB_config,$@)" ]; then \
816 echo "RAM_TEXT = 0x57e00000" >> $(obj)board/samsung/smdk6400/config.tmp;\
817 else \
818 echo "RAM_TEXT = 0xc7e00000" >> $(obj)board/samsung/smdk6400/config.tmp;\
819 fi
820 @$(MKCONFIG) smdk6400 arm arm1176 smdk6400 samsung s3c64xx
821 @echo "CONFIG_NAND_U_BOOT = y" >> $(obj)include/config.mk
823 #########################################################################
824 #########################################################################
826 clean:
827 @rm -f $(obj)examples/standalone/82559_eeprom \
828 $(obj)examples/standalone/atmel_df_pow2 \
829 $(obj)examples/standalone/eepro100_eeprom \
830 $(obj)examples/standalone/hello_world \
831 $(obj)examples/standalone/interrupt \
832 $(obj)examples/standalone/mem_to_mem_idma2intr \
833 $(obj)examples/standalone/sched \
834 $(obj)examples/standalone/smc911{11,x}_eeprom \
835 $(obj)examples/standalone/test_burst \
836 $(obj)examples/standalone/timer
837 @rm -f $(obj)examples/api/demo{,.bin}
838 @rm -f $(obj)tools/bmp_logo $(obj)tools/easylogo/easylogo \
839 $(obj)tools/env/{fw_printenv,fw_setenv} \
840 $(obj)tools/envcrc \
841 $(obj)tools/gdb/{astest,gdbcont,gdbsend} \
842 $(obj)tools/gen_eth_addr $(obj)tools/img2srec \
843 $(obj)tools/mk{env,}image $(obj)tools/mpc86x_clk \
844 $(obj)tools/mk{smdk5250,}spl \
845 $(obj)tools/mxsboot \
846 $(obj)tools/ncb $(obj)tools/ubsha1 \
847 $(obj)tools/kernel-doc/docproc
848 @rm -f $(obj)board/cray/L1/{bootscript.c,bootscript.image} \
849 $(obj)board/matrix_vision/*/bootscript.img \
850 $(obj)board/voiceblue/eeprom \
851 $(obj)u-boot.lds \
852 $(obj)include/u-boot.lst \
853 $(obj)arch/blackfin/cpu/bootrom-asm-offsets.[chs] \
854 $(obj)arch/blackfin/cpu/init.{lds,elf}
855 @rm -f $(obj)include/bmp_logo.h
856 @rm -f $(obj)include/bmp_logo_data.h
857 @rm -f $(obj)lib/asm-offsets.s
858 @rm -f $(obj)include/generated/asm-offsets.h
859 @rm -f $(obj)$(CPUDIR)/$(SOC)/asm-offsets.s
860 @rm -f $(TIMESTAMP_FILE) $(VERSION_FILE)
861 @$(MAKE) -s -C doc/DocBook/ cleandocs
862 @find $(OBJTREE) -type f \
863 \( -name 'core' -o -name '*.bak' -o -name '*~' -o -name '*.su' \
864 -o -name '*.o' -o -name '*.a' -o -name '*.exe' \) -print \
865 | xargs rm -f
867 # Removes everything not needed for testing u-boot
868 tidy: clean
869 @find $(OBJTREE) -type f \( -name '*.depend*' \) -print | xargs rm -f
871 clobber: tidy
872 @find $(OBJTREE) -type f \( -name '*.srec' \
873 -o -name '*.bin' -o -name u-boot.img \) \
874 -print0 | xargs -0 rm -f
875 @rm -f $(OBJS) $(obj)*.bak $(obj)ctags $(obj)etags $(obj)TAGS \
876 $(obj)cscope.* $(obj)*.*~
877 @rm -f $(obj)u-boot $(obj)u-boot.map $(obj)u-boot.hex $(ALL-y)
878 @rm -f $(obj)u-boot.kwb
879 @rm -f $(obj)u-boot.pbl
880 @rm -f $(obj)u-boot.imx
881 @rm -f $(obj)u-boot.ubl
882 @rm -f $(obj)u-boot.ais
883 @rm -f $(obj)u-boot.dtb
884 @rm -f $(obj)u-boot.sb
885 @rm -f $(obj)u-boot.spr
886 @rm -f $(obj)u-boot-*.gph
887 @rm -f $(obj)nand_spl/{u-boot.{lds,lst},System.map}
888 @rm -f $(obj)nand_spl/{u-boot-nand_spl.lds,u-boot-spl,u-boot-spl.map}
889 @rm -f $(obj)spl/{u-boot-spl,u-boot-spl.bin,u-boot-spl.map}
890 @rm -f $(obj)spl/{u-boot-spl.lds,u-boot.lst}
891 @rm -f $(obj)spl/{u-boot-spl.gph,u-boot-spl-pad.gph}
892 @rm -f $(obj)MLO MLO.byteswap
893 @rm -f $(obj)SPL
894 @rm -f $(obj)tools/xway-swap-bytes
895 @rm -f $(obj)arch/powerpc/cpu/mpc824x/bedbug_603e.c
896 @rm -f $(obj)arch/powerpc/cpu/mpc83xx/ddr-gen?.c
897 @rm -fr $(obj)include/asm/proc $(obj)include/asm/arch $(obj)include/asm
898 @rm -fr $(obj)include/generated
899 @[ ! -d $(obj)nand_spl ] || find $(obj)nand_spl -name "*" -type l -print | xargs rm -f
900 @rm -f $(obj)dts/*.tmp
901 @rm -f $(obj)spl/u-boot-spl{,-pad}.ais
903 mrproper \
904 distclean: clobber unconfig
905 ifneq ($(OBJTREE),$(SRCTREE))
906 rm -rf $(obj)*
907 endif
909 backup:
910 F=`basename $(TOPDIR)` ; cd .. ; \
911 gtar --force-local -zcvf `LC_ALL=C date "+$$F-%Y-%m-%d-%T.tar.gz"` $$F
913 #########################################################################